Controls an IMD or IMDx measurement configuration.
|
SENSe:IMD: CSO: | OFFSet CTB | OFFSet FREQuency | DFRequency | [:CW] | STARt | STOP | F1[:CW] | F2[:CW] | FCENter | [:CW] | STARt | STOP | CENTer | SPAN HOPRoduct | ACTive? IFBWidth | MAIN | IMTone NORMalized | MODE | INPut | LO1 | LO2 | OUTPut | RF2 RECeiver | CONFig | COMBiner | PATH | REFerence | SORDer | ACTive? TPOWer | F1 | F2 | F1:START | F1:STOP | F2:START | F2:STOP | LEVel | SET |
Click on a keyword to view the command details.
Blue commands are superseded.
CALCulate:MEASure:DEFine - creates a Swept IMD measurement.
Swept IMD Calibration - these are supplemental to the Guided Cal commands.
Use std channel commands to set Source and Receiver Attenuation.
SENS:ROLE:DEVice “RF2” - use an external source for f2.
See Also
Example Create and Cal an IMD Measurement
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the sweep type for the IMD measurement. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<char> |
Sweep type. Choose from:
For each sweep type, use the commands that follow: FCENTer: DFRequency POWer CW SEGMent - Not available for IMDx.
LOPower - IMDx ONLY |
|
Examples |
SENS:IMD:SWEep:TYPE CW sense2:imd:sweep:type power |
|
Query Syntax |
SENSe<cnum>:IMD:SWEep:TYPE? |
|
Return Type |
Character |
|
Default |
FCENTer |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the “N = number of distortion products” value for the calculation of the CSO parameter. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Number of distortion products. |
|
Examples |
SENS:IMD:CSO:NDPR 30 sense2:imd:cso:ndproducts 7 |
|
Query Syntax |
SENSe<cnum>:IMD:CSO:NDPRoducts? |
|
Return Type |
Numeric |
|
Default |
40 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the CSO Power for POWER normalization mode. Valid only with measurement parameters: CSO2Lo and CSO2Hi and for Normalization Modes dBm and dBmV. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Power level. The units are determined by Sens:IMD:Norm:Mode, which must be set first. |
|
Examples |
SENS:IMD:CSO:NORM:POW 0 sense2:imd:cso:normalized:power -5 |
|
Query Syntax |
SENSe<cnum>:IMD:CSO:NORMalized:POWer? |
|
Return Type |
Numeric |
|
Default |
0 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the offset that is applied to CSO measurements. Valid only with measurement parameters: CSO2Lo and CSO2Hi. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Offset value in dBm |
|
Examples |
SENS:IMD:CSO:OFFS 3 sense2:imd:cso:offset 7 |
|
Query Syntax |
SENSe<cnum>:IMD:CSO:OFFSet? |
|
Return Type |
Numeric |
|
Default |
0 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the “N = Total number of carriers” value used in the calculation of the XMOD parameter. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Number of carriers. |
|
Examples |
SENS:IMD:CTB:NCAR 10 sense2:imd:ctb:ncarriers 50 |
|
Query Syntax |
SENSe<cnum>:IMD:CTB:NCARriers? |
|
Return Type |
Numeric |
|
Default |
40 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the CTB Power. Valid only with measurement parameters: CTBLo and CTBHi and for Normalization Modes dBm and dBmV. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Power level. The units are determined by Sens:IMD:Norm:Mode, which must be set first. |
|
Examples |
SENS:IMD:CTB:NORM:POW 0 sense2:imd:ctb:normalized:power -5 |
|
Query Syntax |
SENSe<cnum>:IMD:CTB:NORMalized:POWer? |
|
Return Type |
Numeric |
|
Default |
0 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the offset that is applied to CTB measurements. Valid only with measurement parameters: CTB, CTBLo, CTBHi, CTBE, CTBELo, and CTBEHi. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Offset value in dBm |
|
Examples |
SENS:IMD:CTB:OFFS 3 sense2:imd:ctb:offset 7 |
|
Query Syntax |
SENSe<cnum>:IMD:CTB:OFFSet? |
|
Return Type |
Numeric |
|
Default |
0 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns fixed tone spacing. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Tone spacing frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:DFR 1e6 sense2:imd:frequency:dfrequency:cw 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:DFRequency[:CW]? |
|
Return Type |
Numeric |
|
Default |
1 MHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the starting main tone separation for sweep type = DFRequency (delta frequency). |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Starting tone separation between F1 and F2 in Hz. Both F1 and F2 tones MUST be within the frequency range of the VNA where: F1 (start) = FREQ:FCEN – DFR:Start / 2 F2 (start) = FREQ:FCEN + DFR:Start / 2 |
|
Examples |
SENS:IMD:FREQ:DFR:STAR 1e6 sense2:imd:frequency:dfrequency:start 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:DFRequency:STARt? |
|
Return Type |
Numeric |
|
Default |
1 MHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the stopping main tone separation for sweep type = DFRequency (delta frequency). |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Stopping tone separation between F1 and F2 in Hz. Both F1 and F2 tones MUST be within the frequency range of the VNA where: F1 (stop) = FREQ:FCEN – DFR:Stop / 2 F2 (stop) = FREQ:FCEN + DFR:Stop / 2 |
|
Examples |
SENS:IMD:FREQ:DFR:STOP 1e6 sense2:imd:frequency:dfrequency:stop 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:DFRequency:STOP? |
|
Return Type |
Numeric |
|
Default |
10 MHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the frequency of the F1 tone. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
F1 tone frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:F1 1e9 sense2:imd:frequency:F1:cw 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:F1[:CW]? |
|
Return Type |
Numeric |
|
Default |
.9995 GHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the frequency of the F2 tone. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
F2 tone frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:F2 1e9 sense2:imd:frequency:F2:cw 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:F2[:CW]? |
|
Return Type |
Numeric |
|
Default |
1.0005 GHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the center frequency of the main tones. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Tone center frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:FCEN 1e9 sense2:imd:frequency:fcenter:cw 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:FCENter[:CW]? |
|
Return Type |
Numeric |
|
Default |
1.0 GHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the sweep center frequency when sweeping the main tones. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Center frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:FCEN:CENT 1e9 sense2:imd:frequency:fcenter:center 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:FCENter:CENTer? |
|
Return Type |
Numeric |
|
Default |
13.255 GHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the frequency span when sweeping the main tones. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Frequency span in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:FCEN:SPAN 1e9 sense2:imd:frequency:fcenter:span 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:FCENter:SPAN? |
|
Return Type |
Numeric |
|
Default |
26.489 GHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the start frequency when sweeping the main tones. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Start frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:FCEN:STAR 1e9 sense2:imd:frequency:fcenter:start 2e7 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:FCENter:STARt? |
|
Return Type |
Numeric |
|
Default |
10.5 MHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the stop frequency when sweeping the main tones. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Stop frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the VNA. |
|
Examples |
SENS:IMD:FREQ:FCEN:STOP 1e9 sense2:imd:frequency:fcenter:stop 2e9 |
|
Query Syntax |
SENSe<cnum>:IMD:FREQuency:FCENter:STOP? |
|
Return Type |
Numeric |
|
Default |
26.4995 GHz |
|
Applicable Models: N522xB, N524xB (Read-only) Returns the highest order product that can be measured by SweptIMD. |
|
|
Parameters |
None |
|
Examples |
SENS:IMD:HOPR? 'always returns 9 |
|
Return Type |
Numeric |
|
Default |
9 |
|
(Read-only) Returns the highest order product measured by SweptIMD. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
Examples |
SENS:IMD:HOPR:ACT? |
|
Return Type |
Numeric |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the IF Bandwidth for measurement of the main F1 and F2 tones. Learn more about setting IFBW for IMD. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Choose from: 1 | 2 | 3 | 5 | 7 | 10 | 15 | 20 | 30 | 50 | 70 | 100 | 150 | 200 | 300 | 500 | 700 | 1k | 1.5k | 2k | 3k | 5k | 7k | 10k | 15k | 20k | 30k | 50k | 70k | 100k | 150k| 200k | 280k | 360k | 600k If an invalid number is specified, the analyzer will round up to the closest valid number. |
|
Examples |
SENS:IMD:IFBW:MAIN 280e3 sense2:imd:ifbwidth:main 150K |
|
Query Syntax |
SENSe<cnum>:IMD:IFBWidth:MAIN? |
|
Return Type |
Numeric |
|
Default |
1 kHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the IF Bandwidth for measurement of the intermodulation products. Learn more about setting IFBW for IMD. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Choose from: 1 | 2 | 3 | 5 | 7 | 10 | 15 | 20 | 30 | 50 | 70 | 100 | 150 | 200 | 300 | 500 | 700 | 1k | 1.5k | 2k | 3k | 5k | 7k | 10k | 15k | 20k | 30k | 50k | 70k | 100k | 150k| 200k | 280k | 360k | 600k If an invalid number is specified, the analyzer will round up to the closest valid number. |
|
Examples |
SENS:IMD:IFBW:IMT 50 sense2:imd:ifbwidth:imtone 200 |
|
Query Syntax |
SENSe<cnum>:IMD:IFBWidth:IMTone? |
|
Return Type |
Numeric |
|
Default |
1 kHz |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the method by which CTB and CSO calculations are performed. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<char> |
Normalization mode. Choose from: NONE - the normalized power is not used in calculation NCARrier - CTB and CSO is corrected by subtracting 10*log(N/2), where
DBM - the composited normalized power for CTB or CSO is treated as a dBm value DBMV - the composited normalized power for CTB or CSO is treated as a dBmV value. Note: Power values are stored using the currently-set units. Therefore, first set units with this command, then set power values using: |
|
Examples |
SENS:IMD:NORM:MODE NCAR sense2:imd:normalized:mode none |
|
Query Syntax |
SENSe<cnum>:IMD:NORMalized:MODE? |
|
Return Type |
Character |
|
Default |
NCARrier |
|
Applicable Models: N522xB, N524xB (Write-only) Sets the input port and output port of an IMD or IMDx channel. This setting is necessary only when using the limited port mapping feature. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<input> |
VNA port connected to the DUT Input. Choose from 1 or 3. When input is 3, an external combiner must be used. |
|
<output> |
VNA port connected to the DUT Output. When input is 1, output must be 2. When input is 3, output must be 4. |
|
Examples |
SENS:IMD:PMAP 3,4 sense2:imd:pmap 3,4 |
|
Query Syntax |
Not Applicable |
|
Default |
1,2 |
|
Applicable Models: N522xB, N524xB (Read-only) Returns the VNA test port to be connected to the DUT input for an IMD or IMDx channel. Set the VNA port to DUT mapping using SENS:IMD:PMAP |
|
|
Parameters |
|
|
<cnum> |
IMD channel number. If unspecified, value is set to 1. |
|
Examples |
SENS:IMD:PMAP:INP? sense2:imd:pmap:input? |
|
Default |
1 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the source used as the LO1 tone for a Swept IMDX channel. |
|
|
Parameters |
|
|
<cnum> |
IMD channel number. If unspecified, value is set to 1. |
|
<string> |
Name of source. |
|
Example |
SENS:IMD:PMAP:LO1 "MyMXG" |
|
Query Syntax |
SENSe<cnum>:IMD:PMAP:LO1? |
|
Return Type |
String |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-only) Returns the available sources that can be used as the LO1 tone for a Swept IMDX channel. |
|
|
Parameters |
|
|
<cnum> |
IMD channel number. If unspecified, value is set to 1. |
|
Example |
SENS:IMD:PMAP:LO1:CAT? |
|
Query Syntax |
SENSe<cnum>:IMD:PMAP:LO1:CATalog? |
|
Return Type |
String |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the source used as the LO2 tone for a Swept IMDX channel. |
|
|
Parameters |
|
|
<cnum> |
IMD channel number. If unspecified, value is set to 1. |
|
<string> |
Name of source. |
|
Example |
SENS:IMD:PMAP:LO2 "MyMXG" |
|
Query Syntax |
SENSe<cnum>:IMD:PMAP:LO2? |
|
Return Type |
String |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-only) Returns the available sources that can be used as the LO2 tone for a Swept IMDX channel. |
|
|
Parameters |
|
|
<cnum> |
IMD channel number. If unspecified, value is set to 1. |
|
Example |
SENS:IMD:PMAP:LO2:CAT? |
|
Query Syntax |
SENSe<cnum>:IMD:PMAP:LO2:CATalog? |
|
Return Type |
String |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-only) Returns the VNA test port to be connected to the DUT output for an IMD or IMDx channel. Set the VNA port to DUT mapping using SENS:IMD:PMAP |
|
|
Parameters |
|
|
<cnum> |
IMD channel number. If unspecified, value is set to 1. |
|
Examples |
SENS:IMD:PMAP:OUTP? sense2:imd:pmap:output? |
|
Default |
2 |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the source used as the RF2 tone for a Swept IMD or IMDX channel. |
|
|
Parameters |
|
|
<cnum> |
IMD or IMDX channel number. If unspecified, value is set to 1. |
|
<string> |
Name of source. |
|
Example |
SENS:IMD:PMAP:RF2 "MyMXG" |
|
Query Syntax |
SENSe<cnum>:IMD:PMAP:RF2? |
|
Return Type |
String |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-only) Returns the available sources that can be used as the RF2 tone for a Swept IMD or IMDX channel. |
|
|
Parameters |
|
|
<cnum> |
IMD or IMDX channel number. If unspecified, value is set to 1. |
|
Example |
SENS:IMD:PMAP:RF2:CAT? |
|
Query Syntax |
SENSe<cnum>:IMD:PMAP:RF2:CATalog? |
|
Return Type |
String |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the receiver configuration. The number of reference receivers is set using the SENSe:IMD:RECeiver:CONFig:REFerence:COUNt command. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<enum> |
Receiver configuration. Choose from: INT - (default) this configuration is one reference receiver + internal combiner mode. EXT - this configuration is an external combiner + one reference receiver or two reference receivers. For two reference receivers, each port uses its own reference receiver. DUT - this configuration uses two reference receivers for two input tones applied to a combiner inside the DUT. Each port uses its own reference receiver. |
|
Examples |
SENSe:IMD:RECeiver:CONFig:COMBiner:PATH EXT |
|
Query Syntax |
SENSe<cnum>:IMD:RECeiver:CONFig:COMBiner:PATH? |
|
Return Type |
Enumerator |
|
Default |
INT |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the number of receivers to use in the receiver configuration. The receiver configuration is set using the SENSe:IMD:RECeiver:CONFig:COMBiner:PATH command. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Sets the number of receivers to use in the receiver configuration. |
|
Examples |
SENSe:IMD:RECeiver:CONFig:COMBiner:PATH EXT SENSe:IMD:RECeiver:CONFig:REFerence:COUNt 2 |
|
Query Syntax |
SENSe<cnum>:IMD:RECeiver:CONFig:REFerence:COUNt? |
|
Return Type |
Numeric |
|
Default |
1 |
|
Applicable Models: N522xB, N524xB (Read-only) Returns the state of whether or not 2nd order parameters are measured. A "1" or "ON" indicates 2nd order parameters are measured. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
Examples |
SENS:IMD:SORD:ACT? |
|
Return Type |
Boolean |
|
Default |
Not applicable |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the state of power coupling for F1 and F2. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<bool> |
Tone power level coupling state. Choose from: ON (or 1) - F1 and F2 power is coupled. OFF (or 0) - F1 and F2 power is NOT coupled. Set power levels individually. |
|
Examples |
SENS:IMD:TPOW:COUP 0 sense2:imd:tpower:couple:state ON |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:COUPle[:STATe]? |
|
Return Type |
Boolean |
|
Default |
ON |
|
Applicable Models: N522xB, N524xB (Read-Write) This command is replaced with SENS:IMD:TPOW:LEV Sets and returns the state of Equal Tone Power setting. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<bool> |
Equal Tone Power state. Choose from: ON (or 1) - Equalize f1 and f2 power. OFF (or 0) - Do NOT equalize f1 and f2 power. Use source power cal. |
|
Examples |
SENS:IMD:TPOW:EQU 0 sense2:imd:tpower:equalize:state ON |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:EQUalize:STATe? |
|
Return Type |
Boolean |
|
Default |
OFF |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the power level of the F1 tone. When SENS:IMD:TPOW:COUP ON (tone power is coupled), setting either F1 or F2 power sets both. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Tone power level in dBm. Choose a value between +30 dBm and -30 dBm. |
|
Examples |
SENS:IMD:TPOW:F1 0 sense2:imd:tpower:F1 -10 |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:F1? |
|
Return Type |
Numeric |
|
Default |
-24 dBm |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the power level of the F2 tone. When SENS:IMD:TPOW:COUP ON (tone power is coupled), setting either F1 or F2 power sets both. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Tone power level in dBm. Choose a value between +30 dBm and -30 dBm. |
|
Examples |
SENS:IMD:TPOW:F2 0 sense2:imd:tpower:F2 -10 |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:F2? |
|
Return Type |
Numeric |
|
Default |
-24 dBm |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the start power level of the F1 tone. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Start power in dBm. Choose a value between +30 dBm and -30 dBm. |
|
Examples |
SENS:IMD:TPOW:F1:STAR 0 sense2:imd:tpower:F1:start -10 |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:F1:STARt? |
|
Return Type |
Numeric |
|
Default |
-24 dBm |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the stop power level of the F1 tone. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Stop power in dBm. Choose a value between +30 dBm and -30 dBm. |
|
Examples |
SENS:IMD:TPOW:F1:STOP 0 sense2:imd:tpower:F1:stop 10 |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:F1:STOP? |
|
Return Type |
Numeric |
|
Default |
-10 dBm |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the start power level of the F2 tone. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Start power in dBm. Choose a value between +30 dBm and -30 dBm. |
|
Examples |
SENS:IMD:TPOW:F2:STAR 0 sense2:imd:tpower:F2:start -10 |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:F2:STARt? |
|
Return Type |
Numeric |
|
Default |
-24 dBm |
|
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the stop power level of the F2 tone. Learn more about tone power. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<num> |
Stop power in dBm. Choose a value between +30 dBm and -30 dBm. |
|
Examples |
SENS:IMD:TPOW:F2:STOP 0 sense2:imd:tpower:F2:stop 10 |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:F2:STOP? |
|
Return Type |
Numeric |
|
Default |
-10 dBm |
|
Applicable Models: N522xB, N524xB (Read-Write) This command replaces SENS:IMD:TPOW:EQU and SENS:IMD:TPOW:SET Sets and returns the tone power leveling mode. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<char> |
Choose from: NONE - (Set Input Power) The specified f1 and f2 power levels are set at the DUT input. INPut - (Set Input Power, receiver leveling) The specified f1 and f2 power levels are set at the DUT input using receiver leveling at the input reference receiver. EQUal - (Set Input Power, equal tones at output) The specified f1 and f2 power levels are set at the DUT input and a measurement is made at the output. OUTPut - (Set Output Power, receiver leveling) The specified f1 and f2 power levels are set at the DUT output. |
|
Examples |
SENS:IMD:TPOW:LEV INP sense2:imd:tpower:level output |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:LEV? |
|
Return Type |
Character |
|
Default |
NONE |
|
Applicable Models: N522xB, N524xB (Read-Write) This command is replaced with SENS:IMD:TPOW:LEV Sets and returns whether tone power is specified at the DUT input or output. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
|
<char> |
Choose from: INPUT - Specified power level is set at the DUT input. OUTPUT - Specified power level is set at the DUT output. |
|
Examples |
SENS:IMD:TPOW:SET INPUT sense2:imd:tpower:set output |
|
Query Syntax |
SENSe<cnum>:IMD:TPOWer:SET? |
|
Return Type |
Character |
|
Default |
INPUT |