Power Calibration


Note: It is recommended that SmartCal be used instead of the following Power Calibration procedures. The procedures in this topic are for those who cannot change their existing test program/procedure with their installed-base PNAs.

Note: Source and Receiver Power Calibrations are NOT available in M937xA/P937xA PXI.

Source and Receiver Power Calibrations work together to provide very accurate power levels from the source, and very accurate power measurements from the VNA receivers.

Other Source Power Cal choices

See other Calibration Topics

Source Power Calibration Overview

Note: Source and Receiver Power Calibrations are NOT available in M937xA PXI.

Perform Source Power Calibration when you need accurate power levels at some point in the measurement path between the VNA test ports. For example, you need to characterize the gain of an amplifier across a frequency range at a specified input power. You would perform a source power cal at the input of the amplifier to ensure the exact power level into the amplifier across the frequency range.

Using a Source Power Cal, you can expect the power at the point of calibration to be within the range of the uncertainty of the power meter and sensor that is used.

Source Power Calibration...

Overview of How it works:

See Important First-time USB connection note.

Click to see the detailed procedure

  1. Specify the measurement settings (frequency range, IFBW and so forth).

  2. Start Source Power Calibration.

Note: When using a Keysight N848X power sensor (sensors that do NOT have built-in calibration factors), enter the Cal Factors using the Configure Power Sensor dialog, because the VNA instructs the power meter to NOT use the Cal Factor tables internal to the power meter.

  1. Connect a power meter sensor to the point at which you want a known power level. This may be at the input or output of your device, or some other point between the test ports.

  2. The VNA source is stepped through the specified frequency range, and power is measured with the power meter. At each data point, the source power is adjusted until the measured power is within your specified accuracy level.

  3. When complete, the power meter is preset. The source power calibration can be saved as part of the instrument state.

  4. The power meter is removed and the measurement path reconnected.

  5. The calibration is automatically applied to the channel. All measurements on that channel using that source port benefit from the source power cal.

  6. Perform an S-parameter calibration AFTER a Source Power Cal. The S-parameter cal is performed using the corrected stimulus power levels for the relevant ports.

Verify the source power calibration using the following procedure.

  1. Connect the power meter as it was during the source power calibration.

  2. Set the VNA to Point Trigger mode.

  3. Trigger the VNA across the trace. Read about the behavior of the sweep indicator.

  4. At each data point, the power meter should read the corrected power level within the specified tolerance.

Supported Power Meters and Sensors

See Keysight's Power Meters and Sensors web page.

Also, to generate a list of your instrument's supported power meters and Sensors, open a command prompt window and enter the following:

reg query "HKLM\SOFTWARE\Keysight\Network Analyzer\Power Calibration\AvailablePowerMeterDrivers" /s

USB Power Sensors

USB Notes:

LAN Power Sensors

LAN Notes:

Power Meters

Power Meter Notes:

Non-Keysight Power Sensors

How to perform Source Power Calibration

Note: Guided Power Cal can be performed during an S-parameter Guided Calibration. Learn more.

  1. Setup your measurement (sweep type, frequency range, IFBW, and so forth). By default, a Source Power Cal is performed on the source port of the active measurement.

  2. Connect coax cable, GPIB cable, and power sensors to the VNA as shown in graphic below.  

This image does NOT apply to USB power sensors, which are connected directly to a VNA USB port.

See Important First-time USB connection note.

Note [E5080B-xPx] An external filter is required above 45 GHz to reduce sub-harmonics. See the power calibration at 45 GHz and above.

  1. Apply power to the power meter and allow 30 minutes warm-up time before beginning calibration.

  2. Select Source Power Cal as follows:

Using Hardkey/SoftTab/Softkey

  1. Press Cal > Main > Other Cals > Source Power Cal....

Programming Commands

  1. Complete the Source Power Cal dialog box (below), including Options, Loss Compensation and Configure Power Sensor, as needed.

Note: When using a Keysight N848X power sensor (sensors that do NOT have built-in calibration factors), enter the Cal Factors using the Configure Power Sensor dialog, because the VNA instructs the power meter to NOT use the Cal Factor tables internal to the power meter.

  1. When complete, click Calibrate in the Source Power Cal dialog box.

  2. Follow the prompts to connect the sensors as required.

  3. At this time you can change the Source Port setting and perform a Source Power Cal on a different port.

  4. When calibration is finished, click OK. Correction is then applied and turned ON for the relevant ports on the active channel.

  5. Remove sensor.

  6. SrcPwrCal is displayed in the status bar when Source Power Correction is applied to the Active Measurement.

  7. Perform a S-parameter calibration, which would use the corrected stimulus power levels for the relevant ports.

Power Calibration Setup at 45 GHz and above for M9808A, P50x8A/B/M, E5080B-xPx

When calibrating the power level at 45 GHz and above with a power sensor, a high pass filter or band pass filter (ex. Marki Microwave FH4000) is required at test port to reduce sub-harmonics. Otherwise, the power calibration cannot compensate the power level correctly due to sub harmonics. It is also recommended to use the filter during measurement, if DUT is sensitive to sub-harmonics level. (Case 1)

If the high pass filter is only used during power calibration, the insertion loss of the filter must be compensated by one of the following way (Case 2). The power calibration can be performed at several frequency segment as Use Multiple Sensors.

 

To turn Source Power Correction OFF:

  • On the Calibration menu,then click Source Power Correction on/OFF.

  • ONLY correction for the source port of the ACTIVE MEASUREMENT is turned OFF (regardless of port power coupling setting.)

Interpolation or Extrapolation

If the original stimulus settings are changed then interpolation or extrapolation is applied to the Source Power Cal and the VNA status bar will display "SrcPwrCal*".  This indicates that the correction has been modified.  If the original settings are restored, then the VNA status bar will once again display "SrcPwrCal".  This operation is different from S-Parameter correction which supports interpolation but is disabled if extrapolation is required.

 

Source Power Cal dialog box help

Note: Be sure that the frequency range of your power sensor covers the frequency range of your measurement. This does NOT occur automatically.

Channel and Port Selection

Channel  Specifies the channel on which to perform the calibration. This setting defaults to the active channel.

Source Port  Specifies the source port to be corrected. This setting defaults to the source port for the active measurement.

Note: External sources can be calibrated using this dialog. Learn more.

Calibration Reference  Choose power meter/VNA receiver to use to measure power.

  • Cal Using Power Sensor. Traditional source power calibration using only a power meter to measure the source power at each data point. Most accurate (at higher power levels) and slowest method.

Note: Because the following two settings use VNA receivers to make power measurements, they do NOT work correctly when a Frequency Offset value is being used.

  • Cal Using Sensor + Receiver.  When checked, the first reading at each data point uses a power meter to calibrate the reference receiver. Subsequent readings, if necessary to meet your accuracy requirement, are measured using the reference receiver. This technique is much faster than using the power meter, and more accurate when measuring low power levels.

Note: Do NOT use this setting if there is a component before the power sensor that exhibits non-linear behavior, such as a power amplifier in compression.  Use a power meter and Calibrate the source at multiple power levels.

  • Cal Using Receiver Only.  Select a VNA Receiver

  • Cal Using Source PMax Table  Used to provide power leveling with mmWave test set and modules. Learn more.

Buttons

Sensor Name  All power sensors are displayed in this menu even if "Active - Show in UI" has been disabled in the External Devices setup dialog. You can select "Add Sensor..." to open the External Device Configuration dialog to the power meters page and configure more sensors. If you have pressed the "Options" button and selected "Receiver Only" or "Source Power Table", then this menu displays "None" and contains no entries.

Note: Default Sensor Auto-Switching. This feature is only available for Source Power Cal and SMC Smart Cal (GUI or SCPI) when the "Enable Frequency Checking" checkbox is selected. It automatically switches the sensor channel (A - B - C - D) when the calibration frequency is out of range for the current sensor channel's specified frequency range. See also, Enable Frequency Checking.

Sensor Settings  Opens the Configure Power Sensor dialog for the currently selected power sensor.

Calibrate  Begins source power calibration measurement.This button becomes "Abort Cal" during calibration and clears the current calibration data and process if pressed. 

Multiple Sensors... Opens a new dialog box for defining multiple sensors across different frequency ranges. When selected, the readout displays "Multiple Sensors..."

Power

Cal Power  The calculated power (in dBm) at the calibration point. This value is the specified VNA source power plus the Power Offset value.

Power Offset  Allows you to specify a gain or loss (in dB) to account for components you connect between the source and the reference plane of your measurement. These components will remain during a measurement. For example, specify 10 dB to account for a 10 dB amplifier in the path to your DUT. Following the calibration, the VNA power readouts are adjusted to this value.

To account for components that will be removed when the calibration is complete, use the Loss Compensation table.

Cal Accuracy

At each data point power is measured, then adjusted until the reading is within this Cal Accuracy Tolerance or the Max Number of Readings has been met. The last power reading is plotted on the screen against the Tolerance limit lines.

Tolerance  Sets the maximum desired deviation from the specified Cal Power level in 0.005 dB increments from 0 to 5 dB

Max Number of Readings  Sets the maximum number of readings to take at each data point for iterating the source power. Enter a value between 1 and 1000.

Sensor Settling

Tolerance This value used for sensor settling. When two successive measurements differ by less than the tolerance value, then the sensor is considered to be settled, and the last measurement is used. If tolerance is set to zero, then rather than testing successive meaurements, the sensor will be measured Max Readings times and the mean of the readings will be returned. The sensor settling tolerance is defined in the Sensor Settings dialog.

Max Readings Maximum number of readings allowed for sensor settling. Default is 10.

Options

Note: At low power levels (less than -30 dBm) most power meters are not as accurate as a VNA receiver.

  • Update Active Cal Set with Source Power Cal Stores the source power correction and timestamps to the active cal set.

  • Cal Reference Receiver and Update Active Cal Set   Check to calibrate the appropriate reference receiver to the power level that is measured at the calibration plane. Do this to make very accurate measurements using the calibrated reference receiver. This cal is done in addition to the standard source power cal using the any of the methods listed above. At the end of the source power cal measurement sweep, you can optionally save the reference receiver cal to a Cal Set to be recalled at a later time. The Cal is saved when the Finish button is clicked to close the Source Power Cal dialog.

  • Characterize Source Power Linearity   Used primarily with mmWave measurements. This feature can also be used with standard VNA measurements when a component is used in the source path such as a booster amp which does NOT have linear gain or loss over frequency. If this is not true for your setup but want to improve your source power accuracy, consider using the Receiver Leveling feature. When checked, source power is measured using the specified 'Cal Reference' device (power meter/sensor or VNA receiver) and iterated on a sweep-to-sweep basis to construct a 2-dimensional power table: Power IN, Power OUT, over all frequencies.

  • Click Power Levels to launch the Source Cal Power Levels dialog box to set the power levels at which source power is to be measured.

  • The source power cal is saved, but the power table is NOT accessible.

 Source Power Cal Frequency Extenders

An uncalibrated frequency extender is inherently nonlinear. To compensate for this, the VNA provides two levels of calibration.

• Source Linearity Cal This first level cal creates a Pin/Pout table to provide a linear, controllable output power level.

• Source Power Cal This second level cal adjusts the output power to match  the requested target power.

Recommendation: the preferred method for calibrating a frequency extender starts with an installation cal launched from the Millimeter Configuration dialog.

The installation cal will create a PIn/Pout table that will survive power cycles and will be associated with a specific millimeter configuration. This calibration is often referred to as the source linearity cal.

Source Power Cal dialog This calibration behaves differently depending on the presence of a source-linearity cal created by the installation cal.

With an Installation Cal:

When an installation cal is present the extender output power can be controlled in a reasonable manner. To verify linear control, do this:

1. Create a channel

2. Measure the receiver on the port where the extender is connected. (eg: a1,1)

3. Sweep the channel

4. Normalize the reference receiver trace

5. Now adjust the power in x db steps

6. The trace should move by approximately x dB.

To achieve more accurate port power, a 2nd level source power calibration should be performed. This can be done in the Source Cal Dialog.

Power Calibration Reference The reference for this calibration can be either a power sensor or a Source PMax table.

Source PMax Table  A Source PMax Table is generally provided by the manufacturer of the extender. The data in the table represents the maximum output power available from the extender when the device is driven into saturation. The RF input power required to achieve saturation depends on the specific device and typically ranges from +2 to +12 dBm. The  Source PMax table file indicates the RF input power used to acquire the table. See the Input Power line at the top of the file. Also note that the RF Input Power to the head is limited by the setting for "RF Max Power In" defined by the Millimeter configuration dialog.

When a Source PMax table is used as the reference, the head will temporarily be driven into saturation. The VNA's reference receiver is then corrected to report the output power levels indicated by the table. The VNA reference receiver is then used to measure the extender output power and produce an offset correction array. 

When a sensor is used instead of a Source PMax table, a similar sequence is executed except that the VNA measures the extender output power using the sensor and transfers the result to the VNA reference receiver. Then the cal proceeds to servo power to the desired level and produce an offset cal while using the VNA receiver to measure the power.

Note: Unlike the Source Linearity cal, the results of this 2nd tier cal reside in the channel. It is volatile.

Without an Installation Cal If no installation cal is present, the source power cal dialog can still be used to calibrate the extender. However this calibration will take longer because it must perform both a Source Linearity cal and a Source Power cal. It may also produce a less accurate result.This calibration can be done with either a power table or a sensor. Using a sensor will be slow.

The calibration starts out at saturated levels and will show the available output power on the display. It will then loop through a long series of sweeps, dropping the input RF power to the head to acquire a PIn/POut table. This table is used to linearize the source power. The second part of the calibration will calibrate the source output power at the currently set power level. Depending on point density, some points in the sweep may fall outside the limit lines.

This entire calibration is scoped to the active channel and will be destroyed when the channel is deleted. (See above recommendation.)

Important

1.Check your port power level setting before starting this calibration! On units with no linearity cal, the default power level is usually +10 dBm. It's likely that this extender output power level cannot be achieved across the entire range of the extender. You must set the channel power below the lowest point of the maximum output power curve for the frequency range being calibrated. If the requested channel power is higher than what the extender can output across the x-axis range, then the calibration will fail. 

2.The calibration will loop over a range of Extender input RF powers. The input power range may be adjusted by pressing the "Power Levels..." button and editing the table on that dialog. 

Warnings

Calibration Warning Dialog:

If a power cal is going to be performed on a source which has the RF Pulse Modulator enabled, a warning dialog is displayed when you click Calibrate.

Disable Pulse During Power Cal  Select the checkbox to disable the RF Pulse Modulator on the source being calibrated during the power cal only and will be re-enabled after the power cal.

For Noise Figure calibrations using a noise source, the Disable Pulse during Power Cal warning can be ignored.

If the channel is NFX with a controlled LO signal that is being modulated, and the LO is being power calibrated, the pulse warning should be considered.

Finish  Applies calibration to all ports that have been calibrated. This button is disabled until there's a completed calibration on any port. 

Cancel  If a sweep is in progress, cancels the sweep. Press again to close the dialog.

Attention please: the power meter is operating in 200 r/s mode.

During a measurement, some Keysight power meters may display this message on the screen: It means that the meter is operating in 200 readings/sec which is the fastest speed setting for this meter. This is normal operation.

Frequency Checking Error Dialog:

If frequency checking has been enabled, then the VNA will check that the power sensors are defined over the calibration frequency range. If not, then this error dialog (see below) is displayed when you click the Calibrate button or, in the case of a Guided Power Calibration, the Next button.Frequency Checking is enabled in the Sensor Settings dialog.

Edit Sensor...  Opens the "Configure Power Sensor" dialog for the selected sensor. The sensor I/O is connected automatically so the dialog displays all the settings and controls, rather than just showing the "Sensor Settings..." button. From this page, you can change the sensor settings. Clicking OK returns you directly to the Source Power Cal dialog.

Cancel  Closes this dialog and returns you to the Source Power Cal dialog.

Pass / Fail Limits

Limit lines are drawn on the Source Power Cal measurement graticule area. These lines are at the Cal Power +/- the current setting of Accuracy Tolerance.  A FAIL during the Source Power Cal sweep means that the VNA was unable to measure power to within the Accuracy Tolerance. Tight tolerances are more difficult to achieve at lower Cal Power levels. When a FAIL indication appears, increase the Max Number of Readings. If this does not cause a PASS condition, then decrease the Accuracy Tolerance value.

See Also

 

 

Source Cal Power Levels dialog box help

This dialog appears when you click Power Levels on the Source Power Cal dialog.

Specify the power levels at which the Source Power will be calibrated. These values should be set to a few dB more or less than the measurement power levels.

Max Power - The highest power level at which to calibrate. This value should be a few dB higher than the highest power level of your measurement.

Note: Setting the Max Power will override power settings entered manually in a Power Table (InputPower). Therefore, when using a power table, set the Max Power value to the same value shown in the Power Table (InputPower).

Min Power - The lowest power level at which to calibrate.  This value should be a few dB lower than the lowest power level of your measurement.

Power Step - Calibrate at every incremental power level, between the Max and Min Power settings.

 

Copy a Source Power Calibration to other Channels

A macro application is now available that copies a Source Power Calibration to other channels. Once downloaded and installed on a VNA, the macro is automatically configured up. To learn more, click Help on the application main dialog.

Saving a Source Power Calibration

Because Source Power Cal calibrates source hardware, the calibration data is saved as part of the Instrument State in a .csa file only. This correction is applied to all measurements on the channel that uses the calibrated source. See Save Instrument State.

Reducing Time to Complete a Source Power Calibration

The time required to perform a Source Power Calibration depends on source power, number of points, and number of readings taken. You can reduce this measurement time with the following methods:

Receiver Power Calibration

Note: Source and Receiver Power Calibrations are NOT available in M937xA PXI.

Note: A Guided Power Cal can be performed during an S-parameter Guided Calibration. Learn more.

Receiver power calibration mathematically removes frequency response errors in the specified VNA receiver, and adjusts readings to the same, or a value offset from, the source power calibration level. It is the same as doing a Response Cal or Data / Memory, (Normalization) but with the data shifted to the Cal Power value.

Use Receiver Power Calibration to make very accurate absolute power (amplitude) measurements.

Receiver Power Calibration:

Interpolation

Like other calibration types, if the original stimulus settings are narrowed, interpolation is applied and C* Rcvr Pwr is displayed in the status bar. If the original stimulus settings are made wider, the VNA will turn Receiver Power Correction OFF.

If the original settings are restored, then receiver power calibration returns to full correction.

How to perform a Receiver Power Calibration

  1. Perform a Source Power Calibration.

  2. Set the active measurement to unratioed. Learn How.

  3. Connect a THRU line from the source port to the receiver port.

  • When performing a receiver power cal on a reference receiver (source 1 and receiver R1), no connection is necessary as the receiver is internally connected to the source.

  • When the source port and receiver port are the same (receiver A, source port 1), then connect an open or short to get maximum power to the receiver. This practice is not recommended. It is best to use different ports for the source and receiver.

  1. Ensure correction for Source Power Calibration is ON as indicated by Src Pwr Cal or Src Pwr Cal* in the status bar.

  2. Start the Calibration Wizard

Using Hardkey/SoftTab/Softkey

  1. Set the active measurement to unratioed. Learn How.

  2. Press Cal > Main > Other Cals > Receiver Power Cal....

Programming Commands

 

Select Calibration Type for Unratioed Measurement dialog box help

Cal Type Selection  Select Receiver Power

Receiver Power Configuration

Cal Power  Specifies the power level to be displayed on the measurement when complete. (Source Port Power + Power Offset).

Source Port Power  Test port Power set for the measurement.  Learn how to change Test Port Power

Power Offset  Allows you to specify a gain or loss (in dB) to account for components you connect between the source and the reference plane of your measurement AFTER a source power cal has been performed. Following the calibration, the VNA power readouts are adjusted to the Cal Power value.

Next  Click to continue the Calibration Wizard.

Notes:

  • When Receiver Power Cal is finished, 'Response' is displayed in the status bar and correction data is applied to subsequent sweeps. This is done because Receiver Power Cals are essentially Response Cals once they are stored and applied. See Saving a Receiver Power Cal below.

  • To turn correction OFF, click Cal > Main > Correction > Channel Correction OFF.

Learn more about Receiver Power Cal (scroll up).

Saving a Receiver Power Calibration

Beginning with VNA Revision 5.0, Receiver Power Cal is saved to a Cal Register and optionally to a User Cal Set. It can be applied to measurements in the same way as other Cal Types. Previously, Receiver Power Cal data was saved as part of an Instrument State and was only applied to the measurement on which it was performed.

Learn more about Saving VNA files types.