File  |  Instrument  |  Response  |  Stimulus  |  Utility  |  Cal  |  Apps  |  Remote ONLY


 

Unguided | SmartCal (Guided) | ECAL | Guided Power Cal | Cal All | Save-Recall | Cal Sets | Cal Types | Prefer's |Correction | Port Ext | Fixturing | CPM | Cal Kits | Standards | | Multiple Sensors | Source Pwr Cal | Power Sensors | Receiver Cal | Cal Data | CalPod | Custom Cal Window | AFR | Cal Update

Description

SCPI

See Also: Calibration commands for Apps

Perform an Unguided Calibration

Launch Cal Wizard

SYSTem:CORRection:WIZard

Set Cal Type

SENSe:CORRection:COLLect:METHod

Select a Cal Kit

SENSe:CORRection:COLLect:CKIT

Get a Handle to the Active Cal Kit

None

Simultaneous 2-Port Calibration

SENSe:CORRection:TSTandards

Acquisition Direction

SENSe:CORRection:SFORward

Measure a Standard

SENSe:CORRection:COLLect

Calculate Errors

SENSe:CORRection:COLLect:SAVE

Do Isolation

SENSe:CORRection:COLLect

Perform and apply Response (Normalization) cal

SENSe:CORRection:COLLect:METHod

 

Perform a Guided Cal

Initiate a Guided Cal

SENSe:CORRection:COLLect:GUIDed:INITiate

List valid Connector Types for a Port

SENSe:CORRection:COLLect:GUIDed:CONNector:CATalog?

List valid Cal Kits for a Connector type.

SENSe:CORRection:COLLect:GUIDed:CKIT:CATalog?

Select a Connector Type

SENSe:CORRection:COLLect:GUIDed:CONNector:PORT

Select a Cal Kit

SENSe:CORRection:COLLect:GUIDed:CKIT:PORT

Set cal method for each port pair.

SENSe:CORRection:COLLect:GUIDed:PATH:CMEThod

Set Thru Method for each port pair.

SENSe:CORRection:COLLect:GUIDed:PATH:TMEThod

Set Thru Port Pairs

SENSe:CORRection:COLLect:GUIDed:THRU:PORTs

Return Number of Steps in a Cal

SENSe:CORRection:COLLect:GUIDed:STEPs?

Return a Description of a Cal Step

SENSe:CORRection:COLLect:GUIDed:DESCription?

Measure a Cal Standard in a Guided Cal

SENSe:CORRection:COLLect:GUIDed:STAN

Save Cal

SENSe:CORRection:COLLect:GUIDed:SAVE

Return Number of Steps in a Cal

SENSe:CORRection:COLLect:GUIDed:LIST:COUNt?

Return number of standards for step[n]

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:COUNt?

Return step description

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:DESCription?

Return label for complete standard

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:LABel?

Return number of ports on standard used in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:PORTs?

Return label for one of the standards in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:LABel?

Return number of ports on one of the standards used in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:PORTs?

Return the enumeration for the type of standard

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:STYPe?

Return list of VNA test ports to which one of the standards is attached

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:TPORts?

Return enumeration for the type of standard device used in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STYPe?

Return list of VNA test ports to which the standard(s) in this step is attached

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:TPORts?

Return measurement parameters measured in the specified step number of a guided calibration

SENSe:CORRection:COLLect:GUIDed:DATA:CATalog?

Set and return measurement data for a specified measurement parameter of a particular step of a guided cal

SENSe:CORRection:COLLect:GUIDed:DATA

Enable/disable using existing source power calibration array when acquiring calibration standard data:

SENSe:CORRection:COLLect:GUIDed:PCAL:APPLy

Return list of ports being calibrated by an active calibration session

SENSe:CORRection:COLLect:GUIDed:PORTs?

 

Adapter settings for Unknown Thru or Adapter Removal

Sets use of a THRU adapter

SENSe:CORRection:COLLect:GUIDed:ADAPter:CREate

Set adapter delay

SENSe:CORRection:COLLect:GUIDed:ADAPter:DELay

Set adapter description

SENSe:CORRection:COLLect:GUIDed:ADAPter:DESCription

Set port pairs for adapter

SENSe:CORRection:COLLect:GUIDed:ADAPter:PATHs

Clear the settings

SENSe:CORRection:COLLect:GUIDed:ADAPter:COUNt:ZERO

Return number of adapters

SENSe:CORRection:COLLect:GUIDed:ADAPter:COUNt?

 

Optional Guided Cal commands

Auto-Orient  ECal

SENSe:CORRection:PREFerence:ECAL:ORIentation

Manual orient ECAL

SENSe:CORRection:PREFerence:ECAL:PMAP

Read orientation

SENSe:CORRection:CKIT:ECAL:ORIent?

Calculate Error Terms from a Guided Cal

SENSe:CORRection:COLLect:GUIDed:SAVE

Save Cal to an existing Cal Set GUID

SENSe:CORRection:COLLect:GUIDed:SAVE:CSET

Load Eterms during a cal

SENSe:CORRection:COLLect:GUIDed:ETERms:LOAD

Perform Isolation

SENSe:CORRection:COLLect:GUIDed:ISOLation:PATHs

Increment Avg for Isolation

SENSe:CORRection:COLLect:GUIDed:ISOLation:AVERage:INCRement

Abort Guided cal

SENSe:CORRection:COLLect:GUIDed:ABORt

Execute the Ecal calibration

SENSe:CORRection:COLLect:GUIDed:ECAL:ACQuire

Specifies the Ecal Kit for Ecal Calibration

SENSe:CORRection:COLLect:GUIDed:ECAL:SELect

Compute Error Terms

SENSe:CORRection:COLLect:GUIDed:ETERms:COMPute

 

Guided Power Cal

Use standard Source Power commands to make advanced settings.

Use Power Sensor commands to configure the power sensor.

Perform power cal

SENSe:CORRection:COLLect:GUIDed:PSENsor

Power sensor connector type

SENSe:CORRection:COLLect:GUIDed:PSENsor:CONNector

Cal Kit for power cal

SENSe:CORRection:COLLect:GUIDed:PSENsor:CKIT

Power Level for cal

SENSe:CORRection:COLLect:GUIDed:PSENsor:POWer:LEVel

Perform match-correction

SENSe:CORRection:METHods:MATCh

Sets and returns the selected ports to include in a full NPort correction.

SENSe:CORRection:METHods:PORT:SUBSet:FULL[:VALue]

Resets the full and response list to their default values.

SENSe:CORRection:METHods:PORT:SUBSet:RESet

Sets and returns the selected ports to be corrected with enhanced response calibration.

SENSe:CORRection:METHods:PORT:SUBSet:RESPonse[:VALue]

Set and return the ON/OFF subset correction state.

SENSe:CORRection:METHods:PORT:SUBSet:[:STATe]

Load Power Table

SENSe:CORRection:COLLect:GUIDed:PSENsor:POWTable

 Used with SMC on mmWave systems.

 

Perform Enhanced Response Cal

Set guided Cal method

SENSe:CORRection:COLLect:GUIDed:PATH:CMEThod

Set guided Thru method

SENSe:CORRection:COLLect:GUIDed:PATH:TMEThod

 

Perform Sliding Load Acquisition

Set preference to not prompt

SENSe:CORRection:COLLect:GUIDed:PREFerence:SLIDingload

Read iteration step

SENSe:CORRection:COLLect:GUIDed:ITERations:COUNt?

Read minimum iterations

SENSe:CORRection:COLLect:GUIDed:ITERations:MINimum?

Reset iterations

SENSe:CORRection:COLLect:GUIDed:ITERations:RESet

 

Perform an ECAL

Specify Module and Characterization

SENSe:CORRection:COLLect:ACQuire

Do ECAL 1-Port

SENSe:CORRection:COLLect:CKIT 99

Do ECAL 2-Port

SENSe:CORRection:COLLect:CKIT 99

Get ECAL Module Info

SENSe:CORRection:COLLect:CKIT:INFormation?

SENSe:CORRection:CKIT:ECAL:INFormation?

Get list of ECal Modules attached to PNA

SENSe:CORRection:CKIT:ECAL:LIST?

Get list of characterizations in ECal module

SENSe:CORRection:CKIT:ECAL:CLISt?

Perform Module Orientation during calibration

SENSe:CORRection:PREFerence:ECAL:ORIentation

Maps ECAL Module to PNA Ports

SENSe:CORRection:PREFerence:ECAL:PMAP

Reads ECal orientation

SENSe:CORRection:CKIT:ECAL:ORIent?

Perform ECal Isolation

SENSe:CORRection:COLLect:ISOLation:ECAL

Increment Avg for ECal Isolation

SENSe:CORRection:COLLect:ISOLation:AVERage:INCRement

Return the ID string of ECals

SYSTem:COMMunicate:ECAL:CATalog?

Return a list of characterizations

SYSTem:COMMunicate:ECAL:CLISt?

Return the number of installed cal kits

SYSTem:COMMunicate:ECAL:COUNt?

Delete user characterizations from VNA disk memory

SYSTem:COMMunicate:ECAL:DMEMory:CLEar

Import file into VNA disk memory

SYSTem:COMMunicate:ECAL:DMEMory:IMPort

Save existing ECal characterization to a file

SYSTem:COMMunicate:ECAL:EXPort

Read identification and characterization information for ECal module

SYSTem:COMMunicate:ECAL:INFormation?

Read identification and characterization information from  ECal module or VNA disk memory

SYSTem:COMMunicate:ECAL:KNAMe:INFormation?

Return list of index numbers for ECal modules

SYSTem:COMMunicate:ECAL:LIST?

Return number of unique states for specified path name on selected ECal module

SYSTem:COMMunicate:ECAL:PATH:COUNt?

 

Perform ECal User Characterizations

Perform User ECal Characterization

All SCPI commands

Manage PNA Disk Memory Characterizations

Delete disk memory characterizations.

SENSe:CORRection:CKIT:ECAL:DMEMory:CLEar

Saves a disk memory characterization to an archive file.

SENSe:CORRection:CKIT:ECAL:EXPort

Imports the ECal characterization from the specified archive file.

SENSe:CORRection:CKIT:ECAL:DMEMory:IMPort

Reads the user-characterization info from ECal module or PNA disk memory.

SENSe:CORRection:CKIT:ECAL:KNAMe:INFormation?

 

ECal Confidence Check

Confidence Check Parameter

SENSe:CORRection:CCHeck:PARameter

Confidence Check Acquire

SENSe:CORRection:CCHeck

Confidence Check Done

SENSe:CORRection:CCHeck:DONE

Set/Read ECal State

Sets the state of an ECAL module

CONTrol:ECAL:MODule:PATH:STATe

Read ECal state data

SENSe:CORRection:CKIT:ECAL:PATH:DATA?

Read number of ECal states for specified path

CONTrol:ECAL:MODule:PATH:COUNt?

SENSe:CORRection:CKIT:ECAL:PATH:COUNt?

 

Calibrate All Channels

Select the channels to be calibrated.

SYSTem:CALibrate:ALL:SELect

Set the IFBW

SYSTem:CALibrate:ALL:IFBW

Set the power level

SYSTem:CALibrate:ALL:PORT:SOURce:POWer

Set the power offset

SYSTem:CALibrate:ALL:PORT:SOURce:POWer:OFFSet

Set the receiver atten

SYSTem:CALibrate:ALL:PORT:RECeiver:ATTen

Set the source atten

SYSTem:CALibrate:ALL:PORT:SOURce:POWer:ATTen

Set the User Calset Prefix

SYSTem:CALibrate:ALL:CSET:PREFix

Read unique Cal properties

SYSTem:CAL:ALL:MCLass:PROPerty:NAME:CATalog?

Read unique property values

SYSTem:CAL:ALL:MCLass:PROPerty:VALue:CATalog?

Set property name/value

SYSTem:CAL:ALL:MCLass:PROPerty:VALue

Read primary Cal channel

SYSTem:CALibrate:ALL:GUIDed:CHANnel[:VALue]?

Get GuidedCal handle

None

For each channel, sets the ports to be calibrated.

SYSTem:CALibrate:ALL:CHANnel:PORTs

Returns a final list of ports to be calibrated.

SYSTem:CALibrate:ALL:GUIDed:PORTs?

Read generated Cal Sets

SYSTem:CALibrate:ALL:CSET:CATalog?

Returns all cal all guided calibration channels

SYSTem:CALibrate:ALL:GUIDed:CHANnel:LIST?

Returns available ports for independent power calibration.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:CATalog?

Adds a power cal range for a specific port <n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:ADD

Resets all ranges for the given source port <n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:CLEar

Queries how many ranges are included in the calibration for source port <n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:COUNt?

Sets and gets the number of points for range <m> for source port<n>. 

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:POINts

Sets and gets the start frequency for range <m> for source port<n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:STARt

Sets and gets the stop frequency for range <m> for source port<n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:STOP

 

Recall / Save / Apply a Calibration or Error Term

Recall a Calibration

SENSe:CORRection:CSET

Apply a Calibration to a measurement

SENSe:CORRection:CSET

Save a Calibration

SENSe:CORR:CSET:SAVE

Save or Recall an Error Term

CALCulate:DATA Scorr

Read/ Write Cal Set data

SENSe:CORRection:CSET:DATA

Apply an Error Term after Uploading

SENSe:CORRection:COLLect:APPLy

Cal Sets

Quickly test a prototype of automation software

SENSe:CORRection:CSET:CREate:DEFault

Create a Cal Set

SENSe:CORRection:CSET:CREate

Delete a Cal Set

SENSe:CORRection:CSET:DELete

List Cal Sets

CSET:CATalog?

List Cal Sets in VNA

None

Get Cal Set Information

None

List Cal Set Error Terms

SENSe:CORRection:CSET:ETERM:CATalog?

Return if a Cal Set exists

CSET:EXISts?

Select a Cal Set by GUID

SENSe:CORRection:CSET:ACTivate

Apply a Cal Set to a channel

SENSe:CORRection:CSET:ACTivate

Copy a Cal Set

SENSe:CORRection:CSET:COPY

Save a Cal Set

SENSe:CORRection:CSET:SAVE

Save Cal Sets

None

Automatically save to User Cal Set

SENSe:CORRection:PREFerence:CSET:SAVE

Change the Description of a Cal Set

SENSe:CORRection:CSET:DESCription

Change the Name of a Cal Set

SENSe:CORRection:CSET:NAME

Recall a Cal File

MMEMory:LOAD

Save 'in-memory' Cal Set to disk.

SENSe:CORRection:CSET:FLATten

Create Cal Set with De-embeded fixture removed.

CSET:FIXTure:DEEMbed

Create Cal Set with Matching Network included.

CSET:FIXTure:EMBed

Adds stimulus data to a specific buffer.

None

Returns the stimulus values over which the specific error term was acquired.

None

Returns FOM stimulus values from a Calset.

SENSe:CORRection:CSET:STIMulus?

Returns the Cal Types from the calset.

None

Returns the properties of the calset.

None

Returns the numbers of the channels using the calset.

None

Unselect Cal Set

SENSe:CORRection:CSET:DEACtivate

 

Cal Set Items

Returns names of the items in a cal set

SENSe:CORRection:CSET:ITEM:CAT?

Remove name-value pair from cal set

None

Read the value of the Cal Set item.

SENSe:CORRection:CSET:ITEM[:DATA]?

Enumerate name-value pair items in the cal set.

None

 

Apply Cal Types

Catalog ALL Cal Types for the PNA

SENSe:CORRection:TYPE:CATalog?

Catalog Cal Types in the Cal Set

SENSe:CORRection:CSET:TYPE:CATalog?

Is a specific Cal Type contained in the Cal Set?

None

Set and return the measurement Cal Type

CALCulate:MEASure:CORRection:TYPE

Set port to measure QSOLT reflection standards.

None

 

Correction Settings

Turn Correction ON|OFF for a channel

SENSe:CORRection

Turn Correction ON|OFF for a measurement

CALCulate:MEASure:CORRection[:STATe]

Interpolation ON|OFF

SENSe:CORRection:INTerpolate

Returns the error correction state for the measurement

CALCulate:MEASure:CORRection:INDicator?

 

Preferences

Set default  Cal Set Save behavior

SENSe:CORRection:PREFerence:CSET:SAVE

Sets behavior for simulated cal

SENSe:CORRection:PREFerence:SIMCal

External or internal trigger during cal

SENSe:CORRection:PREFerence:TRIG:FREE

Set ECal Auto-orient

SENSe:CORRection:PREFerence:ECAL:ORIentation

Set ECal Port Map

SENSe:CORRection:PREFerence:ECAL:PMAP

Set default Cal Type

None

 

Port Extensions

Extensions ON|OFF

SENSe:CORRection:EXTension

Port 1 Extensions Value

SENSe:CORRection:EXTension:PORT

Port 2 Extensions Value

SENSe:CORRection:EXTension:PORT

Set Freq 1|2

SENSe:CORRection:EXTension:PORT:FREQuency

Set Loss 1|2

SENSe:CORRection:EXTension:PORT:LOSS

Use 1|2

SENSe:CORRection:EXTension:PORT:INCLude

Set Loss at DC

SENSe:CORRection:EXTension:PORT:LDC

Relative Velocity

SENSe:CORRection:RVELocity:COAX

Port Ext in distance

SENSe:CORRection:EXTension:PORT:DISTance

Set distance units

SENSe:CORRection:EXTension:PORT:UNIT

Set Media per port

SENSe:CORRection:EXTension:PORT:MEDium

Set waveguide cutoff freq per port

SENSe:CORRection:EXTension:PORT:WGCutoff

Set Velocity Factor per port

SENSe:CORRection:EXTension:PORT:VELFactor

Couple to system Velocity Factor

SENSe:CORRection:EXTension:PORT:SYSVelocity

Couple to system Media type

SENSe:CORRection:EXTension:PORT:SYSMedia

 

Auto Port Extensions

Measure OPEN or SHORT for Auto Port Ext.

SENSe:CORRection:EXTension:AUTO:MEASure

Sets the frequencies used for Auto Port Ext. calculation.

SENSe:CORRection:EXTension:AUTO:CONFig

Include loss correction in Auto Port Ext.?

SENSe:CORRection:EXTension:AUTO:LOSS

Include DC Offset in Auto Port Ext.?

SENSe:CORRection:EXTension:AUTO:DCOFfset

Enable specified port for Auto Port Ext..

SENSe:CORRection:EXTension:AUTO:PORT<n>

Clears old port extension delay and loss data.

SENSe:CORRection:EXTension:AUTO:RESet

Set user span start frequency for Auto Port Ext.

SENSe:CORRection:EXTension:AUTO:STARt

Set user span stop frequency for Auto Port Ext.

SENSe:CORRection:EXTension:AUTO:STOP

 

Fixturing Commands

See also Ground Loop De-embedding/Embedding commands

Turn fixturing ON and OFF

CALCulate:FSIMulator:STATe

Change order of operations

CALCulate:FSIMulator:SENDed:OORDer

2and 4-port Extrapolate

CALCulate:FSIMulator:SNP:EXTRapolate

2-Port Fixturing

Port matching ON and OFF

CALCulate:FSIMulator:SENDed:PMCircuit:STATe

Reverse ports

CALCulate:FSIMulator:SENDed:DEEMbed:PORT<n>:SNP:REVerse

Sets Port Matching circuit model.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:TYPE

Sets Port Matching 'S2P' file name.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:USER:FILename

Sets Capacitance 'C' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:C

Sets Conductance 'G' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:G

Sets Inductance 'L' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:L

Sets Resistance 'R' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:R

De-embed ON and OFF

CALCulate:FSIMulator:SENDed:DEEMbed:STATe

Sets De-embedding circuit model.

CALCulate:FSIMulator:SENDed:DEEMbed:PORT

Sets De-embedding 'S2P' file name.

CALCulate:FSIMulator:SENDed:DEEMbed:PORT:USER:FILename

Port Impedance ON and OFF

CALCulate:FSIMulator:SENDed:ZCONversion:STATe

Port Z Real

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:REAL

Port Z Imag

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:IMAG

Port Z Real and Imag

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:Z0

4-Port Network Embed/De-embed commands

Specifies the PNA / DUT topology

CALCulate:FSIMulator:EMBed:TYPE

Specifies the 4-port touchstone file

CALCulate:FSIMulator:EMBed:NETWork:FILename

Embed|De-embed?

CALCulate:FSIMulator:EMBed:NETWork:TYPE

Specify PNA port connections

CALCulate:FSIMulator:EMBed:TOPology:A:PORTs

CALCulate:FSIMulator:EMBed:TOPology:B:PORTs

CALCulate:FSIMulator:EMBed:TOPology:C:PORTs

CALCulate:FSIMulator:EMBed:TOPology:D:PORTs

4-port remap

CALCulate:FSIMulator:EMBed:NETWork<n>:PMAP

Turn ON or OFF

CALCulate:FSIMulator:EMBed:STATe

Maps the physical VNA ports to a device of balanced and single-ended logical ports for multi-port systems with greater than 4 ports

CALCulate:DTOPology

Differential Port Arbitrary Impedance

Sets the impedance value

CALCulate:FSIMulator:BALun:DZConversion:BPORT:Z0

Sets real part of impedance

CALCulate:FSIMulator:BALun:DZConversion:BPORT:REAL

Sets imaginary part of impedance

CALCulate:FSIMulator:BALun:DZConversion:BPORT:IMAG

Turn ON or OFF

CALCulate:FSIMulator:BALun:DZConversion:STATe

Common Mode Port Arbitrary Impedance

Sets the impedance value

CALCulate:FSIMulator:BALun:CZConversion:BPORT:Z0

Sets real part of impedance

CALCulate:FSIMulator:BALun:CZConversion:BPORT:REAL

Sets imaginary part of impedance

CALCulate:FSIMulator:BALun:CZConversion:BPORT:IMAG

Turn ON or OFF

CALCulate:FSIMulator:BALun:CZConversion:STATe

Differential Port Matching

Sets type of circuit to embed.

CALCulate:FSIMulator:BALun:DMCircuit:BPORt

Specifies the 2-port touchstone file

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:USER:FILename

Sets Capacitance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:C

Sets Conductance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:G

Sets Inductance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:L

Sets Resistance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:R

Turns ON/OFF

CALCulate:FSIMulator:BALun:DMCircuit:STATe

Power Compensation

Compensate source power

CALCulate:FSIMulator:SENDed:POWer:PORT:COMPensation

Remote ONLY

Create Cal Set with De-embeded fixture removed.

CSET:FIXTure:DEEMbed

Create Cal Set with Matching network included.

CSET:FIXTure:EMBed

 

Cal Plane Manager

SCPI

Characterize a fixture

CSET:FIXTure:CHARacterize

Creates a single S2P file from two existing files.

CSET:FIXTure:CASCade

 

 

Manage and Modify Cal Kits

Set a Cal Kit Active

SENSe:CORRection:COLLect:CKIT

Clear all Cal Kits from PNA

SENSe:CORRection:CKIT:CLEar

Get a Handle to the Active Cal Kit

None

Save All Cal Kits after Modifying

None

Load collection of Kits

SENSe:CORRection:CKIT:LOAD

Load (Recall) All Cal Kits

None

Import a specified kit.

SENSe:CORRection:CKIT:IMPort

Restore Cal Kit Default

SENSe:CORRection:COLLect:CKIT:RESet

Restore ALL Cal Kits Default

SENSe:CORRection:CKIT:INITialize

Build a Hybrid Cal Kit

None

Set the Name of a Cal Kit

SENSe:CORRection:COLLect:CKIT:NAME

Set a description of a Cal Kit

SENSe:CORRection:COLLect:CKIT:DESCription

Get the amount of installed kits

SENSe:CORRection:CKIT:COUNt?

Set the Port Label of a Cal Kit

None

Saves a Cal Kit to a file.

SENSe:CORRection:CKIT:EXPort

 

Modify TRL Cal Kit

Set reference plane

SENSe:CORRection:COLLect:CKIT:TRLoption:RPLane

Set impedance standard

SENSe:CORRection:COLLect:CKIT:TRLoption:IMPedance

Set LRL auto-characterization

SENSe:CORRection:COLLect:CKIT:TRLoption:LRLChar

 

Modify Cal Standards

Select a Cal Standard

SENSe:CORRection:COLLect:CKIT:STANdard

Delete a standard

SENSe:CORRection:COLLect:CKIT:STANdard:REMove

Change description of a standard

SENSe:CORRection:COLLect:CKIT:STANdard:SDEScription

Assign a Class to a Standard

SENSe:CORRection:COLLect:CKIT:ORDer1

Set Standard Type

SENSe:CORRection:COLLect:CKIT:STANdard:TYPE

Add connector family name

SENSe:CORRection:COLLect:CKIT:CONNector:ADD

Delete connector family name

SENSe:CORRection:COLLect:CKIT:CONNector:DELete

List connector family names used in a Cal Kit

SENSe:CORRection:COLLect:CKIT:CONNector:CATalog?

Replace connector family name.

SENSe:CORRection:COLLect:CKIT:CONNector:FNAMe

Assign connector family name to a standard

SENSe:CORRection:COLLect:CKIT:CONNector:SNAMe

Set Delay

SENSe:CORRection:COLLect:CKIT:STANard:DELay

Set Loss

SENSe:CORRection:COLLect:CKIT:STANdard:LOSS

Set Impedance

SENSe:CORRection:COLLect:CKIT:STANdard:IMPedance

Set Max Frequency

SENSe:CORRection:COLLect:CKIT:STANdard:FMAXimum

Set Min Frequency

SENSe:CORRection:COLLect:CKIT:STANdard:FMINimum

Set Label

SENSe:CORRection:COLLect:CKIT:STANdard:LABel

Set Medium (coax | waveguide)

SENSe:CORRection:COLLect:CKIT:STANdard:CHARacter

Set Capacitance (C0 to C3)

SENSe:CORRection:COLLect:CKIT:STANdard:C0

Set Inductance (L0 to L3)

SENSe:CORRection:COLLect:CKIT:STANdard:L0

Set Arbitrary Impedance (TZReal, TZImag)

SENSe:CORRection:COLLect:CKIT:STANdard:TZReal

 

Modify TRL Cal Kit

Set reference plane

SENSe:CORRection:COLLect:CKIT:TRLoption:RPLane

Set impedance standard

SENSe:CORRection:COLLect:CKIT:TRLoption:IMPedance

Set LRL auto-characterization

SENSe:CORRection:COLLect:CKIT:TRLoption:LRLChar

 

 

 

 

 

 

Multiple Power Sensors

 See commands to configure a Power Meter as Receiver (PMAR)

Enable multiple sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple

Add sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:ADD

Assign power sensor name

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:NAME

Remove sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:REMove

Read the number of configured sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:COUNt?

Set start freq

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:FREQuency:STARt

Set stop freq

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:FREQuency:STOP

Set connector type

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:CONNector

Set Cal Kit

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:CKIT

 

Source Power Calibration

Copy Source Power cal to another channel

SYSTem:MACRo:COPY:CHANnel:SOURce

GPIB Power Meter Address

SYSTem:COMMunicate:GPIB:PMETer:ADDRess

Set source power cal method

SOURce:POWer:CORRection:COLLect:ACQ

Turn correction ON|OFF

SOURce:POWer:CORRection

Applies correction values after completing a source power cal acquisition sweep.

Optionally do reference receiver cal.

SOURce:POWer:CORRection:COLLect:SAVE

Returns the currently-selected power sensor channel (A or B) for use at a specific frequency.

None

Set power level

SOURce:POWer:CORRection:LEV

Set power offset

SOURce:POWer:CORRection:OFFSet

Set settling tolerance

SOURce:POWer:CORRection:COLLect:AVERage:NTOLerance

Set max readings for settling

SOURce:POWer:CORRection:COLLect:AVERerage:COUNt

Set accuracy tolerance

SOURce:POWer:CORRection:COLLect:ITERation:NTOLerance

Set max readings for accuracy

SOURce:POWer:CORRection:COLLect:ITERation:COUNt

Turn ON|OFF display of readings

SOURce:POWer:CORRection:COLLect:DISPlay

Acquire receiver-only readings

SOURce:POWer:CORRection:COLLect:ACQuire:REC

Initiates a source power cal acquisition.

SOURce:POWer:CORRection:COLLect:ACQuire

Aborts a source power cal acquisition sweep that is currently in progress.

SOURce:POWer:CORRection:COLLect:ABORt

Launches the Configure Power Sensor dialog on the PNA.

None

Frequency checking (ON|OFF)

SOURce:POWer:CORRection:COLLect:FCHeck

Check test port power

None

Calibrate the source at multiple power levels.

None

Specifies if the source power cal in the calset linked to a measurement cal should be enabled or disabled with that cal

None

Enable/disable use of error messages during a source calibration if calibration fails to achieve desired power level at the power sensor

SOURce:POWer:CORRection:COLLect:WARN

 

Power Meter/Sensor settings

 See commands to configure a Power Meter as Receiver (PMAR)

 See commands to configure multiple power sensors for guided Power Cal

Specifies the type of power sensor to be used

SYSTem:COMMunicate:PSENsor

Specifies the location of the power sensor to be used.

SYSTem:COMMunicate:PSENsor

Returns the ID string of connected USB power meters / sensors.

SYSTem:COMMunicate:USB:PMETer:CATalog?

Pwr meter Max Readings for settling

SOURce:POWer:CORRection:COLLect:AVERerage:COUNt

Pwr meter settling tolerance

SOURce:POWer:CORRection:COLLect:AVERage:NTOLerance

Minimum Frequency

SOURce:POWer:CORRection:COLLect:<>SENsor

Maximum Frequency

SOURce:POWer:CORRection:COLLect:<>SENsor

Power meter channel

None

Set sensor cal factor

SOURce:POWer:CORRection:COLLect:<>SENsor:RCFactor

Set table type

SOURce:POWer:CORRection:COLLect:TABLe <>SENsor

Read/Write cal data

SOURce:POWer:CORRection:DATA

Use Loss table?

SOURce:POWer:CORRection:COLLect:TABLe:LOSS

Cal Factor Table

SOURce:POWer:CORRection:COLLect:TABLe:SELect

Read number of segments in table

SOURce:POWer:CORRection:COLLect:TABLe:POINts?

Segment number

None

Add segment

None

Cal factor of the segment

SOURce:POWer:CORRection:COLLect:TABLe:DATA

Frequency of the segment

SOURce:POWer:CORRection:COLLect:TABLe:FREQuency

Power Loss Table

SOURce:POWer:CORRection:COLLect:TABLe:SELect

Read number of segments in table

SOURce:POWer:CORRection:COLLect:TABLe:POINts?

Segment number

None

Add segment

None

Frequency

SOURce:POWer:CORRection:COLLect:TABLe:FREQuency

Loss value

SOURce:POWer:CORRection:COLLect:TABLe:DATA

Receiver Cal

Set offset from test port power

SENSe:CORRection:RPOWer:OFFSet[:AMPLitude]

Set cal method to receiver cal

SENSe:CORRection:COLLect:METHod RPOWer

Take measurement

SENSe:CORRection:COLLect[:ACQuire] POWer

Turn receiver cal ON | OFF

SENSe:CORRection[:STATe] ON|OFF

Do interpolation

SENSe:CORRection:INTerpolate[:STATe] ON|OFF

 

CalPod

Command used to send other commands as arguments

CONTrol:CALPod:COMMand

Start the CalPod software

Calpod:LAUNch

Assign Calpod serial number to a port.

Calpod:ENABle

Unassign Calpod serial number from a port.

Calpod:Disable

Initialize the selected channel

Calpod:INITialize:ACTive

Initialize ALL channels

Calpod:INITialize:ALL

Recorrect the selected channel

Calpod:Recorrect:ACTive

Recorrect ALL channels

Calpod:Recorrect:ALL

Show refresh dialog

Calpod:SHOW

Hide refresh dialog

Calpod:HIDE

Sets impedance state

Calpod:STATe

Read Calpod temperature

Calpod:TEMP?

 

Custom Cal Window

Turn ON | OFF Custom Cal window.

SENSe:CORRection:COLLect:DISPlay:WINDow

Show NO Custom Cal windows.

SENSe:CORRection:COLLect:DISPlay:WINDow:AOFF

Specify channel to sweep before Cal acquisition.

SENSe:CORRection:COLLect:SWEep:CHANnel

Sweep NO channel before Cal acquisition.

SENSe:CORRection:COLLect:SWEep:CHANnel:AOFF

Preview sweep before remote Cal acquisition.

SENSe:CORRection:COLLect:GUIDed:PACQuire

 

Retrieve and Put Calibration Data

Retrieve Cal Data from the PNA

SENSe:CORRection:CSET:DATA

Put Cal Data in the PNA

SENSe:CORRection:CSET:DATA

 

Automatic Fixture Removal (AFR)

Turns on or off the option "Automatically iterate when ‘Impedance Method Auto’ is checked."

AFR:ADVanced:AUTO:ITERate:METHod:CHECk[:STATe] 

Turns on or off the option "Automatically iterate when Calibration Reference Z0 is set to System Z0 or custom value.

AFR:ADVanced:AUTO:ITERate:REFZ:SET[:STATe] 

Gets or sets the DUT gate coefficient.

AFR:ADVanced:DUTGate:COEFficient

Sets or gets the description of the AFR DUT Gate Domain (single-ended or differential).

AFR:ADVanced:DUTGate:DOMain

Turns ON or OFF the Fitting Thru after AFR DUT Gate.

AFR:ADVanced:DUTGate:ILFitting:MANual[:STATe]

Turns ON or OFF AFR DUTGate

AFR:ADVanced:DUTGate:MANual[:STATe]

Turns ON or OFF AFR DUTGate Only Reflection Option

AFR:ADVanced:DUTGate:REFLection:MANual[:STATe]

Applies advanced algorithm to fixture impedance mismatching cases for better results.

AFR:ADVanced:FIXTure:IMPedance:FTUNe[:STATe]

Turns ON of OFF AFR mode conversion.

AFR:ADVanced:MCONversion[:STATe]

Sets or reads the gating mode in 1-port characterization.

AFR:ADVanced:REFLection:GATing:MODE 
Gets or sets the position parameter in 1-port characterization. AFR:ADVanced:REFLection:GATing:MODE::CUSTom:POSition
Gets or sets the N parameter in 1-port characterization. AFR:ADVanced:REFLection:GATing:MODE:MINimum:NVALue
Gets or sets the spike tolerance parameter in 1-port characterization. AFR:ADVanced:REFLection:GATing:SPIKe:TOLerance
Gets or sets the ratio of the merge center for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:MCENter
Gets or sets the ratio of the merge span for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:MSPan
Gets or sets the start ratio for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:STARt
Gets or sets the stop ratio for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:STOP
Gets or sets the ratio of the merge center for IL fitting at low frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:LOW:MCENter 

Gets or sets the ratio of the merge span for IL fitting at low frequency range 1-port characterization.

AFR:ADVanced:REFLection:ILFitting:LOW:MSPan
Gets or sets the start ratio for IL fitting at low frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:LOW:STARt

Gets or sets the stop ratio for IL fitting at low frequency range 1-port characterization.

AFR:ADVanced:REFLection:ILFitting:LOW:STOP

Resets the AFR configuration.

AFR:ADVanced:RESet

Gets or sets the manual start time in AFR configuration.

AFR:ADVanced:TIME:STARt

Gets or sets the manual stop time in AFR configuration.

AFR:ADVanced:TIME:STOP

Gets the AFR Version. AFR:ADVanced:VERSion?

Gets or sets the manual window type in AFR configuration.

AFR:ADVanced:WINDow:COEFficient

Turns ON of OFF the manual window coefficient of the AFR.

AFR:ADVanced:WINDow:MANual[:STATe]

Selects whether the fixture is band limited or not.

AFR:FIXTure:BLIMited[:STATe]

Selects whether to use DUT correction or not when the characterization fixture is not equal to the DUT measurement fixture.

AFR:FIXTure:CDUT[:STATe]

Selects Fixture Length A not equal to B correction.

AFR:FIXTure:CLENgth[:STATe]

Selects Fixture Match A not equal to B correction.

AFR:FIXTure:CMATch[:STATe]

Describes the fixture inputs (single ended or differential).

AFR:FIXTure:INPuts

Selects the number of fixtures to be characterized.

AFR:FIXTure:MEASurement

Refreshes preview data.

AFR:FIXTure:PREView

Reads the impedance profile of the calculated fixture model.

AFR:FIXTure:PREView:DATA[:IMPedance]?

Reads the impedance profile of the calculated fixture model at a specified position.

AFR:FIXTure:PREView:DATA[:IMPedance]:MARKer:Y?

Chooses the calibration reference Z0 after fixture removal.

AFR:FIXTure:REFZ

Sets "System Z0" to Calibration Reference Z0.

AFR:FIXTure:SET:SYSZ[:STATe]

Specifies whether thrus are used in case of multi-port fixtures.

AFR:FIXTure:USE:THRUs[:STATe]

Restores the default AFR settings.

AFR:INITialize

Specifies the file paths of saved fixture data.

AFR:SAVE:FILename

Specifies whether the port impedances are normalized in saving the AFR fixture files.

AFR:SAVE:IMPedance:NORMalize[:STATe]

Assigns the ports for saved fixture data in several formats.

AFR:SAVE:PORTs

Sets the file type to save fixture data.

AFR:SAVE:TYPE

Selects all OPEN standards.

AFR:STANdard:ALLOpen[:STATe]

Selects all SHORT standards.

AFR:STANdard:ALLShort[:STATe]

Reads the impedance profile of the measured standard.

AFR:STANdard:DATA[:IMPedance]?

Reads the impedance of the measured standard at a specified position.

AFR:STANdard:DATA[:IMPedance]:MARKer:Y?

Sets the fixture length for the selected fixture (for 1X AFR only).

AFR:STANdard:EDIT:FLENgth

Sets the gate position for the selected fixture.

AFR:STANdard:EDIT:GATE

Sets the impedance for the selected term.

AFR:STANdard:EDIT:IMPedance

Sets the impedance method.

AFR:STANdard:EDIT:IMPedance:METHod

Loads the calibration standards data from a file.

AFR:STANdard:LOAD

Measures calibration standard.

AFR:STANdard:MEASure

Specifies fixture thru settings.

AFR:STANdard:THRU

Chooses the calibration standards.

AFR:STANdard:USE

 

Cal Update

Sets and returns the averaging used to improve noise errors.

SYSTem:CALibrate:CALupdate:AVERage:COUNt

None

Sets and returns the IF bandwidth used by the measurement channel.

SYSTem:CALibrate:CALupdate:BWIDth[:RESolution]

None

Selects the channel(s) to calibrate.

SYSTem:CALibrate:CALupdate:CHANnel[:SELect]

None

Sets and returns the gate start value for time domain gating.

SYSTem:CALibrate:CALupdate:GATE:STARt

None

Sets and returns the state of gate coupling for gate start value.

SYSTem:CALibrate:CALupdate:GATE:STARt:COUPle[:STATe]

None

Sets and returns the gate stop value for time domain gating.

SYSTem:CALibrate:CALupdate:GATE:STOP

None

Sets and returns the state of gate coupling for gate stop value.

SYSTem:CALibrate:CALupdate:GATE:STOP:COUPle[:STATe]

None

Initializes the selected ports.

SYSTem:CALibrate:CALupdate:INITialize

None

Recorrects the list of previously initialized ports.

SYSTem:CALibrate:CALupdate:RECorrect

None

Sets and returns the reference cal set name.

SYSTem:CALibrate:CALupdate:REFerence

None

Selects the port numbers to initialize.

SYSTem:CALibrate:CALupdate:PORTs[:SELect]

None

Use a channel's existing IF BW, Averaging, and Power value settings or enter the values manually.

SYSTem:CALibrate:CALupdate:SETTings:AUTO

None

Manually sets and returns the source power for the active measurement channel.

SYSTem:CALibrate:CALupdate:SOURce:POWer

None