Listing of Commands

Last Updated: August 29, 2007

This topic lists all of the available SCPI commands in the E6890A General Purpose Application.

It is recommended that you print this topic because it provides a useful syntax reference for all of the available General Purpose Application commands. To print:

The SCPI commands in this topic are categorized by subsystem:

ABORt Subsystem

CALCulate Subsystem

DISPlay Subsystem

FETCh Subsystem

INITiate Subsystem

RFANalyzer Subsystem

RFGenerator Subsystem

SETup Subsystem

 

Related Topics