Last Updated: August 29, 2007
The Adjustment Software is used to restore the test set to Agilent Technologies factory specifications after a repair or upgrade.
Full (recommended)
RF Generator 2 (if installed)
|
|
Do not make any setting changes to the test set while performing Adjustments. Remove all RF power from the RF IN/OUT and RF OUT ONLY connectors on the front panel before performing Alignments. |
RF Generator Alignment and Full Alignment are included when a Full Adjustment is performed. A Full Alignment is a subset of an Adjustment.

Adjustment is intended be performed to restore factory specifications after a repair. The test set may need to be adjusted to pass the Performance Tests. Adjustments must be performed after a hardware upgrade or a after swapping a module as part of a repair.
This parameter sets the type of adjustment procedure to run.
SCPI command: SYSTem:TOOLs:ADJustment:PROCedure[?]
This parameter sets the level of messages reported during an adjustment procedure.
SCPI command: SYSTem:TOOLs:ADJustment:VERBose[?]
Select Run to start the currently selected adjustment procedure.
SCPI command: SYSTem:TOOLs:ADJustment[:IMMediate]
By selecting the Full Adjustment all of the adjustments listed below are performed as well as some additional adjustments not available separately.
|
|
Full Adjustment is the recommended choice when selecting an Adjustment. |
A Full Adjustment takes about 20 minutes.
SCPI command: SYSTem:TOOLs:ADJustment:FULL:LAST[:DTIMe]?
This adjustment is included in the Full Adjustment. RF Generator 1 and 2 are adjusted independently of each other. The IQ, level accuracy, gain and the VCO tune voltage for the Upconverter are adjusted when RF Generator Adjustment is selected. The accuracy of the step attenuator is restored with RF Generator Adjustment. IQ Adjustment calibrates the IQ modulated signals from the Upconverter.
This adjustment is included in the Full Adjustment. RF Analyzer Adjustment calibrates the Downcoverter module including Channel Power Calibration.
|
Adjustment |
Why |
After 30 Minute Warm-up |
After 48 Hour Warm-up |
Ambient Temperature Requirement |
|
Full Adjustment |
Restore factory specifications |
Channel Power specification (± 0.7 dBm) |
Channel Power specification (± 0.6 dBm) |
+25 degrees C ± 5 degrees |