Last Updated: August 29, 2007
These commands are only applicable with an IQ Capture license.
These commands return results for the IQ Capture measurement in the RF Channel (RFCH) measurement suite.
Queries the RF Channel measurement suite integrity indicator, the IQ sample period, the number of samples, and either the magnitude/phase or real/imaginary results. The format of the results depends on the setting of SETup:RFCHannel:IQCapture:FORMat[?].
For polar measurements the magnitude results are unit-less, and the phase results are in degrees.
For rectangular measurements the results are unit-less.
No averaging is available for this measurement. If FETCh:RFCHannel:ICOunt? is set to a value greater than 1, then the results returned are those of the last measurement.
Query Range:
RF Channel measurement suite integrity indicator: See Measurement Integrity Indicator.
IQ sample period: <nr3> in seconds and 9.91 E+37 (NAN)
IQ number of samples: <nr1>
IQ samples: These values are returned as a comma separated list in the range of <nr3> and 9.91 E+37 (NAN). The results are either magnitude/phase or real/imaginary, for example:
<nr3>[0] (Magnitude),<nr3>[0] (Phase) {, <nr3> [1], <nr3> [1], ¼<nr3>[n], <nr3>[n] }
<nr3>[0] (Real),<nr3>[0] (Imaginary) {, <nr3> [1], <nr3> [1], ¼<nr3>[n], <nr3>[n] }
Test Set Requirements: E6601A WCTS Program Version A.05 and above
Example:
' Query the IQ capture measurement results.
TestSet.WriteString("FETCh:RFCHannel:IQCapture:TRACe?")
Queries the RF Channel measurement suite integrity indicator, the IQ sample period, and the number of either magnitude/phase or real/imaginary results. The format of the results depends on the setting of SETup:RFCHannel:IQCapture:FORMat[?].
Query Range:
RF Channel measurement suite integrity indicator: See Measurement Integrity Indicator.
IQ sample period: <nr3> in seconds and 9.91 E+37 (NAN)
IQ number of samples: <nr1>
Test Set Requirements: E6601A WCTS Program Version A.05 and above
Example:
' Query the number of IQ capture measurement results.
TestSet.WriteString("FETCh:RFCHannel:IQCapture:TRACe:PARameters?")