Last Updated: August 29, 2007
The RF Analyzer tab on the RF Control window provides access to the RF Analyzer (receiver) parameters.
This parameter sets the RF analyzer frequency control mode, either Auto or Manual. When set to Manual, you can specify the RF analyzer frequency.
SCPI command: RFANalyzer:CONTrol:FREQuency:AUTO:TCALibration[?]
This parameter sets the DPCH Channel number. This setting only applies when the Control Mode is Auto.
SCPI command: TRANsceiver:CHANnel:TCALibration[?]
This parameter sets the manual mode, either Manual UL Channel or Manual UL Frequency. This setting only applies when the Control Mode is Manual.
SCPI command: RFANalyzer:CONTrol:FREQuency:MANual:TCALibration[?]
This parameter sets the manual frequency of the RF analyzer. This setting only applies when the Control Mode is Manual and Manual Mode is Frequency.
SCPI command: RFANalyzer:MANual:FREQuency:TCALibration[?]
This parameter sets the UTRA UL manual channel. This setting only applies when the Control Mode is Manual and Manual Mode is Channel.
SCPI command: RFANalyzer:MANual:CHANnel:TCALibration[?]
This parameter sets the power level in dBm that the test set's RF analyzer is expecting the wireless device burst to transmit at.
SCPI command: RFANalyzer:MANual:POWer[:AMPLitude]:BURSt[1]:TCALibration[?]
This parameter sets the DPCH channel type.
SCPI command: RFANalyzer:CHANnel:UPLink:DPCHannel:TYPE[?]
This parameter sets the DPCH Basic Midamble Code.
SCPI command: RFANalyzer:UPLink:DPCHannel:MIDamble[:BASic][?]
This parameter sets the DPCH Max Midamble Shift. This setting will affect the Midamble Offset.
SCPI command: RFANalyzer:UPLink:DPCHannel:MIDamble:SHIFt:MAXimum[?]
This parameter sets the DPCH Midamble Shift Index. This setting will affect the Midamble Offset.
SCPI command: RFANalyzer:UPLink:DPCHannel:MIDamble:SHIFt[:INDex][?]
This parameter represents the chip offset from the basic midamble and it is read only.
SCPI command: RFANalyzer:UPLink:DPCHannel:MIDamble:OFFSet?