TRANsceiver

Last Updated: August 29, 2007

This command sets up channels for the TD-SCDMA Cal Application.

For more information on the conventions used in the programming examples click here.

TRANsceiver:CHANnel:TCALibration[?]

Sets the DPCH channel number. This setting applies to both DPCH Channel of RF Generator when Control Mode of RF Generator is Auto and DPCH Channel of RF Analyzer when Control Mode of RF Analyzer is Auto.

Setting Range:

*RST Setting: 10087

Test Set Requirements: E6601A WCTS Program Version A.05 and above

Example:

' Set the DPCH channel number to 10087.

TestSet.WriteString("TRANsceiver:CHANnel:TCALibration 10087")