Mean Power (MPOW) Measurement Description

Last Updated: August 29, 2007

This topic describes the Mean Power measurement. Mean Power is a measurement in the Dedicated Physical Channel measurement suite.

How is a Mean Power Measurement Made?

The Mean Power is the average power measured in a bandwidth of at least (1+a) times the chip rate. The period of the measurement is 1 timeslot. This measurement is only intended to measure the power of the W-CDMA modulated carrier, which in theory is 100% contained in this bandwidth. The 3GPP definition of Mean Power is located in TS 34.121 section 3.1.

Mean Power Measurement Parameters

Mean Power is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Measurement Suite Measurement Parameters for details of the parameters that apply to measurements in the suite.

Mean Power Measurement Limits

Mean Power is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Measurement Suite Measurement Limits for details of the limits parameters that apply to measurements in the suite.

Mean Power Measurement Results

Integrity Indicator

This result provides the integrity indicator for the Dedicated Physical Channel measurement suite. Normal indicates that the measurement suite completed successfully without error and the result is accurate. For details of other integrity indicators, see Measurement Integrity Indicator.

SCPI command: FETCh:WDPChannel:INTegrity?

Mean Power Pass/Fail

This result provides the overall pass/fail result for the Mean Power measurement.

SCPI commands: FETCh:WDPChannel:MPOWer[:PARTial]?, FETCh:WDPChannel:MPOWer:ALL?

Mean Power Result

This result provides the measured mean power. If the Multi-Measurement Count is on, then the intermediate count is displayed in the lower-left area of the window and the Maximum, Minimum, and Standard Deviation (Std Dev) are displayed in the Mean Power results window.

SCPI commands:FETCh:WDPChannel:MPOWer:ALL?, FETCh:WDPChannel:MPOWer[:PARTial]?

Mean Power Input Signal Requirements

Adjacent Channel Leakage Ratio is a measurement in the Dedicated Physical Channel measurement suite. See Dedicated Physical Channel Input Signal Requirements for details of the input signal requirements that apply to all measurements in the suite.   

 

Related Topics