RF Analyzer

Last Updated: August 29, 2007

The RF Analyzer tab on the RF Control window provides access to the RF Analyzer (receiver) parameters.

Control Mode

This parameter sets the RF analyzer frequency control mode, either Auto or Manual. When set to Manual, you can specify the RF analyzer Frequency or Uplink Channel, depending on the Manual Mode setting.

SCPI command: RFANalyzer:CONTrol:FREQuency:AUTO:WCALibration[?]

Uplink Channel Separation

This parameter sets the UTRA FDD uplink separation. See Uplink Channel UARFCN for details on which uplink channels and frequencies the test set supports. This parameter only applies when the Control Mode is set to Auto.

SCPI command: TRANsceiver:CHANnel:UPLink:SEParation:FDD[?]

Manual Mode

This parameter sets the manual mode, either Channel or Frequency.

SCPI command: RFANalyzer:CONTrol:FREQuency:MANual:WCALibration[?]

Frequency

This parameter sets the manual frequency of the RF analyzer. See Uplink Channel UARFCN for details on which uplink channels and frequencies the test set supports. This parameter only applies when the Control Mode is set to Manual and the Manual Mode is set to Frequency.

SCPI command: RFANalyzer:MANual:FREQuency:WCALibration[?]   

Uplink Channel

This parameter sets the UTRA FDD UL channel. See Uplink Channel UARFCN for details on which uplink channels and frequencies the test set supports. This parameter only applies when the Control Mode is set to Manual and the Manual Mode is set to Channel.

SCPI command: RFANalyzer:MANual:CHANnel:WCALibration[?]  

Expected Power

This parameter sets the power level in dBm that the test set's RF analyzer is expecting the wireless device burst to transmit at.

SCPI command: RFANalyzer:MANual:POWer[:AMPLitude]:WCALibration[?]

DPCH Scrambling Code

This parameter sets the UTRA FDD UL DPCH scrambling code.   

SCPI command: RFANalyzer:UPLink:DPCHannel:SCODe[?]

DPCH Channel Type

This parameter sets the DPCH channel type.

SCPI command: RFANalyzer:CHANnel:UPLink:DPCHannel:TYPE[?]

 

Related Topics