Specifies the settings to remotely control the rear panel connectors, an external test set, and ECal Module state.
|
CONTrol CHANnel:INTerface:CONTrol | [STATe] ECAL:MODule | PATH | COUNt? | STATe MULTiplexer | OUTPut |
Click on a Red keyword to view the command details.
See Also
See a pinout and detailed description of the rear panel connectors:
External Test Set IO connector
Material Handler IO connector
Applicable Models: E5080A
|
(Write-only) Recalls an Interface Control configuration file. Learn more about Interface Control. |
|
|
Parameters |
|
|
<string> |
File name and extension (.xml) of the configuration file to recall. Files are typically stored in the default folder "D:\". To recall from a different folder, specify the full path name. |
|
Examples |
CONT:CHAN:INT:CONT:CONF:REC 'MyFile.xml' control:channel:interface:control:config:recall:state 'D:\MyFile01.xml' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
Applicable Models: E5080A
|
(Read-Write) Enables and disables ALL Interface Control settings. To send data, the individual interfaces must also be enabled. Learn more about Interface Control. |
|
|
Parameters |
|
|
<bool> |
OFF or 0 - Interface Control is disabled; NO control data is sent. ON or 1 - Interface Control is enabled. |
|
Examples |
CONT:CHAN:INT:CONT 1 control:channel:interface:control:state 0 |
|
Query Syntax |
CONTrol:CHANnel:INTerface:CONTrol[:STATe]? |
|
Return Type |
Boolean |
|
OFF or 0 |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Returns the number of unique states that exist for the specified path name on the selected ECal module. This command performs exactly the same function as SENS:CORR:CKIT:ECAL:PATH:COUNt? Use the CONT:ECAL:MOD:PATH:STAT command to set the module into one of those states. Use SENS:CORR:CKIT:ECAL:PATH:DATA? to read the data for a state. |
|
|
Parameters |
|
|
<num> |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
|
<name> |
Name of the path for which to read number of states. Choose from: Reflection paths
Transmission paths
Note: For each transmission path, the first of the available states is the through state, the second is the confidence (attenuator) state. |
|
Examples |
CONT:ECAL:MOD:PATH:COUNt? A control:ecal:module2:path:count? cd See example program |
|
Return Type |
Integer |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Write-only) Sets the internal state of the selected ECAL module. This command supersedes CONT:ECAL:MOD:STAT.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Parameters |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<num> |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<path> |
Path name for which to set a state. Note: The impedance paths are not independent. For example, changing the impedance presented on path A will cause a change to the impedance on path B. Choose from: Reflection paths
Transmission paths
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<stateNum> |
Number of the state to set. Refer to the following table to associate the <stateNum> with a state in your ECal module. In addition, CONT:ECAL:MOD:PATH:COUNt? returns the number of states in the specified ECal module.
** The following modules have only FOUR Impedance states (1, 2, 3, 4): N4690B ,N4691B ,N4692A ,N4696B. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Examples |
CONT:ECAL:MOD:PATH:STATe A,5 control:ecal:module2:state BC,1 See example program |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Query Syntax |
Not Applicable |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Not Applicable |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Applicable Models: E5080A
|
(Read-Write) Sets or returns the output port data for specified group with id of the E5092A multiport test set. Notes: This command is available only for E5092A multiport test set. |
|||||||||||||||||||
|
Parameters |
|
||||||||||||||||||
|
<id> |
Id of the multiport test set either 1 or 2. If unspecified, Id is assumed to be 1. |
||||||||||||||||||
|
<grp> |
A | B | C | D |
||||||||||||||||||
|
<num> |
An integer specifying the decimal value of the control line. Values are obtained by adding weights from the following table that correspond to individual lines. The output port data range is between 0 to 255 (0=All line are turns OFF and 255 all lines are turn ON).
|
||||||||||||||||||
|
Examples |
CONT:MULT1:OUTP:B 8 |
||||||||||||||||||
|
Query Syntax |
CONTrol:MULTiplexer<id>:OUTPut:<grp>[:DATa]? |
||||||||||||||||||
|
Return Type |
Numeric |
||||||||||||||||||
|
0 |
|||||||||||||||||||
Applicable Models: E5080A
|
(Read-Write) Sets or returns the output voltage for specified group with id of the E5092A multiport test set. Notes: This command is available only for E5092A multiport test set. |
|
|
Parameters |
|
|
<id> |
Id of the multiport test set either 1 or 2. If unspecified, Id is assumed to be 1. |
|
<grp> |
A | B | C | D |
|
<volt> |
Output voltage range for <grp> is between 0 to 5.2V and resolution is 10mV. |
|
Examples |
CONT:MULT1:OUTP:B:VOLT 4.2 |
|
Query Syntax |
CONTrol:MULTiplexer<id>:OUTPut:<grp>:VOLtage[:DATa]? |
|
Return Type |
Numeric |
|
0 V |
|
Last Modified:
|
18-May-2016 |
First Release |
![]()