Controls output functions: RF power and Noise Source.
|
OUTPut: |
Click on a Red keyword to view the command details.
See Also
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns RF power from the source ON or OFF. See note about source power state with instrument state save and recall. |
|
|
Parameters |
|
|
<bool> |
ON (or 1) - turns RF power ON OFF (or 0) - turns RF power OFF |
|
Examples |
OUTP ON |
|
Query Syntax |
OUTPut[:STATe]? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
ON |
|
Last modified:
|
18-May-2016 |
First Release |