Power level is the power of the VNA source at the test ports.
See other 'Setup Measurements' topics
The test port output power is specified over frequency.
How to make Power settings |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|

|
Basic control of VNA source power for a specific port. See advanced control of source power and attenuation. Power On (All Channels) - also same function as RF Power. Check to enable source power for all channels. Only turns power ON if channel power setting is ON or Auto. See Advanced Power. Port 'n' - Active source port for which power is being set. Port Power - Sets the power level for the specified port.
Start/Stop Power - Set the start and stop power values of a power sweep.
Power Slope - Helps compensate for cable and test fixture power losses at increased frequency. Slope - Select to set the power slope. Clear to set power slope OFF. |
How to make Power and Attenuators settings |
|
Using Hardkey/SoftTab/Softkey |
|
|
Details setting for Power and Attenuators
|

|
Defines and controls the VNA source power and attenuation for the active channel. External sources can be controlled from this dialog. Learn more.
Power On (All Channels) - also same function as RF Power. Check to enable source power for all channels. Only turns power ON if channel power setting is ON or Auto.
Name - Lists the VNA test ports. State
Port Power - Sets the power level at the output of the source.
Start/Stop Power - Available ONLY when sweep type is set to Power Sweep. Set the start and stop power values of a power sweep. Learn more about Power Sweep.
Leveling Mode (ALC Hardware in Softkey)
Channel Power Slope - Helps compensate for cable and test fixture power losses at increased frequency. With power slope enabled, the port output power increases (enter positive value) or decreases (enter negative value) as the sweep frequency increases. Slope - Select to set the power slope. Clear to set power slope OFF. Power slope is computed and applied from 0 GHz – not from the measurement start frequency. For example, with the following measurement settings:
The power into the DUT from 1 GHz to 2 GHz is 1 dBm sloping to 2 dBm. Offset and Limits - Launches the Power Offset and Limits dialog. Receiver Leveling - Launches the Receiver Leveling dialog. Receiver Attenuator - Launches the Receiver Attenuator dialog. |
When the power level that is required at a test port is higher than the VNA can supply, a Source Unleveled error message appears on the screen and the letters LVL appear on the status bar
To resolve an unleveled condition, change either the Test Port Power . If an Unleveled condition exists within the specified power range, contact Technical Support. To set report source unleveled events as errors, please refer enable the preferences dialog.
Important Note: The available power range can also be adjusted AUTOMATICALLY by a Source Power Calibration, Guided Power Cal, or Power Compensation. If you are NOT seeing the range that you expect, or the correct power level at your DUT, view the Power Offset column in the Power Limits and Offsets dialog.
|
Receiver Attenuation is used to protect the VNA test port receivers from damage or compression. Attenuator level can be set either 0 dB or 35 dB for each receiver attenuator per channel. This setting is valid when segment sweep mode is not selected. When the segment sweep mode is selected, the setting in the segment is applied. Test attenuator and reference attenuator can be set independently. CAUTION! You can damage the analyzer receivers if the power levels exceed the maximum values.
|
Last modified:
|
18-May-2016 |
First Release |
![]()