The
Hardware options include up to six baseband cards and up to four I/O cards.
Each baseband card has two DSP units that can be used in any combination for baseband generation and/or fading. With the split fading firmware option (N5106A-169), the number of DSP units can be extended for larger MIMO configurations (e.g., 4x4 MIMO and 2x8 MIMO).
Each I/O card has two I/O ports that can be used for analog I/Q output or digital I/Q input or output to/from supported instruments.
Licensed firmware options include: baseband generation, fading for SISO and MIMO channels, split fading for large MIMO configurations (e.g., 4x4 MIMO and 2x8 MIMO), MIMO channel models with standard or custom settings, and AWGN. Licenses for these options enable the respective functionality on all installed licensed hardware.
All ordered licenses for DSP units and firmware options are installed at the time of purchase; however, if you want to add hardware or firmware licenses at another time, you will need to follow the steps below.
|
|
PXB firmware version 1.9 and later includes Revision to Current (R2C) licensing. Under R2C licensing, new features and enhancements are enabled on the instrument with a purchased and installed N5106AK-R2C upgrade license. Bug fixes are not considered enhancements and do not require an R2C license. See the Release Notes or www.agilent.com/find/N5106AK-R2C for more information. |
Step 1
-
Step 2 - Receive the Entitlement Certificate
Step 3 - Redeem the License
Step 4 - Install the License