2. Basic
The following figure is a composite of all supported instruments, so some parameters may not apply to your instrument.
Frequency
Range: for specified range values, see the signal generator's data sheet
Enter a value to set the signal generator’s output frequency. Use abbreviations for faster entry (example: 1g = 1.000000000000 GHz).
Amplitude
ESG, PSG, EXT, EXG, or MXG
Range: for amplitude range values, see the signal generator's data sheet
Enter a value to set the signal generator’s output amplitude in dBm.
RF Output
Double-click or use the drop-down menu to control the signal generator’s RF output state.