5. Dual ARB
The following figure is a composite of all supported instruments, so some parameters may not apply to your instrument.
5. Dual ARB: Baseband Frequency Offset (EXT)
ARB Sample Clock
Range: 1 kHz to 125 MHz
Default: 100 MHz
The sample clock frequency of the signal generator is automatically calculated by the program (read-only). The range depends on the connected instrument.
VCO Clock
Choice: Internal | External
Default: Internal
Double-click or use the drop-down menu to select the signal generator’s VCO Clock.
-
Internal - the signal generator uses its internal VCO Clock.
-
External - the signal generator uses an external VCO Clock.
VCO Clock is enabled with E4438C-HEC and E8267D only.
Waveform Runtime Scaling
Range: 1%−100%
Default: 90%
Enter a scaling value for the signal generator to apply to the waveform while it is playing. Use scaling to get the best dynamic range without overflowing the I and Q digital-to-analog converters (DAC) and reduce the overshoot associated with the DAC interpolation filter.
I/Q Modulation Filter
Choice: Auto | 2.1 MHz | 40 MHz | Through
Default: Auto
Double-click or use the drop-down menu to select a filter for I/Q signals modulated onto the RF carrier. The bandwidth of the baseband signal should dictate the minimum reconstruction filter bandwidth you choose. Depending on the oversampling ratio and where the image frequencies appear, you may want to select a wider bandwidth.
-
Auto − automatically selects a digital modulation filter.
-
2.1 MHz − applies a 2.1 MHz baseband filter to the I/Q signals.
-
40 MHz − applies a 40 MHz baseband filter to the I/Q signals.
-
Through − bypasses filtering.
This parameter is not available with all instrument model numbers and may be grayed out.
I/Q Output Filter
Choice: Auto | 40 MHz | Through
Default: Auto
Double-click or use the drop-down menu to select a filter or through path for routing I and Q signals to the rear panel I/Q outputs.
-
Auto − automatically selects an I/Q output filter.
-
40 MHz − applies a 40 MHz baseband filter.
-
Through − bypasses filtering.
This parameter is not available with all instrument model numbers and may be grayed out.
Modulation Attenuation Mode
Choice: Auto | Manual
Default: Auto
Select the mode of the internal I/Q modulator.
-
Manual − manually set the attenuation level of the I/Q modulator using the Modulation Atten cell.
-
Auto − automatically sets the attenuation level to a value that provides the best performance, based on the digital modulation settings.
Modulation Attenuation
Range: 0.00−40.00 dB
Default: 6.00 dB
Set the attenuation of the I/Q signals being modulated through the signal generator RF path. Adjusting the attenuation may reduce signal distortion and improve the overall dynamic range.
Set to to enable this parameter.
High Crest Mode
Choice: On | Off
Default: Off
Double-click or use the drop-down menu to enable or disable the signal generator’s high crest mode.
-
On − processes high-crest-factor arbitrary I/Q waveforms with less distortion. For crest factors higher than 4 dB, you should reduce I/Q Modulation Attenuation levels by 1 dB for each dB above that level. High Crest Mode reduces the maximum output level and degrades power level accuracy.
-
Off − disables the high crest mode.
This parameter is not available with all instrument model numbers and may be grayed out.
ARB Reference
Choice: Internal | External
Default: Internal
Double-click or use the drop-down menu to select the signal generator’s ARB Reference source .
-
Internal − the signal generator uses its internally generated 10 MHz signal as the reference source.
-
External − the signal generator uses an external signal as the reference frequency for the baseband I/Q signal. See the signal generator’s user’s guide for information on external references.
This parameter is not available with all instrument model numbers and may be grayed out.
Reference Frequency
Range: 0.2500000–100.0000000 MHz
Default: 10.0000000 MHz
Enter the frequency value of the external reference when using an externally supplied reference signal. See the signal generator’s user’s guide for information on external references.
Set to to enable this parameter.
This parameter is not available with all instrument model numbers and may be grayed out.
Baseband Frequency Offset (EXT)
Range: -50.00 MHz to 50.00 MHz
Default: 0.000 Hz
Set to to enable this parameter.
Enter a frequency value by which the baseband frequency is offset relative to the carrier. This parameter is only available when connected to the E6607 EXT.