These settings control the Multiple PRACH message functionality. These settings are only active when the PRACH Generation Mode is set to Multiple in the PXB's PRACH node.
See also PRACH (General Settings) tab,
PRACH Structure tab, and to Message.
|
Parameter |
Description |
|---|---|
|
UE |
UE number that is assigned to a PRACH. Up to eight UEs are configurable at one time. |
|
ON/OFF |
Indicates whether the UEn is enabled or disabled for multi-PRACH data generation. See :PRACH:MULTi:UE[:STATe]. |
|
Pre Sig |
Indicates the preamble signature of the PRACH preamble. This is same value as the signal PRACH mode. Range: 0 to 15. See :PRACh:MULTi:UE:PREamble:SIGNature. |
|
Ch Code: Ctl |
Indicates the channel code of the message control part. This value is calculated by the preamble signature (Pre Sig) of the related UEn setting. See :PRACh:MULTi:UE:CPARt:CCODe and see :PRACh:MULTi:UE:DPARt:CCODe. |
|
Ch Code: Dat |
Indicates the channel code of the message data part. This value is calculated by the preamble signature (Pre Sig) of the related UEn setting. |
|
Start Access Slot Positions in 80 ms Period (0 to 7) |
Indicates the PRACH start position in access slot number. Range: 0 to 59, OFF. The start position can be set at 8 locations maximally. The configured pattern is repeated every 80 ms. See :PRACH:MULTi:UE[:ASLot]. |