The following illustration shows the Menu bar and the Toolbar for the N7601B Signal Studio for cdma2000/1xEV-DO software.
Select a command from the displayed menus for a description of the command.
Select an icon from the toolbar for a description of the icon's command.
Sets the software to its initial state (one IS95A Forward link carrier
configured with the 9 Ch Forward configuration) using the current hardware configuration. The window name changes
to
Untitled.
Rename and save the new setup as a settings (.scp)
file (saving only the software parameters), or as a Quick Setup (saving the current hardware and
software parameters).
You must save the current software parameter settings before selecting New to prevent the loss of data.

Opens a saved settings (.scp) file. Opening a settings file configures only the waveform data parameters for use with the currently selected hardware. To use a settings file with a different hardware configuration, select Change Hardware Connections, or Run System Configuration Wizard to configure new hardware.
Use Quick Setup to open a saved settings file that includes the hardware connection and software settings.
Saves only waveform data settings to a specified settings (.scp) file. Settings files do not contain the hardware configuration data. To save a settings file with a specific hardware configuration, select Change Hardware Connections, or Run System Configuration Wizard to configure new hardware. When a file is saved it is added to the top of the Most Recently Used Files list.
Use Quick Setup to save the current hardware configuration with your waveform setup.
When using Windows Vista operating system, saved settings files (*.scp) are not shared between different users of the same PC unless saved to a common location accessible to all users.
Saves an encrypted waveform file (with a .wfm extension) to your PC. This waveform file can then be downloaded and played in other licensed signal generators or ADS design libraries. If a waveform is configured, but has not been generated, this selection also generates the waveform.
Displays the four most recent settings files that were either opened with Open... or saved with Save As.... The settings file used most recently is added to the top of the list. Deleting a settings file does not immediately remove it from the list. Selecting a deleted settings file displays an error then removes the file from the list.
Stops and closes the software. If you made any waveform setup changes,
a
dialog box
is displayed asking if you want to save the changes as a quick setup before
exiting. The
close button
performs the same function.
To save any hardware parameter changes, you must use the Save As Quick Setup button. You are not prompted to save Hardware parameter changes when closing or exiting the software unless changes are also made to the Waveform Setup parameters.

Enables you to generate a waveform. This allows you to check for waveform errors before downloading or exporting the waveform.

Enables you to generate and download a waveform to the hardware.
When a power-sensitive DUT is connected to the signal generator, ensure that the RF power is off before downloading a waveform.
Sends the current signal generator configuration to the appropriate instrument. If the configuration is not received by the instrument, an error message describing the problem appears.
Displays a list of saved hardware connections. This menu choice opens
Step 2 of the System Configuration Wizard,
where you can select a previously saved hardware configuration, or configure
and save a new hardware setup.
Enables you to configure your system component connections and save
the hardware configuration for later use. Use
Run System Configuration Wizard
to set up a new signal generator connection, or use Quick Setup to save and change between complete
setups that include the hardware connection and software settings.
Enables you to turn the Status Window on or off.
Allows you select whether to display the
Run System
Configuration Wizard
when the software is started.
Opens the Help system and displays the table of contents.
Opens the Help system and displays the Index utility.
Opens the Help system and displays the search utility.
Go to the Keysight Signal Studio Website
http://www.keysight.com/find/signalstudio
Displays the version and release date of the software.