This topic provides a comprehensive listing of the Data node settings for all of the timeslots with and without channel coding except for the combined and non-combined BCH. For the combined and non-combined BCH Data node settings, see the Data BCH topic.
Use the following links to navigate to and view figures and available settings:
|
|
||
|
|
|
|
|
|
|
|
|
|
||
|
|
||
|
|
||
|
|
||
|
|
||
|
|
||
|
|
||
|
|
||
|
|
||
|
|
|
|
|
|
|
|
|
|
|
|
|
Click the |
|
|
Click the button to hide the structure (graph). After clicking this button, the button name changes to . |
Timeslot Type = Custom GMSK, Custom 8PSK
Choices: PN9 | PN11 | PN15 | PN20 | PN23 | EXT | Custom Bit Pattern | User File
Default: PN9
Edit the data by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
The Custom GMSK timeslot uses 148 data bits and 8 guard period bits, and the Custom 8PSK timeslot uses 444 data bits and 24 guard period bits.
Timeslot Type = Normal GMSK, Frequency Correction, Synchronization, Dummy, Access
Channel Coding Type = Normal GMSK: Coded TCH/FS, Coded TCH/HS, Coded CS-1, Coded CS-4, Coded DL MCS-1, Coded UL MCS-1
Displays the tail bits set by the software in accordance with the 3GPP standards.
The Access timeslot uses 3-bits and the other timeslots use 3+3 bits.
Timeslot Type = Normal 8PSK
Channel Coding Type = Normal 8PSK: Coded DL MCS-5, Coded UL MCS-5, Coded DL MCS-9, Coded UL MCS-9, Coded E-TCH/F43.2, Uncoded
Default: 1FF
Use the timeslot with or without the listed channel coding. Edit the tail bits by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
If more bits are entered than the required number of bits, the software changes the first number of required bits to their max value (1) and ignores the remaining bits. If less than the required number of bits are entered, the software enters zeros to the left of the pattern until there are enough bits.
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:T1|T2 <9-bit pattern>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:T1|T2?
Timeslot Type = Access
Default: 3A
Edit the tail bits by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
If more bits are entered than the required number of bits, the software changes the first number of required bits to their max value (1) and ignores the remaining bits. If less than the required number of bits are entered, the software enters zeros to the left of the pattern until there are enough bits.
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:ACCess:ETAil <8-bit pattern>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:ACCess:ETAil?
Timeslot Type = Frequency Correction
Displays the payload bits for the frequency correction burst set by the software.
This setting is not available for a Normal GMSK or Normal 8PSK timeslot without channel coding. To configure these timeslots, see the Encrypted Bits cell.
Timeslot Type = Normal GMSK and Normal 8PSK with the following Channel Coding Types:
|
Timeslot Type |
Channel Coding Type |
|---|---|
|
Normal GMSK |
Coded TCH-FS |
|
Coded CS-1 |
|
|
Coded CS-4 |
|
|
Coded DL MCS-1 |
|
|
Coded UL MCS-1 |
|
|
Custom 8PSK |
Coded DL MCS-5 |
|
Coded UL MCS-5 |
|
|
Coded DL MCS-9 |
|
|
Coded UL MCS-9 |
|
|
Coded E-TCH/F43.2 |
|
|
Uncoded |
Choices: PN9 | PN11 | PN15 | PN20 | PN23 | Custom Bit Pattern | User File
Default: PN9
Set the data payload bits by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
Normal GMSK Channel Coding Data SCPI Commands
Normal 8PSK Channel Coding Data SCPI Commands
Timeslot Type = Normal GMSK with the Coded TCH/HS Channel Coding Type
Choices: PN9 | PN11 | PN15 | PN20 | PN23 |Custom Bit Pattern | User File
Default: PN9
This represents the first user in the shared timeslot scheme. Change the data by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:TCH:HS:DATA PN9|PN11|PN15|PN20|PN23|PATTern|"<file name>"
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:TCH:HS:DATA?
If PATTern is the choice, use the following command to create the data pattern:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:TCH:HS:DATA:PATTern "<bit_string>"
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:TCH:HS:DATA:PATTern?
Timeslot Type = Normal GMSK with Coded TCH/HS Channel Coding
This represents the timeslot for a second user in the shared timeslot scheme. It is uneditable and shows a Dummy burst in the timeslot for the alternate frame, which represents an empty timeslot.
Timeslot Type = Normal GMSK
Channel Coding Type = Coded TCH/FS
Choices: 0 | 1
Default: 0
Use the timeslot with or without the listed channel coding. Enter either a 1 or a 0 to specify the normal stealing bits. The single bit defines the value for both 1-bit fields.
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:STEal 0|1
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:STEal?
This setting is not available for a Normal GMSK or Normal 8PSK timeslot with channel coding turned on. To configure these timeslots with channel coding see Data cell.
Timeslot Type = Normal GMSK, Normal 8PSK, Synchronization, Access
Choices: PN9 | PN11 | PN15 | PN20 | PN23 | EXT | Custom Bit Pattern | User File
Default: PN9
Set the encrypted bits by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
Number of bits by timeslot type:
|
57 + 57 bits |
|
174 + 174 bits |
|
39 + 39 bits |
|
36 bits |
Encrypted Bits SCPI Commands
Timeslot Type = Synchronization
Default: B962040F2D45761B
The default bits reflect the GSM protocol.
For the selected Synchronization timeslot, set the training sequence bits by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
If more bits are entered than the required number of bits, the software changes the first number of required bits to their max value (1) and ignores the remaining bits. If less than the required number of bits are entered, the software enters zeros to the left of the pattern until there are enough bits.
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:SYNC:TSEQuence <bit_string>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:SYNC:TSEQuence?
Timeslot Type = Dummy
Displays the payload bits for the dummy burst set by the software per the 3GPP standards.
|
Normal GMSK |
Normal 8PSK |
|
|
Coded TCH/FS |
Coded DL MCS-5 |
|
|
|
Coded TCH/HS |
Coded UL MCS-5 |
|
|
Coded CS-1 |
Coded DL MCS-9 |
|
|
Coded CS-4 |
Coded UL MCS-9 |
|
|
Coded DL MCS-1 |
Coded E-TCH/F43.2 |
|
|
Coded UL MCS-1 |
Uncoded |
Choices: TSC0 | TSC1 | TSC2 | TSC3| TSC4 | TSC5 | TSC6 | TSC7 | Custom
Default: TSC0
The Training Sequence Bits apply to the Normal GMSK and Normal 8PSK Timeslot Type with or without channel coding:
26-bits for Normal GMSK and Normal GMSK with channel coding
78-bits for Normal 8PSK and Normal 8PSK with channel coding
To set the training sequence bits, click on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
If more bits are entered than the required number of bits, the software changes the first number of required bits to their max value (1) and ignores the remaining bits. If less than the required number of bits are entered, the software enters zeros to the left of the pattern until there are enough bits.
Normal GMSK with or without Channel Coding:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:TSEQuence TSC0|TSC1|TSC2|TSC3|TSC4|TSC5|TSC6|TSC7|<26-bit pattern>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:TSEQuence?
Normal 8PSK with or without Channel Coding:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:TSEQuence TSC0|TSC1|TSC2|TSC3|TSC4|TSC5|TSC6|TSC7|<78-bit pattern>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:TSEQuence?
Timeslot Type = Normal GMSK, Normal 8PSK, Frequency Correction, Synchronization, Dummy, Custom GMSK, Custom 8PSK
|
Normal GMSK |
Coded TCH-FS |
|
|
|
Coded CS-1 |
|
|
|
Coded CS-4 |
|
|
|
Coded DL MCS-1 |
|
|
|
Coded UL MCS-1 |
|
|
|
Normal 8PSK |
Coded DL MCS-5 |
|
|
Coded UL MCS-5 |
|
|
|
Coded DL MCS-9 |
|
|
|
Coded UL MCS-9 |
|
|
|
Coded E-TCH/F43.2 |
|
|
|
Uncoded |
Default (applies to only EDGE timeslots):
7FFFFFF for timeslots 0 and 4
FFFFFF for all other timeslot selections
|
|
GSM Timeslots |
|
|
|
|
For the timeslots Normal GMSK with or with channel coding, Frequency Correction, Synchronization, Dummy, and Custom GMSK, this cell only displays the guard period bits set by the software per the 3GPP standards. Timeslots 0 and 4 use 9-bits, and the other timeslots use 8-bits |
|
|
EDGE Timeslots |
|
|
|
|
For the timeslots Normal 8PSK with or without channel coding and Custom 8PSK, set the Guard Period bits by clicking on the cell. Then click the dialog box icon |
If more bits are entered than the required number of bits, the software changes the first number of required bits to their max value (1) and ignores the remaining bits. If less than the required number of bits are entered, the software enters zeros to the left of the pattern until there are enough bits.
Normal 8PSK with or without Channel Coding:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:GUARd <24 or 27-bit pattern>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:GUARd?
Custom 8PSK:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:CUSTom[:PSK8]:GUARd <24 or 27-bit pattern>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:CUSTom[:PSK8]:GUARd?
Timeslot Type = Access
Default: 096FF335478
Set the synchronized sequence bits by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
If more bits are entered than the required number of bits, the software changes the first number of required bits to their max value (1) and ignores the remaining bits. If less than the required number of bits are entered, the software enters zeros to the left of the pattern until there are enough bits.
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:ACCess:SSEQuence <bit_pattern>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:ACCess:SSEQuence?
Timeslot Type = Access
Displays the guard period bits set by the software per the 3GPP standards.
Timeslot Type = Normal GMSK, Normal 8PSK
|
Normal GMSK |
Coded TCH-FS |
|
|
|
Coded CS-1 |
|
|
|
Coded CS-4 |
|
|
|
Coded DL MCS-1 |
|
|
|
Coded UL MCS-1 |
|
|
|
Normal 8PSK |
Coded DL MCS-5 |
|
|
Coded UL MCS-5 |
|
|
|
Coded DL MCS-9 |
|
|
|
Coded UL MCS-9 |
|
|
|
Coded E-TCH/F43.2 |
|
|
|
Uncoded |
Range: 0–50 %
Default: 0.00%
Use the Normal GMSK and Normal 8PSK timeslots with or without the listed channel coding.
Enter the Bit Error Ratio for the selected timeslot.
Normal GMSK with or without Channel Coding:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:BER <val>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:BER?
Normal 8PSK with or without Channel Coding:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:ENCRyption:BER <val>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:ENCRyption:BER?
Timeslot Type = Normal GMSK with the TCH/FS or TCH/HS Channel Coding Type:
Range: 0–100 %
Default: 0.00%
Enter the Frame Erasure Ratio for the selected timeslot.
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:FER <val>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:FER?
Timeslot Type = Normal GMSK and Normal 8PSK with a listed Channel Codding Type
|
Normal GMSK |
Coded CS-1 |
|
|
|
|
Coded CS-4 |
|
|
|
Coded DL MCS-1 |
|
|
|
Coded UL MCS-1 |
|
|
Normal 8PSK |
Coded DL MCS-5 |
|
|
|
Coded UL MCS-5 |
|
|
|
Coded DL MCS-9 |
|
|
|
Coded UL MCS-9 |
Range: 0–100 %
Default: 0.00%
Use the Normal GMSK and Normal 8PSK timeslots with the listed channel coding.
Enter the Block Error Ratio for the selected timeslot.
Normal GMSK with Channel Coding:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:BLER <val>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:GMSK:ENCRyption:BLER?
Normal 8PSK with Channel Coding:
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:ENCRyption:BLER <val>
[:SOURce]:RADio:EDGE[:BBG]:SLOT0|[1]|2|3|4|5|6|7:NORMal:ENCRyption:BLER?