Real Time

SCPI Command List

NOTES:

1. In the SCPI command syntax, the letter n equates to a numeric value.

2. The following SCPI command list may include duplicates of certain commands. This duplication offers you the convenience of accessing a command's related descriptions when it is valid for more than one instrument model or channel type, and therefore, appears in multiple help topics.

[:SOURce]:FSIMulator[1]:FADer[1]2|3|4|5|6|7|8:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DVPeriod <val>

[:SOURce]:FSIMulator[1]:FADer[1]2|3|4|5|6|7|8:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DVPeriod?

[:SOURce]:FSIMulator[1]:FADer[1]:DLENgth <val>

[:SOURce]:FSIMulator[1]:FADer[1]:DLENgth?

[:SOURce]:FSIMulator[1]:FADer[1]:FREQuency <val>

[:SOURce]:FSIMulator[1]:FADer[1]:FREQuency?

[:SOURce]:FSIMulator[1]:FADer[1]:MODE ON | OFF | THR

[:SOURce]:FSIMulator[1]:FADer[1]:MODE?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:AOA <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:AOA?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:AOD <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:AOD?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ASAOA <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ASAOA?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ASAOD <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ASAOD?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:CFCoupling DFR | VSP

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:CFCoupling?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DELay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DELay?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DELay:TYPE FIXed | MOVing

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DELay:TYPE?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DFRequency <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DFRequency?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DRAOA <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DRAOA?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DRAOD <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DRAOD?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DVARiation <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:DVARiation?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ENABle 1 | 0 | ON | OFF

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ENABle?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:FOFFset <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:FOFFset?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:FTYPe RAYLeigh | RICian | SUZuki | PDOPpler | STATic

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:FTYPe?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:LAOA <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:LAOA?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:LOGNormal On | OFF | 1 | 0

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:LOGNormal?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:LOSS <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:LOSS?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:MAXDelay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:MAXDelay?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:MINDelay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:MINDelay?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:PSHift <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:PSHift?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:RKFactor <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:RKFactor?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ROSCillation <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:ROSCillation?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:SDGaussian <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:SDGaussian?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:SSHape 3DB | C6DB | FLAT | ROUNded | JCLassical | JROunded | GAUSsian | HBAThtub | JHBathtub

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:SSHape?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:VSPeed <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:VSPeed?

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:XPRatio <val>

[:SOURce]:FSIMulator[1]:FADer[1]:PATH[1]|2|3|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18|19|20|21|22|23|24:XPRatio?

[:SOURce]:FSIMulator[1]:FADer[1]:SDEViation <val>

[:SOURce]:FSIMulator[1]:FADer[1]:SDEViation?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:EDELay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:EDELay?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:ELOSs <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:ELOSs?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSIDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSIDistance?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSMDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSMDistance?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:MDFRequency <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:MDFRequency?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:TSPeed <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANDard:LTE:HSTrain:TSPeed?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:SCModel DEFault | <SISO_Channel_Model_Name>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:SCModel?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DBSPacing <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DBSPacing?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DTIMe <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DTIMe?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSIDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSIDistance?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSMDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSMDistance?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:MDFRequency <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:MDFRequency?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:TSPeed <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANDard:WCDMa:HSTrain:TSPeed?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MAXDelay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MAXDelay?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MINDelay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MINDelay?

[:SOURce]:FSIMulator[1]:SEED "<val>"

[:SOURce]:FSIMulator[1]:SEED?