The ensemble, also called multiplexer, could be considered as the transmitted signal, comprising a set of regularly and closely-spaced orthogonal carriers. The ensemble is the entity which is received and processed. In general, it contains programme and data services.
An ensemble could also be considered as a collection of all the broadcasting stations on one fixed frequency.
Click on Ensemble, Services or Service components to see how to set it in N7611C.
As shown in the Ensemble setup view above, one could include multiple . There are two ways to add a to an
Under node.
Notice that using method 1, the added will reside in the root directory, and no are allocated to specific Services (, or others).
Under each Service node (, or others).
While using method 2, the added will not only reside in the root directory, but also are allocated to the specific Service.