NOTES:
1. In the SCPI command syntax, the letter n equates to a numeric value.
2. The following SCPI command list may include duplicates of certain commands. This duplication offers you the convenience of accessing a command's related descriptions when it is valid for more than one instrument model or channel type, and therefore, appears in multiple help topics.
[:SOURce]:RADio:XM[:BBG]:BFILe:FILe ?
[:SOURce]:RADio:XM[:BBG]:BFILe:FILe <FileLocation>
[:SOURce]:RADio:XM[:BBG]:BFILe:FRAMe ?
[:SOURce]:RADio:XM[:BBG]:BFILe:FRAMe <val>
[:SOURce]:RADio:XM[:BBG]:BFILe:TYPe DemoFile | KeysightBasebandFile
[:SOURce]:RADio:XM[:BBG]:BFILe:TYPe ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:DELay ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:DELay <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:DELay ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:DELay <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FOFfset <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FOFfset <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FOFfset ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FOFfset ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FREQuency <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FREQuency ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FREQuency ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:FREQuency <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:POWer <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:POWer ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:POWer <val>
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:POWer ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:STATe ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:STATe ON | OFF | 1 | 0
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:STATe ?
[:SOURce]:RADio:XM[:BBG]:ENA|ENB:CARrier1|2|3:STATe ON | OFF | 1 | 0