CDP Graph

The code domain power (CDP) graph shows the power level of each code channel in each timeslot.

Click Generate or Generate and Download from the main tool bar to generate an I/Q waveform, then select a carrier (Basic or Advanced) under Waveform Setup in the Closedtree view to view the normalized CDP distribution in accordance with the current channel power configuration for that carrier at the bottom of the parameter view window. In Basic mode, click on a timeslot in the common channel setup table to view the Resource Unit Setup for that timeslot.

Any changes to the channel or timeslot power configuration do not appear on the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform generation progress.

CCDF Graph

Resource Unit Graph