Common Channel

Common Channel Summary Table

This table displays the key parameters for each common channel. Double-clicking a row activates the setup table for that channel.

Channel Name

Displays each common channel name

State

Choice: ON | OFF

Displays the state of the channel

Power

Range: –60 to 0 dB.

Default: 0 dB

Display the channel power. The CDP graph displays the normalized power of each RU in each channel after you generate the waveform. Refer to the Power Setting for the power calculation of the carriers, channels/timeslots and RUs.

Allocated RU Number

Range: 1 to 2

Default: Depends on the specified data rate for that channel

Displays the allocated resource unit number. This number depends on the data rate and cannot be edited.

Timing Offset

Range: 2 to 16

Default: 16

Displays the transmitting time offset (in chips) of the channel. The cell is active for uplink only.

Data Source

Choices: STD | PN9 | PN15 | USER

Display the selections for the payload data type for the channel.