Choice: On | Off
Default: On
Double-click or use the drop-down menu to set the state of the timeslot or .
Range: –60 to 0 dB.
Default: 0 dB
Enter a value to set the timeslot n power. The CDP graph displays the normalized power of each RU in each timeslot after you generate the waveform. Refer to the Power Setting for the power calculation of the carriers, channels/timeslots and RUs.
Range: 2 to 16
Step: 2
Default: 16
Enter a value to set a max user number for the selected timeslot. The user id of any resource unit is no greater than the max user number of the timeslot.