The software provides a User Defined DPCH with selectable link direction, timeslot, number of RUs, and number of DCHs (1 to 8).
To add a user defined DPCH channel, click Dedicated Channel in the tree view to access the Dedicated Physical Channel Setup window.
Click in the parameter view and select User defined
DPCH from the
list
of channels.
Selecting as the dedicated physical channel automatically sets the state of HS-SICH to On.
Specify the name, link direction, number of timeslots,
RUs, and number of DCHs to be configured from the
selection box
that appears. Clicking OK in the selection box displays the DPCH Setup
window.
Choice: On, Off
Default: On
Set the state of the selected channel to either on
or off. You can double-click the cell to change the state or use
icon at the right of the cell to make your selection.
Range: 1 to 16
Enter a value to identify the user on this DPCH channel. The User ID is used to set the user's midamble shift in all Resource Units. As the User ID changed, the User ID in all of the RUs will be set to the same value of User ID in DPCH. Meanwhile, each User ID (corresponding to midamble shift) of the RU can be set separately in the Resource Unit Setup.
Range: –60 dB to 0 dB
Enter the channel power level relative to the other channels. See Power Settings for details.
Range: –8 to 8 chips
Default: 0 chips
Enter a value to set the transmit timing offset for the channel. If the OSR is equal to 8, 16, 24 or 32, the timing offset values increment by 0.125 chip; if the OSR is set to other values, the timing offset values increment by 1 chip. Physical channels summed in phase produce a high crest factor (high peak-to-average ratio). Offsetting the timing can minimize the crest factor.
Timing Offset property is only valid for uplink timeslots. For downlink timeslots, it is read-only. The switching point determines how timeslots 2 through 6 are allocated between uplink and downlink. Timeslots before the switching point are allocated to the uplink; timeslots after the switching point are allocated to the downlink.
This cell displays the allocated resource unit number. This number depends on the selected data rate and cannot be edited.
Selections: STD | PN9 | PN15 | Pattern | 0, 1 Text File
Default: STD
Click the cell and the icon at the far right
of the cell to access the data menu.
|
STD |
select data as defined in the standard |
|
PN9 |
select random sequence numbers |
|
PN15 |
select random sequence numbers |
|
Pattern |
this selection activates the Pattern Bits cell, which opens the |
|
0, 1 Text File |
select this to load a user-defined 0, 1 Text File as the data source. When this is selected as the data type, two new cells are added to the cell format.
|
Range: 0000000000 to 1111111111 or pattern type
This cell displays the current bits of binary data or the pattern type to be used for the TFCI data.
Click
to set the coder state.
Selections: On | Off
Default: On
Sets the coder state of TFCI.
|
On |
The TFCI_Value_Decimal cell becomes active. |
|
Off |
The Pattern Type cell becomes active. |
The binary format of the TFCI value. This cell is read only. The value must be entered in decimal format, using the TFCI_Value_Decimal cell.
Enter a decimal value up to 1023. The binary equivalent appears in TFCI_Value_Binary. This cell is active only when the Coder State is set to On.
Selections: PN9 | PN15 | Pattern | 0, 1 Text File
Default: PN9
Set the data pattern for TFCI. Click the cell and the down-arrow
at the far right of the cell to access the data
menu. This cell is active only when the Coder State is set to Off.
|
PN9 |
select random sequence numbers |
|
PN15 |
select random sequence numbers |
|
Pattern |
this selection activates the Pattern Bits cell, which opens the |
|
0, 1 Text File |
select this to load a user-defined 0, 1 Text File as the data source. When this is selected as the data type, two new cells are added to the cell format.
|
Selections: PN9 | PN15 | Pattern | 0, 1 Text File
Default: PN9
Click the cell and the down-arrow
at the far right of the cell to access the data
menu.
|
PN9 |
select random sequence numbers |
|
PN15 |
select random sequence numbers |
|
Pattern |
this selection activates the Pattern Bits cell, which opens the |
|
0, 1 Text File |
select this to load a user-defined 0, 1 Text File as the data source. When this is selected as the data type, two new cells are added to the cell format.
|
Selections: PN9 | PN15 | Pattern | 0, 1 Text File
Default: PN9
Click the cell and the down-arrow
at the far right of the cell to access the data
menu.
|
PN9 |
select random sequence numbers |
|
PN15 |
select random sequence numbers |
|
Pattern |
this selection activates the Pattern Bits cell, which opens the |
|
0, 1 Text File |
select this to load a user-defined 0, 1 Text File as the data source. When this is selected as the data type, two new cells are added to the cell format.
|
The Resource Unit Setup table enables you to configure the resource unit for each channel.