Use this cell to select Basic or Advanced capability.
Basic capability supports configuration of all of the WLAN signal parameters except the channel coding function, and so is suitable for component testing.
Parameters under Basic capability are a subset of the Advanced capability.
Advanced capability supports generation of fully channel-coded waveforms and is suitable for both receiver testing and component testing.
The following parameters are supported only by the Advanced capability
Use this cell to enable or disable a carrier other than the main carrier. The main carrier is always enabled. The state of the carriers will be displayed in the carriers table under Waveform Setup.
When a carrier's state is turned OFF, all of the parameters set for this carrier are stored for use the next time it is enabled.