Multiple Signal Generators Solution with Baseband Timing Alignment, but without RF Phase Coherence for MxN MIMO

This topic describes the following configurations:

Using MXG/EXG X-Series Signal Generators

+

The figure above shows you how to set up two X-Series signal generators (either N5182A, N5172B, or N5182B) for a Mx2 (2-antenna receiver) WLAN Solution with Baseband Timing Alignment, but without RF Phase Coherence. Although this example demonstrates Mx2 MIMO, it is easy to expand it to Mx3 and Mx4 MIMO by adding extra signal generators, connecting the corresponding cables, and configuring the Signal Studio software.

If you are using an N5172B or N5182B and one or more N5182A signal generators, you must configure the N5172B or N5182B as the Primary. In addition, the N5182A secondaries must be at the end of the instrument chain.

The X-Series signal generator provides precise baseband timing alignment as a standard feature, which synchronizes the start of the BBG waveform playback capability of up to 16 signal generators. For the N5182A, or N8300A, the playback is synchronized to within a characteristic value of ± 8 ns between the primary and the last secondary. For the N5172B or N5182B, the playback is synchronized to within a characteristic value of ± 5 ns between the primary and the last secondary. This minor amount of delay (± 8 ns or ± 5 ns) can be reduced further to picosecond resolution by adjusting the I/Q Delay. To reduce the delay, check and adjust the BBG signal alignment for each signal generator in the system. For more information on adjusting the delay, refer to the section entitled "I/Q Adjustments" in the MXG/EXG X-Series user's guide.

The delay value includes compensation for cables that have less than 1 ns of propagation delay between the EVENT 1 and PAT TRIG connectors. To minimize synchronization delay, the Keysight BNC cable 10502A is the recommended cable for the rear-panel daisy chain connections

The Event 1 connector on the primary MXG/EXG rear panel is connected to the Pattern Trigger In connector on the secondary MXG/EXG. This ensures that the two baseband generators are precisely synchronized on the start of the waveform playback. Synchronization occurs after the primary signal generator sends a one-time event pulse through the Event 1 connector to the secondary signal generator. Prior to this event, the secondary signal generator must recognize that it is waiting for this event pulse, which occurs during the system configuration. (Refer to the section entitled "Multiple Baseband Generator Synchronization" in the MXG/EXG X-Series user's guide.) In order to properly send the synchronization pulse, the Dual ARB Player for each signal generator must be turned off. The trigger source on the both signal generators is automatically set by the software. On the primary MXG/EXG, it is set to "Bus" to wait for a SCPI command trigger through the GPIB or LAN bus. On the secondary MXG/EXG, it is set to "External" to receive a trigger through the rear-panel PAT TRIG connector.

When you start the N7617C Signal Studio for WLAN 2027, you will need to choose the IEEE 802.11n Mx22 SG in the System Configuration Wizard. You will be asked for connection information for the corresponding number of signal generators. You can use up to two N5182As. Both signal generators must have valid licenses for N7617C Advanced Capability in order to have access to most of the software features for MIMO. Once you have connected to both MXG/EXG X-Series signal generators, the software sends SCPI commands to both signal generators and automatically completes the system configuration. You can now perform the steps to synchronize the baseband generators of each MXG/EXG. (Refer to the section entitled "Multiple Baseband Generator Synchronization" in the MXG/EXG X-Series user's guide.)

When you generate the waveforms for multiple antennas, the Signal Studio for WLAN software pre-calculates the waveform packets and applies the effects of specific channels, then loads the composite waveform into each signal generator.

Using ESG Signal Generators Plus an N5181A Analog Signal Generator as an External BBG Clock

The figure above shows you how to set up two ESG signal generators for a Mx2 (2-antenna receiver) WLAN Solution with Baseband Timing Alignment, but without RF Phase Coherence. Although this example demonstrates Mx2 MIMO, it is easy to expand it to Mx3 and Mx4 MIMO by adding extra signal generators, connecting the corresponding cables, and configuring the Signal Studio software.

Two signal generators (with the same model number) are used and the 10 MHz references are connected between them. When using E4438C ESG signal generators, each requires the special option HEC to provide the external baseband generator clock input on the rear panel. An N5181A MXG signal generator is used as an external common clock for the two baseband generators to ensure timing alignment of the baseband signals. The Event 2 connector on the primary signal generator is connected to the Pattern Trigger In connector on each of the two signal generators. This ensures that the two baseband generators are triggered simultaneously, eliminating time errors in the waveform output. The synchronization occurs right after downloading the waveforms to the both signal generator. The Signal Studio software will send a SCPI command to the primary signal generator to direct it to send a one-time event pulse through the Event 2 connector to itself and the secondary signal generator. Then, this pulse signal triggers the two signal generator to playback the waveform simultaneously.  

The EVENT 2 signal works as both a Trigger Source and an actual Marker 2 output signal, but in different period of time. Before the waveform playback, EVENT 2 serves as the trigger source. Once waveforms are triggered to playback, EVENT 2 won't work as a trigger source and come back to the Marker 2 output whenever marker 2 is present in the waveform.

When you start the N7617C Signal Studio for WLAN 2027, you will need to choose the IEEE 802.11n Mx22 SG in the System Configuration Wizard. You will be asked for connection information for the corresponding number of signal generators. Both signal generators must be the same model and both must have a valid license for N7617C Advanced Capability in order to have access to most of the software features for MIMO.

When you generate the waveforms for multiple antennas, the Signal Studio for WLAN software pre-calculates the waveform packets and applies the effects of specific channels, then loads the composite waveform into each signal generator and applies it directly to the DUT.

Procedure on Signal Studio Software

  1. Set up the PC and the signal generators as shown above.

  2. Click the Quick Setup button in the tree view and double click the IEEE 802.11n Mx2 in the right pane to open the parameter view main window. If you want to expand your setup to Mx3 or Mx4 MIMO, select IEEE 802.11n Mx3 or IEEE 802.11n Mx4 respectively.

  3. Click Waveform Setup in the tree view to configure waveform parameters. The Waveform Basic section contains the key system parameters.

    1. Format: Select HT for this example.

    2. Generation Mode: Select Framed for this example.

    3. Idle Interval: Use the default setting, 20 us. This parameter determines the length of the idle time between frames.

    4. Bandwidth: Use the default 20 MHz.

    5. Leave the default settings for the other parameters.

  4. Click Signal Configuration in the tree view to configure the parameters for the 802.11n PHY and MAC layer.

  5. Configure Coding and Modulation parameters.

    1. The MCS Index can be changed if desired. It determines the number of spatial streams and the modulation type, coding rate, and data rate as shown in the MCS table. Since we have chosen the IEEE 802.11n Mx2 setup, the range of possible choices for the MCS index is 0 to 15. Use any of these values.

    2. Number of Transmit Chains: set it to 2. This parameter determines the M value in a MxN MIMO system. Since we have chosen Mx2 MIMO in the quick setup, setting this parameters to 2 means that we are configuring a 2x2 MIMO system.

    3. Number of Space Time Streams: Use the default of 2.

    4. Number of Extension Spatial Streams: Use the default value of 0.

    5. Short Guard Interval: Set it to OFF. This sets the guard interval to 800ns.

    6. Operating Mode: Select to GreenField. In GreenField mode, HT packets are transmitted without a legacy compatible part.

    7. Spatial Mapping Scheme: Use the Spatial Expansion scheme.

    8. Scrambler, Convolutional Coder, and Interleaver: Enable scrambler, convolutional coder, and interleaver so that the channel is fully coded.

  6. Configure payload data.

    1. Aggregation MPDU: You can turn A-MPDU ON or OFF. For this example, turn it on to allow multiple MPDUs in one PSDU (PHY service data unit).

    2. The bottom half of the screen allows you to add MPDUs to this zone. One MPDU is present by default. Click Add to add a second one.

    3. Number of Frames: set it to 1.

  7. Click MPDU0 in the tree view or double-click in the first column of the row in the table. This displays a window where you can choose the following for each MPDU.

    1. Data Type: Select PN9 sequence.

    2. Data Length: Use the default setting, 1024 Bytes in this example.

    3. MAC Header: MAC Header format is very important for receiver test. The MAC header provides the DUT with information about the data being transmitted. If the header is formatted incorrectly, the DUT will not recognize the frame, preventing FER/PER testing. It is critical that the frame control in the MAC header be set properly to obtain valid packets. IEEE 802.11, 1999, paragraph 7, Frame formats defines several frame types. To set the frame for data, the MAC header would be formatted to 0800. The second portion of the MAC header specifies addresses. Not all frame types use all the address fields. Signal Studio provides a checkbox that can be cleared if that is desired. Note that the frame length changes when the addresses are not selected. If the address of the DUT is not the same as that being transmitted, the frame will be ignored by the DUT, unless the device is in ad hoc mode. In this example, the MAC header for a data frame with addresses is set as shown in the figure below.

    4. MAC FCS: Enable MAC FCS to append the MAC FCS to the data payload in this example.

    5. Leave the default settings for the other parameters.

  8. Configure Impairments in Waveform by clicking Signal Configuration in the tree view. Set Channel State to ON in this example for a Mx2 MIMO receiver test. (For transmitter test application, set the channel state to OFF.)

    1. Click the button in this Channel cell to configure channel fading parameters.

    2. Channel Mode: Use mode B in this example. Options A to F of model type correspond to channel models defined in IEEE 802.11-03/940r (IEEE p802.11 Wireless WLANs TGn channel models).

    3. Fading Type: Use the default Rayleigh in this example. You may also set it to Rice, depending on your test requirements.

    4. Channel Power Correlation Type: In this example, set it to Complex so that the antenna correlations are computed from the signal voltages (complex).

    5. Number of Transmit Antennae: Displays the number of transmit antennae. It is equal to the number of transmit chains in HT mode in this example.

    6. Number of Receive Antennae: Displays the number of receive antennae. It is determined by the number of signal generators you select in the Quick Setups. In this example, it is 2.

    7. Leave the default settings for the other parameters.

  9. Click Hardware in the tree view and click Signal Generator1 (Primary) to configure the signal generator 1 settings.

    If you are using E4438C ESG signal generators:

    1. Instrument Model Number: In Configuration section, set the instrument model number to E4438C.

    2. VCO Clock: In Dual Arb section, set the VCO clock to external.

    3. Keep the defaults for the other signal generator settings.

    If you are using N5182A MXG signal generators:

    1. Instrument Model Number: In Configuration section, set the instrument model number to N5182A.

    2. Keep the defaults for the other signal generator settings.

  10. Click Hardware in the tree view and click Signal Generator2 (Secondary) to configure the signal generator 2 settings.

    If you are using E4438C ESG signal generators:

    1. Instrument Model Number: In Configuration section, set the instrument model number to E4438C.

    2. VCO Clock: In Dual Arb section, set the VCO clock to external.

    3. Keep the defaults for the other signal generator settings.

    If you are using N5182A MXG signal generators:

    1. Instrument Model Number: In Configuration section, set the instrument model number to N5182A.

    2. Keep the defaults for the other signal generator settings.

  11. Click Graph to view the CCDF curves, if desired.

  12. Click Generate to generate waveform packets.

  13. Click Download to download waveforms to each signal generator after you have configured the instrument connection.