Installation Steps: 1 2 3 4 5 6 7
Some instruments require unique configurations for use with Signal Studio and are not described in this topic.
Ensure the signal generator is turned off.
Connect the signal generator to the computer using one of the following methods for instrument control:
LAN
Network — connect
both the signal generator and the computer to an external LAN network
using standard LAN cables.
Crossover
LAN — connect
the signal generator directly to the computer using a crossover LAN cable.
(You will need to configure
your PC.)
GPIB
— connect
the signal generator directly to the computer using a GPIB cable.