|
1. General Settings |
2. MIMO Settings |
|---|---|
|
3. UL CoMP Settings |
4. Demodulation Reference Signal Settings |
|---|---|
|
5. PUSCH Frequency Hopping Parameters |
6. Transmission Settings |
|---|---|
|
1. General Settings |
2. Demodulation Reference Signal Settings |
3. UL CoMP Settings |
4. Transmission Settings |
|---|---|---|---|
|
Transmission Configuration Length |
Choice: On | Off
Default: On
Double-click or use the drop-down menu to set the Activate-DMRS-with OCC parameter on or off for the corresponding PUSCH transmission.
See 3GPP TS 36.211 and 36.331, for more information.
Displays the identifying number of the selected channel.
Range: (Dependent on the Total Number of Antennas, Number of Layers, and DCI Format.)
N/A (DCI Format 0 case) Default when 1 Antenna is selected under Uplink Cell Parameters or when DCI Format is set to Format 0.
0 to 5 (2 Antennas, 1 Layer case)
0 (2 Antennas, 2 Layers case) Default when 2 Antennas are selected under Uplink Cell Parameters
0 to 23 (4 Antennas, 1 Layer case)
0 to 15 (4 Antennas, 2 Layers case) Default when 4 Antennas are selected under Uplink Cell Parameters
0 to 11 (4 Antennas, 3 Layers case)
0 (4 Antennas, 4 Layers case)
Enter the codebook index for the corresponding PUSCH transmission.
In case of DCI Format 0, N/A is displayed.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn the coding state On or Off.
Use the Data Source Selection dialog box to select , , , or or user defined bits to use for the data in the transport block 1 (codeword 0).
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Use the Data Source Selection dialog box to select , , , or or user defined bits to use for the data in the transport block 2 (codeword 1).
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Choice: None | Every Subframe
Default: None
Sets the data reset method for UL-SCH.
the transport data is continuously repeated seed data which is specified by Data parameter. The transport data is not reset till end of the waveform.
the transport data is reset at the start of each subframe.
Choice: (Dependent on the Total Number of Antennas, Number of Layers and Number of Codewords.)
Format 0 (1 Antenna case) Default when 1 Antenna is selected under Uplink Cell Parameters
Format 0 | Format 4 (2 Antennas, 1 Layer, 1 Codeword case) Default =4 when 2 Antennas are selected under Uplink Cell Parameters
Format 0 | Format 4 (4 Antennas, 1 Layer, 1 Codeword case) Default =4 when 4 Antennas are selected under Uplink Cell Parameters
Default: Format 0
Double-click or use the drop-down menu to select the DCI Format for the corresponding PUSCH transmission.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Range: 1 to 3
Default: 1
Enter a delta shift value which is used to calculate the cyclic shift alpha for the PUCCH.
Refer to 3GPP TS 36.211.
Range: 0 to 29
Default: 0
Enter a value which determines the sequence shift pattern for the demodulation reference signal (DMRS) for PUSCH.
Range: 0 to 509
Default: 0
Coupling: Read only value unless UL CoMP State is set to On
Enter a value that is used in the initialization of the cyclic shift hopping for the generation of the DMRS PUSCH pseudo random sequence. This is used for the virtual cell ID.
See 3GPP TS 36.211 and 36.311 for more information.
Choice: Off | Group Hopping | Sequence Hopping
Default: Off
Double-click or use the drop-down menu to enable the hopping type for the selected transmission.
Choice: (It depends on DCI Format)
Off | Inter-subframe | Intra and inter-subframe (DCI Format 0 case)
Off (DCI Format 4 case)
Default: Off
Double-click or use the drop-down menu to select the PUSCH Hopping Mode in case of DCI Format 0. Otherwise it’s inactive.
See 3GPP TS 36.211, 36.212 and 36.213 for more information.
Range: 0 to 98
Default: 0
Enter a value for the frequency hopping offset of PUSCHs. Refer to the 3GPP technical standards for more information.
Refer to the TS 3GPP 36.211 5.3.4 and 36.213 8.4 about the PUSCH frequency hopping for more information.
Range: 1 to 4
Default: 1
Double-click or use the drop-down menu to select the frequency hopping subbands of PUSCHs.
This parameter is only available when the frequency hopping type is set to Type 2.
Refer to the TS 3GPP 36.211 5.3.4 and 36.213 8.4 about the PUSCH frequency hopping for more information.
Choice: Type1 +1/4 | Type1 -1/4 | Type1 +1/2 | Type2
Default: Type1 +1/2
Double-click or use the drop-down menu to select the frequency hopping type of the PUSCHs.
Type 1 +1/4 and Type 1 -1/4 are only available when the number of system resource blocks is greater than 50.
Refer to the TS 3GPP 36.211 5.3.4 and 36.213 8.4 about the PUSCH frequency hopping for more information.
Displays the name (type) of the selected channel.
UCI = Uplink Control Information
UL-SCH = Uplink Shared Channel
Range: 0 to (Maximum resource elements -1)
Default: 0
Enter the nDMRS(1) value which is used to calculate the cyclic shift alpha of the demodulation reference signal (DMRS).
Refer to 3GPP TS 36.211.
Range: 0 to Calculated Value
This value is dependent on the other related PUCCH settings.
Default: 0
Enter the PUCCH format 2/2a/2b resource index nPUCCH(2,0) for antenna port index 0.
Calculated value is nPUCCH(2) < N_RB(2) * N_RB_sc + Ceiling(N_CS(1)/8) * (N_RBsc – N_CS(1) – 2).
See 3GPP TS 36.211, 36.213 and 36.331, for more information.
Range: 0 to Calculated Value
This value is dependent on the other related PUCCH settings.
Default: 0
Enter the PUCCH format 2/2a/2b resource index nPUCCH(2,1) for antenna port index 1, when the Number of Antennas is 2 Antennas.
Otherwise it’s read only.
Calculated value is nPUCCH(2) < N_RB(2) * N_RB_sc + Ceiling(N_CS(1)/8) * (N_RBsc – N_CS(1) – 2).
See 3GPP TS 36.211, 36.213 and 36.331, for more information.
Displays the total number of ACK bits on the definition of UCI Transmission Configuration as generated by PUCCH Wizard.
Choice: Dependent on the Total Number of Antennas and Number of Layers.)
1 (1 Antenna case) Default when 1 Antenna is selected under Uplink Cell Parameters
1 (2 Antennas, 1 Layer case)
2 (2 Antennas, 2 Layers case) Default when 2 Antennas are selected under Uplink Cell Parameters
1 (4 Antennas, 1 Layer case)
1 | 2 (4 Antennas, 2 Layers case) Default =2 when 4 Antennas are selected under Uplink Cell Parameters
2 (4 Antennas, 3 Layers case)
2 (4 Antennas, 4 Layers case)
Default: 1
Double-click or use the drop-down menu to select the number of codewords for the corresponding PUSCH transmission.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Choice: (Dependent on the Total Number of Antennas.)
1 (1 Antenna case) Default =1 when 1 Antenna is selected under Uplink Cell Parameters
1 | 2 (2 Antennas case) Default =2 when 2 Antennas are selected under Uplink Cell Parameters
1 | 2 | 3 | 4 (4 Antennas case) Default =4 when 4 Antennas are selected under Uplink Cell Parameters
Double-click or use the drop-down menu to select the number of layers for the corresponding PUSCH transmission. The number of layers is less than or equal to the number of antennas.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Displays the total number of NACK bits on the definition of UCI Transmission Configuration as generated by PUCCH Wizard.
Range: 1 to 8
Default: 1
The value you enter sets the number of available hybrid automatic repeat request (HARQ) processes and defines the interval (number of subframes) between retransmissions. Use the Assigned Processes parameter to enable HARQ processes. In the current LTE TDD signal studio it only supports one HARQ process for the UL-SCH.
Range: 0 to 8
Default: 0
Enter a value for the PUCCH and DMRS PUCCH.
Refer to 3GPP TS 36.211.
Range: 0 to Maximum resource block - 1
Default: 1
Enter a value for the PUCCH and DMRS PUCCH.
Refer to 3GPP TS 36.211.
Range: -60.000 to 20.000 dB
Default: 0.000 dB
Enter a power level in dB for the selected channel. See Output Power Calculation (Uplink) for a description of how the software applies your power settings.
Range: 0 to 509
Default: 0
Coupling: Read only value unless UL CoMP State is set to On
Enter a value for the PUCCH Identity (ID) that is used for the virtual cell ID.
See 3GPP TS 36.211 and 36.311 for more information.
Range: 0 to 509
Default: 0
Coupling: Read only value unless UL CoMP State is set to On
Enter a value for the PUSCH Identity (ID) that is used for the virtual cell ID.
See 3GPP TS 36.211 and 36.311 for more information.
Choice: On | Off
Default: Off
Double-click or use the drop-down menu to turn the resource allocation type 3 state on or off for the channel.
When this parameter is changed to on, System Bandwidth is set to 10 MHz or 20 MHz, and Cyclic Prefix is set to Normal, automatically.
When Transmission BW is changed to a value other than 10 MHz or 20 MHz, or Cyclic Prefix is changed to Extended, this parameter is automatically set to off.
This parameter does not affect the parameter setting on the FRC Wizard window.
See 3GPP TS 36.213 8.1.4 for more information.
Range: 0 to 65535
Default: 0
Enter a value for the Radio Network Temporary Identifier (RNTI).
Range: 0 to 65535 (0x0000 to 0xFFFF)
Default: 1 (0x0001)
Enter the Radio Network Temporary Identifier (RNTI) for the corresponding PUCCH transmission.
The input method can be in decimal format or hexadecimal format.
Example: The decimal input "15" is displayed as "15 (0x000F)" and the hexadecimal input "0xf" is displayed as "15 (0x000F)".
See 3GPP TS 36.211 and 36.321, for more information.
Range: 0 to 65535 (0x0000 to 0xFFFF)
Default: 1 (0x0001)
Enter the Radio Network Temporary Identifier (RNTI) for transport block 1 (codeword 0).
The input method can be in decimal format or hexadecimal format.
Example: The decimal input "15" is displayed as "15 (0x000F)" and the hexadecimal input "0xf" is displayed as "15 (0x000F)".
See 3GPP TS 36.211 and 36.321, for more information.
Range: 0 to 65535 (0x0000 to 0xFFFF)
Default: 1 (0x0001)
Enter the Radio Network Temporary Identifier (RNTI) for transport block 1 (codeword 1).
The input method can be in decimal format or hexadecimal format.
If the "number of codewords" parameter is 2, this parameter is displayed. Otherwise it’s hidden.
Example: The decimal input "15" is displayed as "15 (0x000F)" and the hexadecimal input "0xf" is displayed as "15 (0x000F)".
See 3GPP TS 36.211 and 36.321, for more information.
Range of sequence length: 1 to 16
Range of each value: 0 to 3
Default: 0,2,3,1
Enter the numbers of individual RV Index Sequence, separated by commas (for example, 1,2,3).
Choice: Auto | Manual
Default: Auto
Double-click or use the drop-down menu to set the RV Index Configuration for the UL-SCH.
In Auto mode, the RV Index for PUSCH's will be defined by RV Index Sequence. PUSCH will use the first element in RV Index Sequence by default and the index will increase when Retransmission state is on.
In Manual mode, RV Index will be set manually in UL-SCH TX Sequence Dialog and independent with each Retransmission
Choice: On (AUTO) | Off (Manual)
Default: On (AUTO)
Double-click or use the drop-down menu to turn scrambling on or off.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn the channel On or Off.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn the capacity of supporting 64QAM state on or off for the UL-SCH. This parameter determines if 64QAM support is available for Modulation Coding Scheme (MCS) indexes equal to or greater than 14. For MCS indexes less than 14, this parameter has no effect.
Choice: Off | On
Default: Off
Double-click or use the drop-down menu to turn the capacity of supporting 256QAM state on or off for the UL-SCH. This parameter determines if 256QAM support is available for Modulation Coding Scheme (MCS) indexes equal to or greater than 23. For MCS indexes less than 23, this parameter has no effect.
Click the
button in this cell to open the UL-SCH Tx sequence window or UCI Tx sequence window.
Range: 1 frame to Waveform Generation Length, Max 16 frames
Default: 1 frame
Set the length of transmission configuration. The definition of transmission configuration of SCH and UCI will be repeated to the end of the Waveform Generation Length.
UI parameter couplings:
If the Waveform Generation Length parameter is set less than the Transmission Configuration Length, the value of Transmission Configuration Length is changed to be ≤Waveform Generation Length. In summary, the relation between Transmission Configuration Length and Waveform Generation Length is that the Transmission Configuration Length ≤Waveform Generation Length. Refer to the Waveform Generation Length parameter.
Channel
Transmission Configuration Length
Default Value
Uplink
UL-SCH
The value is available to set 1 -16 Frames With following rule:
Transmission Configuration Length ≤Waveform Generation Length
1 Frame
UCI
The value is automatically set to same value corresponding UL-SCH.
Same as UL-SCH
: This is a read only parameter. Use UL-SCH to set the Transmission Configuration Length parameter.
Example: Where the Transmission Configuration Length is set to 2, Frames #0 and #1 configurations (Sequences #1 through #20) will be repeated while generating
SCH.
Displays the transmission mode for the corresponding PUSCH transmission.
The Transmission Mode is dependent on the Total Number of Antennas used.
Transmission Mode 1 is used for single antenna transmission and Transmission Mode 2 is used for multi-antenna transmission.
1 : Single Antenna Port (Port 10) Default when 1 Antenna is selected under Uplink Cell Parameters
2 : Single Antenna Port (Port 10) / Closed Loop Spatial Multiplexing Default when 1 or 4 Antenna(s) is(are) selected under Uplink Cell Parameters
See 3GPP TS 36.211 and 36.213, for more information.
Choice: MCS | Manual
Default: MCS
Double-click or use the drop-down menu to select the PUSCH Transmission Setting Mode.
In the case of MCS, the modulation type, TBS index and transport block size (in UL-SCH Tx sequence window) are automatically selected by the MCS index.
Otherwise manual selection is available to the modulation type, TBS index and transport block size in UL-SCH Tx sequence window.
See 3GPP TS 36.212 and 36.213, for more information.
Choice: On | Off
Default: Off
Double-click or use the drop-down menu to turn the state On or Off.
|
|
On |
|
PUSCH ID and DMRS PUSCH CSH ID are available to set a value |
|
|
Off |
|
PUSCH ID and DMRS PUSCH CSH ID are read only |
See 3GPP TS 36.211 and 36.311 for more information.
Choice: On | Off
Default: Off
Double-click or use the drop-down menu to turn the state On or Off.
|
|
On |
|
PUCCH ID is available to set a value |
|
|
Off |
|
PUCCH ID is read only |
See 3GPP TS 36.211 and 36.311 for more information.