Resource Block (Basic LTE-A TDD Downlink)

Before adding a resource block collection as described below, delete any existing transport channel, physical channel, or resource block collection that occupies the resource blocks that your new resource block collection will occupy. If you add a new resource block collection without first deleting a conflicting channel or resource block collection, a ”code conflicted” error occurs when you generate the waveform.

When you click the Add New resource block button , the software adds a new resource block collection above the currently selected resource block collection in the list. The software assigns an identifying number to the new resource block collection that corresponds to its position in the list and increments the identifying numbers of subsequent resource block collections in the list.

Similarly, if you delete the selected resource block collection using the Delete selected resource block button , the software adjusts the identifying numbers of the subsequent resource block collections according to their new positions in the list.

Resource Block Collection

Resource Block Collection Number

State

Power

Modulation Type

Slot Number

Resource Blocks

Data

Resource Block Collection Number

Displays the identifying number of the currently selected resource block collection.

Before adding a resource block collection as described below, delete any existing transport channel, physical channel, or resource block collection that occupies the resource blocks that your new resource block collection will occupy. If you add a new resource block collection without first deleting a conflicting channel or resource block collection, a ”r;code conflicted” error occurs when you generate the waveform.

State

Choice: Off | On

Default: On

Double-click or use the drop-down menu to turn the selected resource block collection On or Off.

This parameter is read-only for resource block collections that are occupied by a higher layer.

Power

Range: -60.000 to 20.000 dB

Default: 0.000 dB

Enter a power level for the selected resource block collection. See Power Settings (Downlink) for a description of how the software applies your power setting.

Modulation Type

Choice: QPSK | 16QAM | 64QAM | 256QAM

Default: QPSK

Double-click or use the drop-down menu to select the modulation type for the selected resource block collection.

This parameter is read-only for resource block collections that are occupied by a higher layer.

Slot Number

Enter a slot number to assign the selected resource block collection to a specific slot in the frame. The combination of Slot Number and Resource Blocks defines a resource block collection.

This parameter is read-only for resource block collections that are occupied by a higher layer.

Resource Blocks

Enter one or more numbers (separated by commas) or a range (for example, 1-10) to assign specific resource blocks in the frequency domain to the resource block collection. The combination of Slot Number and Resource Blocks defines a resource block collection. Resource blocks in a collection must be in the same slot, but do not have to be contiguous in the frequency domain. The number of resource blocks available in the frequency domain is determined by the System Bandwidth setting defined in the Downlink Setup node.

This parameter is read-only for resource block collections that are occupied by a higher layer.

Data

Use the Data Source Selection dialog box to select PN9, PN15, or User Defined Bits to use for the data.

Higher Layer is displayed in the Data cell if the selected resource block collection is occupied by a higher layer.