Choice:
Basic LTE: E-TM1.1 | E-TM1.2 | E-TM2 | E-TM2a | E-TM2b | E-TM3.1 | E-TM3.1a | E-TM3.1b | E-TM3.2 | E-TM3.3 | E-TM1.1 BC3 CS3 | E-TM1.2 BC3 CS3 | E-TM2 BC3 CS3 | E-TM2a BC3 CS3 | E-TM2b BC3 CS3 | E-TM3.1 BC3 CS3 | E-TM3.1a BC3 CS3 | E-TM3.1b BC3 CS3 | E-TM3.2 BC3 CS3 | E-TM3.3 BC3 CS3 | None
Basic LTE-A: E-TM1.1 | E-TM1.2 | E-TM2 | E-TM2a | E-TM3.1 | E-TM3.1a | E-TM3.2 | E-TM3.3 | E-TM1.1 BC3 CS3 | E-TM1.2 BC3 CS3 | E-TM2 BC3 CS3 | E-TM3.1 BC3 CS3 | E-TM3.2 BC3 CS3 | E-TM3.3 BC3 CS3 | None
Default: None
Double-click or use the
drop-down menu to set the Test Model type.
The software sets the parameters displayed in the lower section of the window to predetermined values for the Test Model type and Reference Channel “A” value selected.
Choice: 1.4 MHz (6RB) | 3 MHz (15RB) | 5 MHz (25RB)) | 10 MHz (50RB) | 15 MHz (75RB) | 20 MHz (100RB)
Default:
LTE: 5 MHz (25RB)
LTE-A: 10 MHz (50RB)
Double-click or use the drop-down menu to set the system bandwidth and number of resource blocks (RB). When you select a system bandwidth, the software automatically adjusts the values in the Total Number of Resource Blocks and Total Number of Occupied Sub-carriers cells.
Advanced LTE and LTE-A carriers only: When the system bandwidth is decreased, the DL-SCH Tx Sequence window's RB size, and some of the other data channel's settings, are reconfigured, similar to when a predefined configuration is executed. But, when the system bandwidth is increased, no change to the DL-SCH Tx Sequence window's RB size, or the other data channel's settings occurs.
Choice: On | Off
Default On
Click in the cell and use the drop-down arrow to select either On or Off.
|
On |
Frequency Offset, Cell ID, Uplink Downlink Configuration, Special Subframe Configuration, and Cyclic Prefix are automatically set by the software. In addition for the secondary cells, Uplink Downlink Configuration, Special Subframe Configuration, and Cyclic Prefix become read only and use the same values as the primary cell. For Cell ID, it is set to the same value as the Component Carrier index number. |
||
|
Off |
Manually set Frequency Offset, Cell ID, Uplink Downlink Configuration, Special Subframe Configuration and Cyclic Prefix. |
Range: 0 to 503
Default: 0 with Auto Carrier Aggregation Configuration set to Off
Same as the CC index number with auto Carrier Aggregation Configuration set to On
With Auto Carrier Aggregation Configuration set to Off, enter a Cell ID value.
The software uses this value to set the Physical Layer Cell ID group and sector cells:
Cell ID = (3 x Physical Cell ID group + Physical Cell ID sector).
See 3GPP TS 36.211 for more information.
Choices: 1 slot (0.5 ms) | 2 slots (1.0 ms) | … | 18 slots (9.0 ms) | 19 slots (9.5 ms) | 1 frame (10 ms) | 2 frames (20 ms) | 3 frames (30 ms) | 4 frames (40 ms)
Default: 1 frame (10 ms)
Double-click or use the drop-down menu to select the waveform generation length.
When the waveform generation length or offset is set, Waveform Generation Length + Waveform Generation Offset <= 1 frame (10 ms) is automatically satisfied by the software.
When the waveform generation length is longer than 1 frame, the waveform generation offset is limited to 0 slot (0.0 ms).
Range: 0 to 8 (Normal CP), 0 to 6 (Extended CP)
0 to 9 (Normal CP), 0 to 7 (Extended CP)
Default: 0
Coupling: For Basic, Advanced UL, and Advanced DL LTE-A TDD when Auto Carrier Aggregation Configuration is set to On, this setting is read only for the secondary cells that has the same value as the primary cell.
Double-click or use the drop-down menu to select the special subframe configuration. The special subframe configurations are defined in Table 4.2-1 of 3GPP TS 36.211.
Range: 0 to 6
Default: 0
Coupling: For Basic, Advanced UL, and Advanced DL LTE-A TDD when Auto Carrier Aggregation Configuration is set to On, this setting is read only for the secondary cells that has the same value as the primary cell.
Double-click or use the drop-down menu to select the uplink-downlink configuration.
The supported uplink-downlink configurations are defined in Table 4.2-2 of 3GPP TS 36.211.
In the case of intra-band carrier aggregation, the PCell parameter is editable, but SCell is read-only. With inter-band carrier aggregation, both parameters are editable.
The resource blocks and some parameters are reconfigured by changing the Uplink Downlink Configuration parameter in the same manner as Predefined Configuration.