When using multiple instruments as shown in the tree view, inaccurate test data may occur if a combination of the GUI and SCPI is used to set or modify the instrument and test parameters. The software will not reflect changes made outside of the GUI even with the use of the Update from Instrument button. For all tests, use only one method to configure the settings, GUI or SCPI.
When configuring multiple instruments with SCPI instead of using the GUI, the commands must be executed for each instrument.
When using multiple instruments as shown in the tree view, after clicking the State On button, all settings for this window gray out and cannot be changed. To change the settings, first click the State Off button.
|
1. UL-SCH Settings |
2. HARQ-ARQ Settings |
3. Hybrid-ARQ ACK/NACK Data Settings |
|---|---|---|
|
|
||
|
|
||
|
|
|
|
|
This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. When using multiple instruments as shown in the tree view, this button is not displayed. |
|
|
This button displays in place of the Settings Current button. It indicates that the instrument settings are not currrent and need to be updated with the new software settings. Click this button to update the insturment's settings. This button shows in all windows regardless of where the change was made. When using multiple instruments as shown in the tree view, this button is not displayed. |
Choice: PN9 | PN15 | Custom Pattern | User Defined
Default: PN9
Click the parameter and then use the
button to launch the data dialog box.
|
PN9 |
Uses PN9 sequence as data bits |
|
PN15 |
Uses PN15 sequence as data bits |
|
Custom Pattern |
Uses the user defined pattern specified in string and '0' or '1' is expected in the string pattern |
|
User Data |
Uses a user-defined sequence in a file as data bits |
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:TYPE PN9|PN15|PATTern|FILE
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:TYPE?
If PATTern is the data type selection, use the following command to set the pattern. To set the pattern, use a series of 0, 1, or a combination of the two, 011100110, up to a maximum of 128,000 bits.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:PATTern <pattern>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:PATTern?
If FILE is the data type selection, use the following commands to load a previously saved file, and to set what length of the file to use.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:NAME <"filename">
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:NAME?
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:LENGth <val>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:LENGth?
Choice: QPSK | 16QAM | 64QAM
Default: QPSK
When Payload Configuration Type in UL-SCH channel is set to Manual, double-click or use the drop-down menu to select the modulation type for the PUSCH. When the Payload Configuration Type in the UL-SCH channel is set to MCS Index, this value is calculated by the MCS Index. Refer 3GPP TS36.211, Table 8.6.1-1 for more details.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:MODulation QPSK|QAM16|QAM64
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:MODulation?
Choice: MCS Index | Manual
Default: MCS Index
Double-click or use the drop-down menu to select the UL-SCH Payload Configuration Type.
|
MCS Index |
Selects a payload size determined by the Table 7.1.7.2.1-1 ( 3GPP TS36.213) which specifies the permissible combinations of transport block size, resource allocation and modulation scheme that are available for transmission. |
|
Manual |
Allows you to enter any payload size within the minimum (16) and maximum limits (75376) of Table 7.1.7.2.1-1 (3GPP TS36.213). |
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:CONFig MINDex|MANual
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:CONFig?
Range: 0 to 28
Default: 5
Enter a value of MCS Index. This parameter is used when the Payload Configuration Type is MCS is set to MCS Index.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:MINDex <val>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:MINDex?
Displays the value of TBS index. The value is calculated by the MCS Index, Refer to 3GPP TS36.211, Table 8.6.1-1 for more details. This parameter is used when the UL-SCH Payload Configuration Type is set to MCS Index.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:TINDex?
Range: 16 to 75376
Default: 2216
Coupling: The Configuration Type selection determines whether this setting is display only or active.
Displays the payload size when the UL-SCH Payload Configuration Type is set to MCS Index. With MCS Index, the payload size is determined by the size of occupied resource blocks and the MCS Index. Refer to 3GPP TS36.213 for more detailed information.
Enter a value to set the payload size when the UL-SCH Payload Configuration Type is set to Manual.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:SIZE <val>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:SIZE?
Range: 0 to 27
Default: 3
Enter the maximum number of times for the uplink shared channel to be retransmitted.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:MNRetrans <val>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:MNRetrans?
Range: 0-65535
Default: 8
Enter the HARQ ACK initial response length. The software uses this setting when the Data Source selection is External.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:PROCess:LENgth:IACK <val>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:PROCess:LENgth:IACK?
Default: 0, 2, 3, 1
Entry format: Array of RV Index (Integer 0-3)
Array length: 1 to 28
Enter the RV (redundancy version) Index sequence pattern for verifying HARQ responses. The RV Index data can be entered as a sequence with values of 0, 1, 2, 3 separated by commas. When the specified length of RV index sequence pattern is shorter than the maximum number of retransmission, the pattern is repeated until reaching the maximum length.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:RVINdex:PATTern:DATA <val>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:RVINdex:PATTern:DATA?
Choice: Internal | External
Default: Internal
Double-click or use the drop-down menu to select HARQ ACK/NACK control signal source.
|
Internal |
Uses an internal user-defined signal. |
|
External |
Uses an external signal from AUX ports. |
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:SOURce INTernal|EXTernal
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:SOURce?
Choice: All ACK| All NACK| Custom Pattern| User Data
Default: All ACK
Coupling: Active when Data Source is set to Internal.
Click the parameter and then use the
button to launch the data dialog box.
|
All ACK |
All ACK sequence |
|
All NACK |
All NACK sequence |
|
Custom Pattern |
Uses the user defined pattern specified in string and 'A' or 'N' is expected in the string pattern |
|
User Data |
Select a user-defined sequence from an existing file on the local drive |
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:TYPE AACK|ANACk|FILE|PATTern
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:TYPE?
If FILE is the selection, use the following command to load an existing file for the ACK/NACK data.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:FILE:NAME <"filename">
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:FILE:NAME?
If PATTern is the selection, use the following command to create the custom pattern with a maximum of 8,192 characters. The pattern is a string that uses "A" (ACK), "N" (NACK), or a combination "ANNANAA".
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:PATTern <"pattern">
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:PATTern?
Displays the fixed delay time (0)of the input port for control of the HARQ ACK/NACK. The delay time is displayed when the HARQ ACK/NACK Data Source is set to External and the AUX Operating Mode is set to Multiplexed.
Displays the fixed delay (0) of the HARQ ACK response in the serial data transmission. The unit of delay is in subframe. The delay is displayed when the HARQ ACK/NACK Data Source is set to External and the AUX Operating Mode is set to Dedicated.
Choice: Choice: NACK | ACK
Default: NACK
Coupling: Grayed out unless Operating Mode is set to and Data Source is set to External.
Double-click or use the drop-down menu to select the default value for the HARQ ACK/NACK response when the feedback signal is not received.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:EXTernal:DATA:SERial:DEFault ACK|NACK
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:EXTernal:DATA:SERial:DEFault?