This Channel Setup Advanced Downlink configuration has several different possible channel setups (e.g. BCH, CFI, ...). The screen shot below shows the parameter choices for a DL-SCHn channel. In the N7625B Signal Studio software, click a different channel to view that channel's parameter choices. The links for all of the channel's parameters and their descriptions are listed in the tables below.
|
1. General Settings |
2. UE Specific Reference Signal Settings (DM-RS) |
3. MIMO Settings |
4. Transmission Settings |
5. Dedicated DCI Settings |
|---|---|---|---|---|
|
Modulation and TBS Index Table |
||||
|
BCH |
CFI |
HI |
|---|---|---|
|
1. General Settings |
1. General Settings |
1. General Settings |
|
DCI |
|||
|---|---|---|---|
|
1. General Settings |
2. Cross Carrier Scheduling |
3. Dedicated PDCCH Setting for DL-SCH |
4. Dedicated PDCCH Setting for UL-SCH |
|
DCI (continued) |
||
|---|---|---|
|
5. Dedicated PDCCH Setting for Random Access Procedure |
6. Dedicated PDCCH Setting for Uplink Power Control |
7. Manual PDCCH Setting |
|
MCH |
||
|---|---|---|
|
1. General Settings |
2. MBSFN Reference Signals |
3. MCH/PMCH |
Choice: 0 or 1 separated by commas
Length: 5 or 20 (Depends on Subframe Allocation)
Default: 1,...,1 (All 1's)
Enter 5 or 20 bits in length (1 = On, 0 = Off), separated by commas, to allocate the Multimedia Broadcast Multicast Service Single Frequency Network (MBSFN) on the Multicast Channel (MCH). For the Subframe Allocation 1 frame and 4 frames, the Allocation Bitmap length is configured 5 bits and 20 bits, respectively. (If you enter fewer than 5 or 20 bits, 0 is inserted to fill in the remaining bits. And, the pattern of 1's and 0's is repeated in the remaining bits.) The Allocation Bitmap assigns the bits according to the Uplink Downlink configuration selected. Uplink subframes are not allocated .
: The 5 bits length bitmap is applied as follows:
The first/leftmost bit defines the MBSFN allocation for subframe #3, the second bit for #4, third bit for #7, fourth bit for #8, and the fifth bit for #9. Uplink subframes are not allocated and the last bit is not used.
: The 20 bits length bitmap is applied as follows:
Starting from the first radio frame and from the first/leftmost bit in the bitmap, the allocation applies to subframes #3, #4, #7 , #8, #9 in the sequence of the four radio-frames. Uplink subframes are not allocated and the last four bits are not used.
For more detail, refer to 3GPP TS 36.331.
Choice: Degree | Complex
Default: Degree
Double-click or use the drop-down menu to set the Antenna Beam Configuration Mode to degree or complex.
|
|
Degree |
|
The antenna beam direction angle is set using degrees and antenna beam ports 5, and 7 to 14 are displayed. The Transmit Antenna Weight for Port 5 (and Ports 7 to 14) parameters are hidden. |
|
|
Complex |
|
The antenna beam pattern is specified by a complex value and the Transmit Antenna Weight for Port 5 (and Ports 7-14) parameters are displayed. Antenna Beam for Port 5 | 7| 8 | … | 14 parameters are hidden. Upon making this selection, the existing degree value is calculated to a complex value. |
This setting is applicable only when using a beam-forming transmission.
Range: –90 to +90 Degrees
Default: 0
Coupling: Visible when Antenna Beam Configuration Mode is set to Degrees and UE-Specific Reference signal state (DM-RS) is .
The number of ports displayed is dependent on the antenna configuration and the Transmit Antenna Port setting.
Enter an antenna beam main lobe direction value. When the value is entered, the antenna weight is calculated.
This is only applicable when Beam-forming is the transmission type.
When Complex is selected as the Antenna Beam Configuration Mode, the entered value for this setting is automatically calculated to a complex value that is used by the Transmit Antenna Weight Port parameter. But the Transmit Antenna Weight Port complex value is not converted to degrees.
Range: 0 or 1 separated by commas
Default: 1
Enter 0 or 1 (1 = On, 0 = Off) separated by commas to assign the PMCH to the physical antenna port number. The comma separate length depends on the total number of antennas that you specify.
Example: If the Total Number of Antennas = 4 and the Antenna Mapping for Port 4 = [1, 1, 1, 1], then PMCH (Physical Multicast Channel) is assigned to all antennas (port 0 to 3).
Range: 0 to (number defined in Number of HARQ Processes -1)
Enter the numbers of individual HARQ processes, separated by commas (for example, 1,2,3) or a range of HARQ processes ( for example, 1-3) to enable specific HARQ processes.
The number of available HARQ processes is defined in the Number of HARQ Processes parameter and this parameter.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to set the Auto MasterInformationBlock State for BCH. If the ”Auto MasterInformationBlock” mode is On, the BCH data source will use the system configuration for the channel code.
The content of a Master Information Block contains 24 bits.
Master Information Block Bits:
|
Bit #0~2: |
DL-Bandwidth |
Enumerated {n6, n15, n25, n75, n100} |
|
Bit #3: |
Phich-Duration |
Enumerated {normal, extended} |
|
Bit #4~5: |
Phich-Resource |
Enumerated {oneSixth, half, one, two} |
|
Bit #6~13: |
SystemFrameNumber |
Bit string {Size(8)} |
|
Bit #14~23: |
Spare |
Bit string {Size(10)} |
Range:
1 to 3 for number of downlink resource blocks > 10 (see System Bandwidth)
2 to 4 for number of downlink resource blocks ≤ 10 (see System Bandwidth)
Displays the control format indicator (CFI) for each subframe in the selected PCFICH channel, separated by commas.
These values correspond to the number of OFDM symbols used for transmission of the PDCCH in each subframe and are set in the PDCCH Allocations cell.
Displays the identifying number of the selected channel.
Choice: On | Off
Default: Off
Double-click or use the drop-down menu to enable or disable the carrier indicator field (CIF) presence state in the PDCCH DCI formats.
Range: 0-2 for number of antenna ports = 2 and Number of Layers = 2
0-3 for number of antenna ports = 2 and Number of Layers = 1
0-15 for number of antenna ports = 3 or 4 and Number of Layers = 1, 2, or 4
Default: 0
Enter a value for the Codebook Index when Spatial Multiplexing is selected as the diversity method. See 3GPP TS 36.211 for more information.
Choice: Off | On
Default: On
This parameter applies to BCH, and DL-SCH channels.
Double-click or use the drop-down menu to turn the coding state On or Off.
Choice: PN9 | PN15 | User Defined Bits
Default: PN9
This parameter applies to DCI, BCH, and MCH channels. Use the Data Source Selection dialog box to select PN9, PN15, or User Defined Bits to use for the data in the transport block.
Use the Data Source Selection dialog box to select PN9, PN15, or to use for the data in data stream 0 (transport block 0) of DL-SCH.
Refer to 3GPP TS 36.211 and 36.212.
Use the Data Source Selection dialog box to select PN9, PN15, or to use for the data in data stream 1 (transport block 1) of DL-SCH.
Refer to 3GPP TS 36.211 and 36.212.
Displays the Data Source of the DCI channel.
Choices: Format 0 | Format 1 | Format 1A | Format 1B | Format 1C | Format 1D | Format 2 | Format 2A | Format 2B | Format 2C | Format 2D | Format 3 | Format 3A
Default: Format 1A
Coupling: Whether this setting is active and what DCI Formats are available depends on Transmission Mode, Virtual Resource Block Type, Resource Allocation Type and Diversity Method.
Double-click or use the drop-down menu to set the DL-SCH DCI format.
The available DCI Format depends on Transmission Mode, Virtual Resource Block Type, Resource Allocation Type and Diversity Method.
When it is read only, the DCI Format is automatically selected by the DL-SCH and system settings.
Refer to 3GPP TS 36.211, 36.212, and 36.213.
Displays the related DL-SCH of the DCI channel.
Click the button in this cell to open the PDCCH Transmission Configuration dialog box. Refer to DL-SCH PDCCH Transmission Configuration dialog box.
Click the button in this cell to open the PDCCH Transmission Configuration dialog box. Refer to UL-SCH PDCCH Transmission Configuration dialog box.
Click the button in this cell to open the PDCCH Transmission Configuration dialog box. Refer to UL-SCH PDCCH Transmission Configuration dialog box.
Click the button in this cell to open the PDCCH Transmission Configuration dialog box. Refer to RACH PDCCH Transmission Configuration dialog box.
Click the button in this cell to open the PDCCH Transmission Configuration dialog box. Refer to Uplink Power Control PDCCH Transmission Configuration dialog box.
Click the button in this cell to open the PDCCH Transmission Configuration dialog box. Refer to User Defined PDCCH Transmission Configuration dialog box.
Display the DCI payload size. The DCI payload size is related with the system bandwidth and DCI format.
The first number indicates the number of information bits while the second number indicates the number of padding bits. Refer to the 3GPP technical standards for more information.
Click to enable or disable the DCI channel.
The physical downlink control channel carries
scheduling assignments and other control information. A physical control
channel is transmitted on an aggregation of one or several consecutive
control channel elements (CCEs), where a control channel element corresponds
to 9 resource element groups. The number of resource-element groups not
assigned to PCFICH or PHICH is
. The CCEs available in the system are numbered from 0 and
, where
. The PDCCH supports
multiple formats as listed in the table below. A PDCCH consisting of n consecutive CCEs may only start on
a CCE fulfilling
,
where i is
the CCE number.
Click the button in this cell to open the DL-SCH PDCCH Tx Setting window.
Supported PDCCH formats
Choice: DL-SCH | Manual
Default: DL-SCH
Double-click or use the drop-down menu to set the transmission couple state between DCI and DL-SCH
Choice: Off | Tx Diversity | Spatial Multiplexing
Default: Off
Double-click or use the drop-down menu to select a diversity method. The Tx Diversity and Spatial Multiplexing selections are available only for multiple antenna configurations. You can select a simulated multiple antenna configuration (M x 2 or M x 4) when you start the software, use a Quick Setup, configure a multiple antenna setup using actual hardware with the System Configuration Wizard, or define multiple antennas in the Total number of Antennas field in the Downlink Setup node.
Refer to Tutorials for MIMO hardware configurations.
Range: 0.001–1.000
Default: 0.931
Enter the maximum coding rate for the selected MCH channel.
If the effective channel code rate is higher than 0.931, the signal may not be successfully decoded. The effective channel code rate is defined as the number of downlink information bits (including CRC bits) divided by the number of physical channel bits on the channel.
When the coding rate of the channel is higher than the maximum coding rate, an error message is displayed.
For more information, refer to 3GPP TS 36.213.
Range: 0 to 255 (Integer)
Default: 0
Enter a value for the Multimedia Broadcast Multicast Service Single Frequency Network Reference Signal (MBSFN) Area ID which identifies the MBSFN Area. It is used for the scrambling of the MBSFN Reference Signals and the Physical Multicast Channel (PMCH). Refer to 3GPP TS 36.211 and TS 36.331.
Range: -60.000 to 20.000
Default: 0.000 dB
Enter a value for the power of the Multimedia Broadcast Multicast Service Single Frequency Network Reference Signal (MBSFN RS) in dB. See Output Power Calculation (Downlink) for a description of how the software applies your power settings.
Choices:Off | 0 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 | 11 | 12 |13 |14 | 15 | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 | 24 | 25 | 26 | 27 | 28
Default: 0
Enter a value to set the MCS index of MCH.The MCS index defines the modulation order, and TBS index. Refer to Table 7.1.7.2.1-1 ( 3GPP TS 36.213) which specifies the permissible combinations of transport block size, resource allocation, and modulation type that are available for transmission.
When the MCS Index is Off, the Modulation and TBS Index parameters are active and can be user-defined.
Where MCS Index = 0 to 29, the Modulation and TBS Index are automatically decided by the software.
Refer to 3GPP TS 36.212, 36.213, and 36.331.
Choice: Off | 0 | 1 | … | 26 | 27 | 28 (Modulation and TBS Index Table 1)
Off | 0 | 1 | … | 26 | 27 (Modulation and TBS Index Table 2)
The choice value selection is dependent on the UE Category selection.
Default: 0
Coupling: With MCS Index set to a value, Modulation and TBS Index are read only and set by the software.
Set the MCH MCS index by either double clicking in the cell or using the drop-down menu to make the selection.
For more information, refer to 3GPP TS 36.212 and 36.331.
Choice: QPSK | 16QAM | 64QAM
When the MCS Index is off, double-click or use the drop-down menu to select modulation type for the subframe.
For MCH: Where the MCS Index = 0 to 28, both the TBS Index and the Modulation are automatically set by the software and not editable.
Choice: QPSK | 16QAM | 64QAM (Modulation and TBS Index Table 1)
QPSK | 16QAM | 64QAM | 256QAM (Modulation and TBS Index Table 2)
Default: QPSK
Coupling: Read only and set by the software until MCS Index is set to Off.
When active, double-click in the cell or use the drop-down menu to make the selection.
For more information, refer to 3GPP TS 36.211, 36.213 and 36.311.
Choices: Table 1 | Table 2
Default: Table 1
Double-click or use the drop-down menu to select the Modulation and TBS Index Table for the PDSCH.
|
|
Table 1 |
|
per 3GPP TS 36.213 Modulation and TBS index table 7.1.7.1-1 |
|
|
Table 2 |
|
per 3GPP TS 36.213 Modulation and TBS index table 7.1.7.1-1A |
With the table selection, there is a relationship between the following DL-SCH Tx sequence window settings:
MCS Index 0/1
Modulation 0/1
TBS Index 0/1
For more information, refer to 3GPP TS 36.213.
Choice: Table 1 | Table 2
Default: Table 1
Double-click or use the drop-down menu to select the Modulation and TBS Index Table for the PMCH.
|
|
Table 1 |
|
per 3GPP TS 36.213 Modulation and TBS index table 7.1.7.1-1 |
|
|
Table 2 |
|
per 3GPP TS 36.213 Modulation and TBS index table 7.1.7.1-1A |
With the table selection, there is a relationship between the following MCH/PMCH settings:
For more information, refer to 3GPP TS 36.213.
Displays the name (type) of the selected channel.
BCH = Broadcast Channel
CFI = Control Format Indicator
HI = HARQ Indicator Channel
DCI = Downlink Control Information
DL-SCH = Downlink Shared Channel
MCH = Multicast Channel
Choice: 1 | 2
Default: 1
Double-click or use the drop-down menu to select the number of Codewords.
When you select Tx Diversity as the Diversity Method, the Number of Codewords is automatically set to the number of downlink antenna ports.
When you select Spatial Multiplexing as the Diversity Method, you can set the number of codewords to 1, 2. The maximum number of codewords is less than or equal to the number of number of layers.
Range:
1 to 4 (UL/DL Configuration 0)
1 to 7 (UL/DL Configuration 1)
1 to 10 (UL/DL Configuration 2)
1 to 9 (UL/DL Configuration 3)
1 to 12 (UL/DL Configuration 4)
1 to 15 (UL/DL Configuration 5)
1 to 6 (UL/DL Configuration 6)
The value you enter sets the number of available hybrid automatic repeat request (HARQ) processes and defines the interval (number of subframes) between retransmissions. Use the Assigned Processes parameter to enable HARQ processes. In the current LTE TDD signal studio it only supports one HARQ process for the DL-SCH. The value of the Number of HARQ Processes is dependent on the UL/DL configuration.
The number of available HARQ processes is defined in the Assigned Processes parameter and this parameter.
Choice: 1 | 2 | 3 | 4
Default: 1
Double-click or use the drop-down menu to select the number of layers.
When you select Tx Diversity as the Diversity Method, the number of layers is automatically set to the number of downlink antenna ports.
When you select Spatial Multiplexing as the Diversity Method, you can set the number of layers to 1, 2, 3, or 4. The maximum number of layers is less than or equal to the number of downlink antenna ports.
Range: 1 to 2 (Integer)
Default: 2
Enter the number of PDCCH symbols (Non-MBSFN Region Length) for all of MBSFN subframe. Where there is a 1 or 2 antenna configuration and N_DL_RB > 10, the parameter range is 1 to 2. Otherwise the value is 2. Where the MCH State is on and some MBSFN subframes are assigned, the Number of PDCCH Symbols (Non-MBSFN Region Length) is coupled to the PDCCH Allocations in DCI for the MBSFN subframe(s).
In case N_DL_RB <= 10, the Number of PDCCH Symbols is only allowed 2.
In case N_DL_RB > 10 and 1 or 2 cell-specific antenna ports, this Number of PDCCH Symbols is allowed 1 or 2.
In case N_DL_RB > 10 and 4 cell-specific antenna ports, the Number of PDCCH Symbols is only allowed 2.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn the OCNG (OFDMA channel-noise generation) for PDCCH on or off. ONCG is allocated on empty resource element groups in the control channel region (PDFICH/PDCCH/PHICH/Cell-Specific RS). OCNG is pseudo-random data and does not include transport channel coding. For more information, refer to 3GPP TS 36.521-1.
|
On |
Unallocated control region is filled with OCNG. When carrier aggregation is used with PHICH, the PDCCH is padded with resource element groups as OCNG. |
|
Off |
Unallocated control region is not filled with OCNG. |
Refer to 3GPP TS 36.521-1.
Choice: Off | -6 dB | -4.77 dB |-3 dB |-1.77 dB | 0 dB | 1 dB | 2 dB | 3 dB
Default: 0 dB
Double-click or use the drop-down menu to select the PDSCH relative power. This power value is applied to all allocations that belong to the UE.
The P_A value selected is applied to the Power parameter.
For more details, refer to 3GPP TS 36.213 and 36.331.
Range: 1 to 1920
Default: 24
Enter a value for the payload size in bits. Refer to the 3GPP technical standards for more information.
Range:
1 to 3 for number of downlink resource blocks > 10 (depends on System Bandwidth)
2 to 4 for number of downlink resource blocks ≤ 10 (depends on System Bandwidth)
Default: 1,1,1,1,1,1,1,1,1,1
For DCI channels, enter the number of OFDMA symbols used for PDCCH (non-MBSFN subframes) in each subframe, separated by commas. Ten inputs for each subframe are available, as described in 3GPP TS 36.211.
If the MCH (Multicast channel) state is set to on and the MBSFN subframe is assigned, the corresponding PDCCH subframes are updated with the number of symbols for MBSFN subframes set by the parameter, Number of PDCCH Symbols, in MCH.
Choice: Common | UE Specific
Default: UE Specific
Double-click or use the drop-down menu to set the search space of the PDCCH channels.
PDCCH Search Space is only available to be set when the current component cell is set to be the Primary Cell component carrier. For secondary cell component carriers, this parameter is inactive.
Choice: UE Port 0 | UE Port 1
Default: UE Port 0
Double-click or use the drop-down menu to set the UE Tx Antenna for the selected DCI channel.
Range: 1 to 4
Default: 3
Enter the starting OFDM symbol of the PDSCH for the concerned SCell.
See 3GPP TS 36.211, 36.212, 36.213 and 36.331 for more information.
Choice: 1/6 | 1/2 | 1 | 2
Default: 1/6
Double-click or use the drop-down menu to set the allocation value for the selected PHICH channel.
The software sets the PHICH Maximum Group Number, based on the PHICH Allocation value.
The PHICH carries the hybrid-ARQ ACK/NACK. Multiple PHICHs mapped to the same set of resource elements constitute a PHICH group, where PHICHs within the same PHICH group are separated through different orthogonal sequences.
A PHICH resource is identified by the
index pair
, where
is the PHICH group number and
is the orthogonal sequence index within
the group.
For
frame structure type 1, the number of PHICH groups
is constant in all subframes and given by
where
is provided by higher layers. The index
ranges from 0
to
.
Range: -60 to 20 dB
Default: 0 dB
Enter a power level in dB for PHICH BPSK symbols. See Output Power Calculation (Downlink) for a description of how the software applies your power settings.
Choice: Normal | Extended
Default: Normal
Double-click or use the drop-down menu to set the PHICH duration for the selected HI channel as defined in 3GPP TS 36.211
Display the maximum number of PHICH groups in each subframe.
The maximum number of PHICH groups is related to Uplink and Downlink Configuration and PHICH Allocation.
Multiple PHICHs mapped to the same set of resource elements constitute a PHICH group, where PHICHs within the same PHICH group are separated through different orthogonal sequences. See 3GPP TS 36.211 for details.
Choice: STD | ETM
Default: STD
Set the Mi definition mode of PHICH channel. if the PHICH Mi definition mode is ETM, all the Mi will be set to 1. See 3GPP TS 36.141 for detail.
Range: -60.000 to 20.000 dB
Default: 0.000 dB
Enter a power level in dB for the PMCH (Physical Multicast Channel). See Output Power Calculation (Downlink) for a description of how the software applies your power settings.
Range: -60.000 to 20.000 dB
Default: 0.000 dB
Enter a power level in dB for the selected channel. See Output Power Calculation (Downlink) for a description of how the software applies your power settings.
Range: -60.000 to 20.000 dB
Default: 0.000 dB
For a UE-specific reference signal, enter a power level in dB. This parameter is only available when UE-Specific Reference signal state is On. See Output Power Calculation (Downlink) for a description of how the software applies your power settings.
Choice: Without CDD | Large-delay CDD
Default: Without CDD
Double-click or use the drop-down menu to select a cyclic delay diversity (CDD) precoding method when Spatial Multiplexing is selected as the diversity method in Diversity Method field. See 3GPP TS 36.211 for detailed information about precoding.
Range: 0 to 7 (Integer)
Default: 0
Enter a value for the MBSFN subframe offset unit in radio frames. The upper range must be less than or equal to the (Radio Frame Allocation Period - 1) or 7.
Radio-frames that contain MBSFN subframes occur when SFN (mod Radio Frame Allocation Period) = Radio Frame Allocation Offset is satisfied.
Refer to 3GPP TS 36.331 for more details.
Choice: 1 frame | 2 frames | 4 frames | 8 frames | 16 frames | 32 frames
Default: 1 frame
Double-click or use the drop-down menu to set the radio frame allocation period. Radio-frames that contain MBSFN subframes occur when the equation Single Frequency Network (SFN) mod Radio Frame Allocation Period = Radio Frame Allocation Offset is satisfied. 4 frames are available only if the Radio Allocation Period is 4, 8, 16, or 32.
Refer to 3GPP TS 36.331.
Choice: 6 |15 |25 | 50 | 75 | 100
Display the PMCH resource block size which is the same as maximum system resource blocks size as follows:
6RB (1.4MHz), 15RB (3MHz), 25RB (5MHz), 50RB (10MHz), 75RB (15MHz) and 100RB (20MHz).
This is a read only parameter.
Refer to 3GPP TS 36.213.
Choice: Type 0 | Type 1 | Type 2
Default: Type 2
Double-click or use the drop-down menu to set the resource allocation type for the DL-SCH.
Range: 1 to 65523 (for C-RNTI), 65535 (for SI-RNTI), 65534 (0xFFFE) (for P-RNTI)
Default: 1
Enter a value for the Radio Network Temporary Identifier (RNTI).
Refer to 3GPP TS 36.211 and 36.321.
Choice: SI-RNTI (System Information) | C-RNTI (Dedicated Traffic) | P-RNTI (Paging Information)
Default: C-RNTI (Dedicated Traffic)
Double-click or use the drop-down menu to select the RNTI type.
Cell RNTI (C-RNTI) and System Information RNTI (SI-RNTI) are supported.
RNTI = 1 to 65523 case, works for C-RNTI.
RNTI = 65535 case, works for SI-RNTI.
RNTI = 65534 case, works for P-RNTI
The SI-RNTI is used for setting SIB transmissions on DL-SCH that can be set manually. Refer to RNTI.
Choice: Auto | Manual
Default: Auto
Double-click or use the drop-down menu to set the RV Index Configuration for the selected DL-SCH channel.
In Auto mode, the RV Index for PDSCH's will be defined by RV Index Sequence. PDSCH will use the first element in RV Index Sequence by default and the index will increase when Retransmission state is on.
In Manual mode, RV Index will be set manually in DL-SCH TX Sequence Dialog and independent with each Retransmission. RV Index Configuration changes to Manual when RNTI Type is SI-RNTI or P-RNTI.
When RNTI Type = P-RNTI, the following parameters are effected:
Transmission Configuration parameter's DL-SCH Tx sequence dialog box parameters are changed as follows:
N_1A_PRB becomes available and is set to 2.
Block Size 0 is set to 32.
Modulation Type is QPSK.
Channel Setup node, the following parameters are changed:
1. General Settings > Transmission Mode will be set to 2, if 2 or 4 antennas are selected.
3. Transmission Settings > RV Index Configuration is Manual (not editable).
Range of sequence length: 1 to 16
Range of each value: 0 to 3
Default: 0,2,3,1
Enter the numbers of individual RV Index Sequence, separated by commas (for example, 1,2,3).
Range: 0 to 7
Default: 0
Enter the serving cell index which cell signals the downlink allocations and uplink grants for the concerned SCell.
Refer to 3GPP TS 36.211, 36.212, 36.213, and 36.331.
Choice: On | Off
Default: On
This parameter applies to DCI, BCH, CFI, HI, and MCH channels.
Double-click or use the drop-down menu to turn scrambling on or off.
Range: 0 to 255
Default: 0
Set Auto MasterInformationBlock to On to make this parameter active.
This is the start number of the SFN (8 bits in binary, 2 bytes in hexadecimal).
If Auto MasterInformationBlock = On, SFN is incremented every 40 subframes (40 ms) and used for part of the payload data. For example, If you generate a 80 ms signal with Auto MasterInformationBlock set to On, the initial 40 ms of the SFN = SFN Start Number and the next 40 ms of the SFN = SFN Start Number +1.
If Auto MasterInformationBlock = Off, SFN is not incremented and the fixed value SFN Start Number is used for part of the payload data in each 40 subframes.
Refer to the 3GPP TS36.331.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn the channel On or Off.
For :
On: Both channel MBSFN Reference Signals and MCH (PMCH) are on.
Off: Both channel MBSFN Reference Signals and MCH (PMCH) are off.
For MCH, where the cyclic prefix (CP) is set to (normal CP) and the MCH State is : the Non-MBSFN region in the MBSFN subframe is configured to normal CP and the MBSFN region in the MBSFN subframe is configured to extended CP.
For more detail, refer to 3GPP TS 36.211.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn the UE Specific Reference Signal state on or off. This is only available when Transmission Mode is 7 or 8.
Choice: 1 frame | 4 frames
Default:1 Frame
Double-click or use the drop-down menu to set the subframe allocation for MBSFN within the radio frame allocation period defined by the two parameters: Radio Frame Allocation Period and Radio Frame Allocation Offset. 4 frames are available only if the Radio Allocation Period is 4, 8, 16, or 32.
Choices:Off | 0 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 | 11 | 12 |13 |14 | 15 | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 | 24 | 25 | 26
Default: 5
Enter a value for the TBS index for the MCH/PMCH. The range of available values depends on the modulation type: QPSK (0 to 10), 16QAM (10 to 19), 64QAM (19 to 26). Where the MCS Index = 0 to 28, both the TBS Index and the Modulation are automatically set by the software and not editable.
|
|
MCS/TBS Index Value |
Status of Coupled Parameters |
|---|---|---|
|
|
MCS Index = 0 to 28 |
Modulation and TBS Index are automatically set by the software |
|
|
MCS Index = Off |
Modulation and TBS Index are settable by the user. |
|
|
TBS Index = 0 to 26 |
TB Size is automatically set by the software. |
|
|
TBS Index = Off |
TB Size is settable by the user. |
Refer to 3GPP TS 36.213.
Choice: Off | 0 | 1 | 2 | … | 26 (Modulation and TBS Index Table 1)
Off | 0 | 1 | 2 | … | 33 (Modulation and TBS Index Table 2)
The choice value selection is dependent on the UE Category selection.
Default: 0
Coupling: Read only and set by the software until MCS Index is set to Off.
When active, double click in the cell or use the drop-down menu to make the selection.
For more information, refer to 3GPP TS 36.211, 36.213 and 36.311.
Range 1 to 75376 (Integer)
Enter a value for the transport block size for the MCH/PMCH.
For more detail, refer to 3GPP TS 36.213.
Range: 1 to 75376 (Modulation and TBS Index Table 1)
1 to 97896 (Modulation and TBS Index Table 2)
The maximum range value is dependent on the UE Category selection.
Coupling: Read only and set by the software until TB Size is set to Off
When active, enter the size of the transport block.
For more information, refer to 3GPP TS 36.211, 36.213 and 36.311.
Choice:
Port 5 ( Transmission Mode 7 case)
Port 7 | Port 8 (Transmission Mode 8 to 10 and Total Number of Antennas is 1)
Port 7 | Port 8 | Port 7 - 8 (Transmission Mode 8 and Total Number of Antennas is 2 to 8)
Port 7 | Port 8 | Port 7 - 8 (Transmission Mode 9 to 10 and Total Number of Antennas is 2)
Port 7 | Port 8 | Port 7 - 8 |Port 7 - 9 | Port 7 - 10 (Transmission Mode 9 to 10 and Total Number of Antennas is 4)
Port 7 | Port 8 | Port 7 - 8 | Port 7 - 9 | Port 7 - 10 | Port 7 - 11 | Port 7 - 12 | Port 7 - 13 | Port 7 - 14 (Transmission Mode 9 to 10 and Total Number of Antennas is 8)
Coupling: This setting is active when UE-Specific Reference signal state (DM-RS) is .
Double-click or use the drop-down menu to set Transmission Antenna Port for UE Specific Reference Signal.
In case of PDCCH Allocations = 4 (1.4MHz System Bandwidth), Port 5 is not available to select.
Refer to 3GPP TS 36.211, 36.212, and 36.213.
Default: 0.0+0.0j, 1.0+0.0j
Coupling: Visible when Antenna Beam Configuration Mode is set to Complex and UE-Specific Reference signal state (DM-RS) is .
The number of ports displayed is dependent on the antenna configuration and the Transmit Antenna Port setting.
Enter a Transmission Antenna Weight complex number(s) for the UE Specific Reference Signal for the corresponding antenna port. When Total Number of Antennas is greater than one, enter a complex array such as "1.0+0.0j, 1.0+0.0j".
When Complex is selected as the Antenna Beam Configuration Mode, the existing value for the Antenna Beam for Port parameter is automatically calculated to a complex value that is available for use by this parameter (Transmit Antenna Weight Port). But the Transmit Antenna Weight Port complex value is not converted to degrees.
Click the
button in this cell to open the DL-SCH Tx sequence window.
Click the
button in this cell to open the
PHICH Tx
configuration window.
Range: 1 frame to Waveform Generation Length, Max 16 frames
Default: 1 frame
Set the length of transmission configuration. The definition of transmission configuration of SCH and DCI will be repeated to the end of the Waveform Generation Length. Refer to Waveform Structure (Long).
If the Waveform Generation Length parameter is set less than the Transmission Configuration Length, the value of Transmission Configuration Length is changed to be ≤Waveform Generation Length. In summary, the relation between Transmission Configuration Length and Waveform Generation Length is that the Transmission Configuration Length ≤Waveform Generation Length. Refer to the Waveform Generation Length parameter.
|
|
Channel |
Transmission Configuration Length |
Default Value |
|---|---|---|---|
|
Downlink |
DL-SCH 1 - 8 |
The value is available to set 1 -16 Frames With the following rule: Transmission Configuration Length ≤Waveform Generation Length |
1 Frame |
|
|
DCI 1 - 8 |
The value is automatically set to same value corresponding DL-SCHs. |
Same as UL-SCH |
|
|
DCI 9 - 12 |
The value is automatically set to same value as Waveform Generation Length. |
1 Frame |
Example: Where the Transmission Configuration Length is set to 2, Frames #0 and #1 configurations (Sequences #1 and #2) will be repeated while generating
SCH.
Choice:
1 | 7 | 8 | 9 | 10 (for single antenna)
2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 (2 or 4 antennas)
7 | 8 | 9 | 10 (8 antennas)
Default: 1
Double-click or use the drop-down menu to set the Transmission Mode for the selected DL-SCH channel.
The following table shows the transmission scheme for each Transmission Mode:
|
Transmission Mode |
Transmission Scheme of PDSCH |
|---|---|
|
1 |
Signal Antenna Port, Port 0 |
|
2 |
Transmit Diversity |
|
3 |
Open-Loop Spatial Multiplexing |
|
4 |
Close-loop Spatial Multiplexing |
|
5 |
Multi-user MIMO |
|
6 |
Close-loop Spatial Multiplexing with Single Layer |
| 7 | Single Antenna Port (Port 5) |
| 8 | Single Antenna Port (Port 7 or 8) / Dual Layer Transmission (Ports 7 or 8) |
| 9 | Single Antenna Port (Port 7 or 8) / Up to 8 Layer Transmission (Ports 7 to 14) |
| 10 |
In case of PDCCH Allocations = 4 with 1.4 MHz system bandwidth, transmission mode 7: Single Antenna Port (Port 5) is not available to select.
Transmission mode 8 is not available, when extended cyclic prefix is used in the downlink.
Refer to 3GPP TS 36.212 and 36.213.
Choice: MCS | Manual
Default: MCS
Double-click or use the drop-down menu to select the PDSCH Transmission Setting Mode.
In MCS mode, the modulation and transport block size of each transmission is determined by the MCS index according to the table in 3GPP 36.213 7.1.7
Choices: 0 |1 | 2 | 3 | 4 | 5 | 6 (2 Layers) | 6 (4 Layers) | 7 (2 Layers) | 7 (4 Layers) | 8 | 9 (2 Layers) | 9 (4 Layers) | 10 (2 Layers) | 10 (4 Layers) | 11 (2 Layers) | 11 (4 Layers) | 12 (2 Layers) | 12 (4 Layers) | 13 (2 Layers) | 13 (4 Layers) | 14 (2 Layers) | 14 (4 Layers) | 15
Default: 15
Double-click or use the drop-down menu to set the UE Category for the corresponding DL-SCH.
Maximum number of supported layers for spatial multiplexing in the downlink is specified for each category respectively.
some UE Categories have two capabilities 2 layers and 4 layers.
UE Category defines a combined uplink and downlink capability.
UE Categories determine the maximum number of DL-SCH transport block bits that the UE is capable of receiving in a single transport block within a DL-SCH TTI. The UE categories for the DL-SCH channels are implemented according to the 3GPP standards as shown in the following table:
|
UE Category |
Maximum number of DL-SCH transport block bits received within a TTI1 |
Maximum number of bits of a DL-SCH transport block received within a TTI |
Total number of soft channel bits |
Maximum number of supported layers for spatial multiplexing in DL |
|---|---|---|---|---|
|
Category 02 |
1000 |
1000 |
25344 |
1 |
|
Category 1 |
10296 |
10296 |
250368 |
1 |
|
Category 2 |
51024 |
51024 |
1237248 |
2 |
|
Category 3 |
102048 |
75376 |
1237248 |
2 |
|
Category 4 |
150752 |
75376 |
1827072 |
2 |
|
Category 5 |
299552 |
149776 |
3667200 |
4 |
|
Category 6 |
301504 |
149776 (4 layers) 75376 (2 layers) |
3654144 |
2 or 4 |
|
Category 7 |
301504 |
149776 (4 layers) 75376 (2 layers) |
3654144 |
2 or 4 |
|
Category 8 |
2998560 |
299856 |
35982720 |
8 |
|
Category 9 |
452256 |
149776 (4 layers) 75376 (2 layers |
5481216 |
2 or 4 |
|
Category 10 |
452256 |
149776 (4 layers) 75376 (2 layers) |
5481216 |
2 or 4 |
|
Category 11 |
603008 |
149776 (4 layers, 64QAM) 195816 (4 layers, 256QAM) 75376 (2 layers, 64QAM) 97896 (2 layers, 256QAM) |
7308288 |
2 or 4 |
|
Category 12 |
603008 |
149776 (4 layers, 64QAM) 195816 (4 layers, 256QAM) 75376 (2 layers, 64QAM) 97896 (2 layers, 256QAM) |
7308288 |
2 or 4 |
|
Category 13 |
391632 |
195816 (4 layers) 97896 (2 layers) |
3654144 |
2 or 4 |
|
Category 14 |
391632 |
195816 (4 layers) 97896 (2 layers) |
3654144 |
2 or 4 |
|
Category 15 |
3916560 |
391656 |
47431680 |
8 |
1. During carrier aggregation operation, the DL-SCH processing capability can be shared by the UE with that of the MCH received from a serving cell. If the total eNB scheduling for DL-SCH and an MCH in one serving cell, for a given TTI, is larger than the defined processing capability, the prioritization between DL-SCH and MCH is left up to the UE implementation.
2. Within one TTI, a UE indicating category 0 shall be able to receive up to 1000 bits for a transport block associated with C-RNTI/Semi-Persistent Scheduling C-RNTI/P-RNTI/SI-RNTI/RA-RNTI and up to 2216 bits for another transport block associated with P-RNTI/SI-RNTI/RA-RNTI
For more information on UE Categories, refer to 3GPP TS 36.212 and 36.306.
Choices: 0 | 1 | 2 | … | 15
Default: 15
Set the UE category by double clicking in the cell or using the drop-down menu to select the category. The UE category determines the maximum number of bits in the MCH transport block.
For more information on the UE categories, refer to 3GPP TS 36.211, 36.212, 36.213, and 36.306.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn the UE Specific Reference Signal state on or off.
Choice: Localized | Distributed
Default: Localized
Double-click or use the drop-down menu to set the Virtual Resource Blocks Type for the Resource Allocation Type 2.
In the distributed allocation mode, the RB gap in the PDSCH will be valid and the RB size will be limited to the maximum number for the distributed type. See the Resource Allocation in 3GPP TS 36.213 for detailed information.