Real Time

Menu Bar and Tool Bar

Click an icon or a command in the menus shown below to view its description.

File

New

Open...

Save As...

Export Waveform Data

Recent Settings Files

Exit

View

Show Legacy Carrier

Control

Generate Waveform

Generate and Download

Update Hardware Settings

System

Change Hardware Connections

Run System Configuration Wizard

Tools

Status Window

Waveform Library...

Envelope Tracking...

Options

Help

Contents F1

Index

Search

API Reference

Software License Terms

Keysight Signal Studio Website

About

File

New sets the software to its standard initial state using the current hardware configuration. The window name changes to ClosedUntitled. Rename and save the new setup as a settings (.scp) file (saving only the software parameters), a GZIP format compressed settings file (.scpz), or as a Quick Setup (saving the current hardware and software parameters).

Open... opens a saved settings (.scp) or compressed settings (.scpz) file. Opening a settings file configures the waveform data parameters for use with the currently selected hardware.

If you have made parameter changes, a Closedwindow opens that enables you to save the settings to a file.

To use a settings file with a different hardware configuration, select Change Hardware Connections, or Run System Configuration Wizard and re-configure the hardware.

Use Quick Setups to open a saved setting that includes the hardware connection and software settings.

Settings files created for legacy (pre-release 9) carriers may generate a “Failed to import” error with the latest software. To support legacy settings files, use software version 7.5, available on the Keysight website.

Save as... saves the parameters configured in the Waveform Setup node and Instrument node to a specified settings file (.scp) or a GZIP format compressed settings file (.scpz). Settings files do not include the hardware configuration information such as LAN or GPIB settings for specific instruments listed in the Hardware node. 

If you need to save a specific hardware configuration together with the Waveform Setup and Instrument node settings, configure the hardware (System > Run System Configuration Wizard) then use the Save As Quick Setup button in the Quick Setups node. Note that the saved Quick Setup can only be accessed from the Quick Setups node of the user interface and is not saved as a .scp file.

When using Windows Vista operating system, saved settings files (*.scp) or compressed files (*.scpz) are not shared between different users of the same PC unless saved to a common location accessible to all users.

Export Waveform Data... saves an encrypted waveform file (.wfm or .fwfm file extension) to your PC. The file includes the settings and parameters from the Waveform Setup and Carrier nodes. This waveform file can then be downloaded and played in other licensed instruments or used with Keysight Advanced Design System (ADS) wireless libraries. 

Do not use spaces in the file name for an exported waveform. The underscore character is allowed.

The software gives you the option to export a high-resolution waveform (.fwfm file extension). This waveform type can then be imported into the library of another Signal Studio application, such as LTE/LTE-Advanced FDD, and used as a component in a multi-standard radio (MSR) waveform. To play the resultant MSR waveform, however, you must purchase Minor Enhancement Update (MEU), Option U02 or greater, for this Signal Studio product. Refer to Licenses for more information.

Refer to your signal generator's Programming Guide or the PXB's online help for information about downloading waveform files to your instruments.

Recent Settings Files displays the four most recent settings files that were opened with Open... or saved with Save as.... The settings file used most recently is added to the top of the list. Deleting a settings file does not immediately remove it from the list. Selecting a deleted settings file displays an error and then removes the file from the list.

If you have changed hardware parameters, but have not changed waveform setup parameters, you are not prompted to save changes when closing or exiting the software. To save hardware parameter changes, you must use the Save As Quick Setup button.

Exit stops and closes the software. If you made any waveform setup changes, a dialog box opens asking if you want to save the changes as a quick setup before exiting. The Closedclose button performs the same function as selecting Exit.

View

Show Legacy Carrier allows you to control whether or not legacy carriers appear when clicking the Add Carrier button. The checkmark indicates legacy carriers are available for use. ClosedView image.

Control

Generate and Download generates and downloads a waveform to the connected instrument(s). 

When a power-sensitive DUT is connected to the instrument, ensure that the RF power is off before downloading a waveform.

Agilent N5106A PXB Baseband Generator and Channel Emulator

If the software displays an error message when you attempt to download a waveform to the PXB, see Instrument Problems in the Troubleshooting section.

To download a waveform to the Agilent N5106A PXB, perform the following procedure:

  1. On the PXB, set up and load a configuration with the appropriate capabilities for the waveform you intend to play. The configuration must include at least one baseband generator (BBG). Refer to the PXB online documentation.

  2. Start Signal Studio and connect to the PXB using the Configuration Wizard. If you are running the Signal Studio software on the PXB’s internal PC, use ”localhost” in the Hostname/IP Address field in Step 4 of the System Configuration Wizard. If you are running Signal Studio on an external PC connected to the PXB, use the IP address or hostname (Machine Name) of the PXB in the Hostname/IP Address field. To find the PXB’s hostname (Machine Name) or IP address click System > Product Information in the PXB user interface.

  3. Set up waveform parameters in Signal Studio. Make sure you enter a name in the Waveform Name cell in the Waveform Setup node. This name identifies the waveform on the PXB.

  4. Click the Generate and Download button. The default location for the waveform file in the PXB is D:\Waveforms\ChannelN.

  5. On the PXB, click Load Waveforms and select the waveform file with the Waveform Name from Step 3.

  6. On the PXB, click Download to download the waveform to the BBG.

  7. On the PXB, click Play to play the waveform.

Keysight E6607 EXT Wireless Communications Test Set

To avoid causing the EXT to timeout during the download process,.verify the EXT's triggering mode is set to Free Run.

If the software displays an error message when you attempt to download a waveform to the EXT see Instrument Problems in the Troubleshooting section.

To download a waveform to the Keysight E6607 EXT perform the following procedure:

  1. On the EXT set up and load a configuration with the appropriate capabilities for the waveform you intend to play. Refer to the EXT online documentation. 

  2. Start Signal Studio and connect to the EXT using the Configuration Wizard. If you are running the Signal Studio software on the EXT, use “localhost” in the Hostname/IP Address field in Step 4 of the System Configuration Wizard. If you are running Signal Studio on a PC connected to the EXT, use the IP address or hostname of the EXT in the Hostname/IP Address field. To find the EXT's hostname or IP address click System > Product Information in the EXT user interface.

  3. Set up waveform parameters in Signal Studio. Make sure you enter a name in the Waveform Name cell in the Waveform Setup node. This name identifies the waveform on the EXT.

  4. Click the Generate and Download button. The default location for the waveform file in the EXT is D:\NVARB. 

Generate Waveform generates a waveform. Use this function to check for waveform errors before downloading or exporting the waveform.

Update Hardware Settings sends the current hardware configuration to the connected instrument(s). If the configuration is not received by the instrument, an error message appears.

System

Change Hardware Connections opens ClosedStep 3 of the System Configuration Wizard, where you can select a previously saved hardware configuration, or define and save a new hardware configuration.

Run System Configuration Wizardenables you to configure your system component connections and save the hardware configuration for later use. Use the System Configuration Wizard to set up a new instrument connection; use Quick Setups to save a new setup or select a saved setup that includes hardware connections and software settings.

Tools

Status Window opens and closes the Status Window.  

Waveform Library...opens the Library Manager window.

Envelope Tracking... opens the Envelope Tracking Control window.

Options enables or disables the Closedwelcome dialog display. 

Help

Contents opens the Help system and displays the table of contents.

F1 opens the Help system and displays the table of contents.

Index opens the Help system and displays the Index.

Search opens the Help system and displays the search utility.

API Reference opens a Help system for the API programming commands and their descriptions.

Software License Terms displays a description of the licensing terms agreement for Keysight's Signal Studio software.

Keysight Signal Studio website opens a webpage of all the Signal Studio products and their available options.

About displays the version and release date of the software.