Installation Steps: 1 2 3 4 5 6 7
The Microsoft .NET Framework versions may come pre-installed with your Windows operating system. If the pre-installed .NET Framework versions are not the same versions as stated in the text below, you must install the required versions. Different versions of .NET Framework can simultaneously reside on the Windows operating system.
Ensure that you have Microsoft .NET Framework 4.6 installed on the Windows operating system (PC or Windows-based instrument) that is to receive the Test Case Manager software download. If they are already installed, proceed to Installation Step 3. If it is not installed, do the following:
Search the site for the required .NET Framework software.
Download and install the software.
If you get a security exception message when you try to open the software, consult your system administrator to resolve the problem.