Installation Steps: 1 2 3 4 5 6 7
To download the software onto your Windows operating system (PC or Windows-based instrument such as the PXB), you must have administrator status. If you receive an access denied message, consult your system administrator for the required permissions. See User Permissions.
If the PC in which Test Case Manager (TCM) is to be installed is also used as a floating license server for Keysight 89600 VSA software, version 14 or earlier, use the alternate procedure below.
Close all open software.
Click the link below to download the setup.exe file that steps you through the installation process.
At the prompt, select to install the software.