Installation Steps: 1 2 3 4 5 6 7
Ensure the signal generator is turned off.
Connect the signal generator to a computer using one of the following methods for instrument control:
LAN Network—connect both the signal generator and the computer to an external LAN network using standard LAN cables.
Crossover LAN—connect the signal generator directly to the computer using a crossover LAN cable. (You will need to configure your PC.)
GPIB—connect the signal generator directly to the computer using a GPIB cable.
If you are using the PXB as the controller, proceed to Installation Step 7.
Ensure the PXB is turned off.
Connect the PXB to the computer using one of the following methods for instrument control. See the PXB's online documentation for GPIB and LAN configuration information.
LAN Network—connect both the PXB and the computer using standard LAN cables.
Crossover LAN—connect the PXB directly to the computer (You will need to configure your PC and the PXB.)
GPIB—connect the PXB directly to the computer using a GPIB cable.