Overview

N290A/N5291A Systems

The N5290A (900 Hz to 110 GHz) and N5291A (900 Hz to 120 GHz with over range to 125 GHz) are broadband network analyzer systems that utilize compact, broadband remote heads.

These system are comprised of the following components:

2-Port System

4-Port System

170 GHz and 220 GHz 2-Port Systems

The N5291A can be extended above 120 GHz with the broadband 170 GHz and 220 GHz 2-port systems.

These systems are comprised of the following components:

 

The N5252A is a banded network analyzer solution that uses compact remote frequency extenders with the PXI based VNA, extending the frequency coverage from 60 GHz to 90 GHz.

In its standard configuration the N5252A consists of the following key components:

In this topic:

See Also

Keysight Double-Ended Torque Wrench for 1.0 mm Connectors (internet connection required)

Features

Capabilities

N5293A/95A Frequency Extender LED States

The following is a list of possible LED states:

See Also

Other Related Topics