Only the Main, Port Power, and Leveling & Offsets Power commands corresponding to the Scalar Mixer/Converter measurement class are documented here. The Attenuators commands are identical to the Attenuator commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtab on the graphic below.
Click here to view links to Power commands for all Measurement Classes.
| Main Tab Commands | |||
| Softkey | Sub-item | SCPI | |
| Power Level | SOURce:POWer[:LEVel][:IMMediate][:AMPLitude] DISPlay:GUI:POWer:SPIN:RESolution | ||
| RF Power | ON/OFF | OUTPut[:STATe] | |
| SMC Setup... (Scalar Mixer/Converter Measurement Class only) | |||
| Port Power Tab Commands | |||
| Softkey | Sub-item | SCPI | |
| Select | Port 1 | None |
|
| Port 2 | None |
||
| Port 3 | None |
||
| Port 4 | None |
||
| Port 1 Src2 | None |
||
| Source3 | None |
||
| Power Level | SOURce:POWer[:LEVel][:IMMediate][:AMPLitude] | ||
| Source State | AUTO | SOURce:POWer:MODE | |
| ON | SOURce:POWer:MODE | ||
| OFF | SOURce:POWer:MODE | ||
| Coupling | ON | SOURce:POWer:COUPle | |
| OFF | SOURce:POWer:COUPle | ||
| Leveling & Offsets Tab Commands | |||
| Softkey | Sub-item | SCPI | |
| Select | Port 1 | None |
|
| Port 2 | None |
||
| Port 3 | None |
||
| Port 4 | None |
||
| Port 1 Src2 | None |
||
| Source3 | None |
||
| Slope | ON/OFF | SOURce:POWer[:LEVel]:SLOPe:STATe | |
| Power Slope | SOURce:POWer[:LEVel]:SLOPe | ||
| Offset | SOURce:POWer:ALC[:MODE]:RECeiver:OFFSet | ||
| Limit | ON/OFF | SYSTem:POWer:LIMit:STATe | |
| Power Limit | SYSTem:POWer:LIMit | ||
ALC Hardware |
Internal |
||
Open Loop |
|||
|
|
||