Controls the settings of the front panel screen.
DISPlay: ANNotation | [:STATus] DISP:CHANnel: | NEW | STATe GUI | POWer | SPIN MEASure | DELete | FEED | MEMory | [:STATe] | MOVE | SELect | [:STATe] | TITLe | DATA | [:STATe] | TYPe | Y[:SCALe] | AUTO | RLEVel SHEet | ARRange | CATalog | LIST | NEW | STATe STATus | LOG | CLEar | SCPI TOOLbar | NEW | STATe UPDate | [:STATe] WINDow | ANNotation | LIMit | MARKer | COUPle | NUMBer | MEASre | NUMBer | RESolution | RESPonse | STIMulus | SIZE | STATe | SYMBol | VISible | [:STATe] | [TRACe] | SCOPe | [:STATe] | CATalog? | ENABle | FEED | SIZE | [STATe] | TABLe | INOise | ENABle | SNOise | ENABle | SPURious | ENABle | TITLe | DATA | [STATe] | TRACe | DELete | FEED | MNUMber | MOVE | NEW | SELect | [STATe] | TITLe | DATA | [:STATe] | X[:SCALe] | RLEVel | Y[:SCALe] | AUTO | BOTTom | COUPle | METHod | [STATe] | RLEVel | TOP | Y:AUTO | Y[:SCALe]
|
|
Click on a keyword to view the command details.
Blue keywords are superseded.
See Also
See an example using some of these commands
Applicable Models: All (Read-Write) Turns frequency information on the display title bar ON or OFF for all windows. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - turns frequency annotation ON. |
Examples |
DISP:ANN:FREQ ON |
Query Syntax |
DISPlay:ANNotation:FREQuency[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON (1) |
Applicable Models: All (Read-Write) Enables and disables error pop-up messages on the display. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - enables error pop-up messages |
Examples |
DISP:ANN:MESS:STAT ON |
Query Syntax |
DISPlay:ANNotation:MESSage:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON (1) |
Applicable Models: All (Read-Write) Turns the status bar at the bottom of the screen ON or OFF. The status bar displays information for the active window. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - turns status bar ON. |
Examples |
DISP:ANN ON |
Query Syntax |
DISPlay:ANNotation[:STATus]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
Last state that was set |
Applicable Models: All (Write-only) Places EXISTING measurements into pre-configured window arrangements. Overlay, Stack(2), Split(3), and Quad(4) creates new windows. To learn more, see Window Layout. |
|
Parameters |
|
<char> |
Window arrangement. Choose from:
|
Examples |
DISP:ARR CASC |
Query Syntax |
Not Applicable |
TILE |
Applicable Models: All (Read-only) Returns the existing Window numbers. Note: If there are no traces in the window, this query returns the "EMPTY" string. To read the window number of the selected trace, use Calc:Par:WNUM. |
|
Return Type |
String of Character values, separated by commas |
Example |
Two windows with numbers 1 and 2 returns: |
Not applicable |
Applicable Models: All (Write-only) Add a new channel according to the <int> parameter. |
|
Parameters |
|
<int> |
Add Type (optional) - 0: Trace + Channel (default), 1: Trace + Channel + Window |
Examples |
DISP:CHAN:NEW 1 |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Create or delete the specified channel. If set ON to an existing channel, just activate the channel. |
|
Parameters |
|
<ch> |
Channel Number. Default is 1. |
<ON | OFF> |
ON (or 1) - creates the channel OFF (or 0) - deletes the channel |
Examples |
DISP:CHAN2:STAT 1 display:channel3:state on |
Query Syntax |
DISPlay:CHANnel:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON (1) for Channel 1, OFF(0) for other channels |
Applicable Models: All (Read-Write) Specifies whether to disable or enable all analyzer display information in all windows in the analyzer application. Marker data is not updated. More CPU time is spent making measurements instead of updating the display. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - turns the display ON. |
Examples |
DISP:ENAB ON |
Query Syntax |
DISPlay:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Shows or hides the window which displays global pass/fail results. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - displays the pass/fail dialog OFF (or 0) - hides the pass/fail dialog |
Examples |
DISP:FSIG ON |
Query Syntax |
DISPlay:FSIGn? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Read-Write) Sets and returns the resolution of the front panel knob when it is used to adjust Source Power manually. |
|
Parameters |
|
<real> |
Spin resolution value (Real value). The range of acceptable values is 0.01 to 100. |
Examples |
DISP:GUI:POW:SPIN:RES 0.01 'Write - Every tick of the front panel knob will change the Power Level by 0.01 dBm. |
Query Syntax |
DISPlay:GUI:POWer:SPIN:RESolution? |
Return Type |
Real |
0.1 |
Applicable Models: All (Write-only) Deletes the trace associated with the specified measurement number. Note: The measurement is not deleted. This command does the reverse of DISP:MEAS:FEED. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
Examples |
DISP:MEAS:DEL |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Write-only) This command creates a new trace in the specified window and connects the trace to measurement which results in the trace displaying the data from measurement. |
|
Parameters |
|
<mnum> |
Measurement number for the measurement. If unspecified, <mnum> is set to 1. |
<wnum> |
Display the measurement in a specified Window number. The window must be turned on. In addition, a window number must be specified. The range is 1 to 500. |
Examples |
DISP:MEAS2:FEED 10 |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Turns the memory trace ON or OFF for the specified measurement. Note: DISP:MEAS:FEED must first be done to feed the measurement to a trace. This command behaves the same as DISP:WIND:TRAC:MEM[:STAT] except that it only requires the measurement number. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<bool> |
ON or 1 - Turns the memory trace ON. |
Examples |
DISP:MEAS:MEM ON |
Query Syntax |
DISPlay:MEASure<mnum>:MEMory[:STATe]? |
Return Type |
Boolean |
OFF |
Applicable Models: All (Write-only) Moves a trace associated with measurement number to the specified window. If the window is OFF, it will be turn ON. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<toWin> |
Number of the window to which the specified measurement is moved. If the window does not exist, it will be created. |
Examples |
DISP:MEAS:MOVE 2 |
Query Syntax |
Not Applicable |
Not Applicable |
Applicable Models: All (Write-only) Activates the specified measurement to be selected. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
Examples |
DISP:MEAS:SEL |
Query Syntax |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Turns ON or OFF the display of a trace associated with the specified measurement. When OFF, the measurement behind the trace is still active. Note: A trace must first be created (via FEED), then the visibility of the trace can be affected with this command. If the trace has not been created, an error is generated: 107,Requested trace not found. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<bool> |
ON or 1 - Turns the trace ON. |
Examples |
DISP:MEAS:STAT ON |
Query Syntax |
DISPlay:MEASure<mnum>[:STATe]? |
Return Type |
Boolean |
ON or 1 |
Applicable Models: All (Read-Write) Sets or gets the title for the specified measurement. The trace title is embedded in the trace status field. Learn more about Trace Titles. Newer entries replace (not append) older entries. The title is turned ON and OFF with DISP:WIND:TRAC:TITL:STAT. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<string> |
Used as the title to be displayed for the measurement. Any characters (not spaces) enclosed with quotes. |
Examples |
DISP:MEAS:TITL:DATA 'MyNewMeas' |
Query Syntax |
DISPlay:MEASure<mnum>:TITLe:DATA? |
Return Type |
String |
Not Applicable |
Applicable Models: All (Read-Write) Turns ON or OFF the measurement title. Note: The measurement and trace need to exist. When turned OFF, the previous trace title returns. Set a new trace title using DISP:WIND:TRAC:TITL:DATA |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<bool> |
ON or 1 - turns the title ON. OFF or 0 - turns the title OFF. |
Examples |
DISP:MEAS:TITL ON |
Query Syntax |
DISPlay:MEAS<mnum>:TITLe[:STATe]? |
Return Type |
Boolean |
OFF or 0 |
Applicable Models: All (Read-Write) Set and get the display type for the specified measurement trace. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<char> |
Choose from:
|
Examples |
DISP:MEAS:TYPE MEM display:measure:type dmemory |
Query Syntax |
:DISPlay:MEASure:TYPE? |
DATA |
Applicable Models: All (Write-only) Performs an Autoscale on the specified trace in the specified measurement, providing the best fit display. Autoscale is performed only when the command is sent; it does NOT keep the trace autoscaled indefinitely. Autoscale behaves differently when scale coupling is enabled. How it behaves depends on the scale coupling method. Learn more. See Also, DISPlay:WINDow:Y:AUTO which performs an Autoscale All. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
Examples |
DISP:MEAS:Y:AUTO |
Query Syntax |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Sets the Y axis Scale Per Division value of the specified trace associated with the specified measurement. Note: The measurement and trace need to exist. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<num> |
Units / division value (Real value). The range of acceptable values is dependent on format and domain. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
Examples |
DISP:MEAS:Y:PDIV 1 |
Query Syntax |
DISPlay:MEASure<mnum>:Y[:SCALe]:PDIVision? |
Return Type |
Numeric |
10 |
Applicable Models: All (Read-Write) Sets the Y axis Reference Level of the specified trace associated with the specified measurement. Note: The measurement and trace need to exist. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<num> |
Reference level value (Real value). The range of acceptable values is dependent on format and domain. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
Examples |
DISP:MEAS:Y:RLEV 0 |
Query Syntax |
DISPlay:MEASure<mnum>:Y[:SCALe]:RLEVel? |
Return Type |
Numeric |
0 |
Applicable Models: All (Read-Write) Sets the Reference Position of the specified trace associated with the specified measurement. Note: The measurement and trace need to exist. |
|
Parameters |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
<num> |
Reference position on the screen measured in horizontal graticules from the bottom (Real value). The range of acceptable values is dependent on format and domain. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
Examples |
DISP:MEAS:Y:RPOS 0 |
Query Syntax |
DISPlay:MEASure<mnum>:Y[:SCALe]:RPOSition? |
Return Type |
Numeric |
5 |
Applicable Models: All (Write-only) This command arranges existing windows to sheets.
|
|
Parameters |
|
<num> |
Sheet number |
<char> |
Sheet arrangement. Choose from: WINDow: one sheet per window CHANnel: one sheet per channel TRACe: one channel per sheet ONE: merge all windows into one sheet |
Examples |
DISP:SHE:ARR CHAN |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
One sheet per window |
Applicable Models: All (Read-only) This command reads and displays comma separated list of window numbers which the sheet contains. |
|
Parameters |
|
<num> |
Sheet number |
Examples |
DISP:SHE:CAT? |
Return Type |
Character |
1 |
Applicable Models: All (Read-only) This command reads and displays a comma separated list of the sheet numbers in use in the order they appear in the GUI. Note: This is not returning sheet names, just their number as you would use in related commands like DISPlay:SHEet<num>:STATe?. Deleting and adding sheets can cause them to be unordered. |
|
Parameters |
|
<num> |
Sheet number |
Examples |
DISP:SHE:LIST? |
Return Type |
Character |
1 |
Applicable Models: All (Write-only) Add a new sheet according to the <int> parameter. |
|
Parameters |
|
<int> |
Add Type (optional) - 0: Sheet (default), 1: Trace + Sheet, 2: Trace + Channel + Sheet |
Examples |
DISP:SHE:NEW 1 display:sheet:new |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Write-only) Sets the sheet visible and invisible: ON: If OFF, sets the sheet visible with a new window. OFF: If ON, sets the sheet invisible with all the containing window state OFF (DISPlay:WINDow:STATe OFF) |
|
Parameters |
|
<num> |
Sheet number |
Examples |
DISP:SHE:STAT ON display:sheet:state off |
Query Syntax |
DISPlay:SHEet:STATe? |
Return Type |
Bool |
OFF except for Sheet 1 |
Applicable Models: All (Read-Write) This command sets or gets the sheet label. |
|
Parameters |
|
<num> |
Sheet number |
<char> |
The label of the sheets. Default and present value is "Sheet 1" |
Examples |
DISP:SHE:TITL:DATA "Sheet 1" |
Query Syntax |
DISPlay:SHEet:TITLe:DATA? |
Return Type |
Character |
"Sheet 1" |
Applicable Models: All (Read-Write) Set and read the display size. The settings are minimum (minimizes the display), maximum, and normal. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<enum> |
Choose from: MIN - Minimizes the display. MAX - Maximizes display to the full size of the display. NORMal - Default size. |
Examples |
DISP:SIZE MAX |
Query Syntax |
DISPlay:SIZE? |
Return Type |
Enumeration |
Default |
NORM |
Applicable Models: All (Write-only) Destroys all existing traces, channels and windows, then creates N windows. No channels are created. |
|
Parameters |
|
<num> |
N is 1 or greater. |
Examples |
DISP:SPL |
Query Syntax |
DISPlay:SPLit? |
Return Type |
Numeric |
Not Applicable |
Applicable Models: All (Write-only) Clears the message region in the status bar. |
|
Parameters |
|
Examples |
DISP:STAT:LOG:CLE |
Query Syntax |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Turn on or off the Display SCPI feature in SCPI recorder. |
|
Parameters |
|
<bool> |
ON (or 1) - Turn on the Display SCPI OFF (or 0) - Turn off the Display SCPI |
Examples |
DISP:STAT:SCPI ON |
Query Syntax |
DISPlay:STATus:SCPI? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Read-Write) Maximizes (isolates) or restores the active trace in the active window. When turned ON, the active trace is the ONLY trace on the display. All other traces are hidden. Learn more. |
|
Parameters |
|
<bool> |
ON (or 1) - Maximize / isolates the active trace. OFF (or 0) - Restores other traces to the normal window setting. |
Examples |
DISP:TMAX ON |
Query Syntax |
DISPlay:TMAX? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
This command is replaced by DISP:ARRange
(Write-only) Tiles the windows on the screen. |
|
Examples |
DISP |
Not Applicable |
Applicable Models: All (Read-Write) Show or hide the calset toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:CSET ON display:toolbar:cset:state off |
Query Syntax |
DISPlay:TOOLbar:CSET:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Read-Write) Specifies whether to show or hide the active entry toolbar. See this toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:ENTR ON display:toolbar:entry:state off |
Query Syntax |
DISPlay:TOOLbar:ENTRy:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Specifies whether to show or hide the port extensions toolbar. See this toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:EXT ON display:toolbar:extensions:state off |
Query Syntax |
DISPlay:TOOLbar:EXTensions:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Read-Write) Specifies whether to show or hide the virtual hardkeys on the VNA display. These are primarily used when the VNA is accessed remotely using VNC or Windows Remote Desktop. |
|
Parameters |
|
<bool> |
ON (or 1) - Keys ON. OFF (or 0) - Keys OFF. |
Examples |
DISP:TOOL:KEYS ON display:toolbar:keys:state off |
Query Syntax |
DISPlay:TOOLbar:KEYS:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Specifies whether to show or hide the marker toolbar. See this toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:MARK ON display:toolbar:marker:state off |
Query Syntax |
DISPlay:TOOLbar:MARKer:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
This toolbar was eliminated with A.10.00 (Read-Write) Specifies whether to show or hide the measurement toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:MEAS ON display:toolbar:measurement:state off |
Query Syntax |
DISPlay:TOOLbar:MEASurement[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
This toolbar was eliminated with A.10.00 (Read-Write) Specifies whether to show or hide the stimulus toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:STIM ON display:toolbar:stimulus:state off |
Query Syntax |
DISPlay:TOOLbar:STIMulus[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
This toolbar was eliminated with A.10.00 (Read-Write) Specifies whether to show or hide the sweep control toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:SWE ON display:toolbar:sweep:state off |
Query Syntax |
DISPlay:TOOLbar:SWEep[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Specifies whether to show or hide the Time Domain toolbar. See this toolbar. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:TOOL:TRAN ON display:toolbar:transform:state off |
Query Syntax |
DISPlay:TOOLbar:TRANsform:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Write-only) Add a new trace according to the <int> parameter. |
|
Parameters |
|
<int> |
Optional. Add Type -0: Trace (default), 1: Trace + Channel, 2: Trace + Window, 3: Trace + Channel + Window |
Examples |
DISP:TRAC:NEW 2 |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Add or delete the specified trace. If set ON to an existing channel, just activate the trace. |
|
Parameters |
|
<ch> |
Trace Number. Default is 1. |
<ON | OFF> |
ON (or 1) - adds the trace OFF (or 0) - deletes the trace |
Examples |
DISP:TRAC2:STAT 1 display:trace3:state on |
Query Syntax |
DISPlay:TRACe:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON (1) for Trace 1, OFF(0) for other traces |
Applicable Models: All (Read-Write) Enables or disables display updates. Disabling display updates improves measurement performance. When disabled, the display windows (traces, markers, etc.) are frozen. |
|
Parameters |
|
<bool> |
ON (or 1) - Toolbar ON. OFF (or 0) - Toolbar OFF. |
Examples |
DISP:UPD ON display:update:state off |
Query Syntax |
DISPlay:UPDate[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Write-only) Executes the display update once when the display update of the LCD screen is set to OFF (specifying False with the DISPlay:ENABle object). |
|
Parameters |
|
Examples |
DISP:UPD:IMM |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Makes the VNA application visible or not visible. In the Not Visible state, the analyzer cycle time for making measurements, and especially data transfer, can be significantly faster because the display does not process data. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - VNA app is visible |
Examples |
DISP:VIS ON |
Query Syntax |
DISPlay:VISible? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Sets and returns the X-axis position of the Limit Line Pass/Fail indicator on the VNA screen. The lower-left corner of the Pass/Fail indicator is the point of reference for positioning. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<num> |
X-axis position. Choose a value between 0 (far left) and 10 (far right). |
Examples |
DISP:WIND:ANN:LIM:XPOS 1.5 display:window:annotation:limit:xposition 5 |
Query Syntax |
DISPlay:WINDow:ANNotation:LIMit:XPOSition? |
Return Type |
Numeric |
7 |
Applicable Models: All (Read-Write) Sets and returns the Y-axis position of the Limit Line Pass/Fail indicator on the VNA screen. The lower-left corner of the Pass/Fail indicator is the point of reference for positioning. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<num> |
Y-axis position. The maximum position is limited to the current Y-axis division value. Choose a value between 2 (bottom) and 30 (top). |
Examples |
DISP:WIND:ANN:LIM:YPOS 1.5 display:window:annotation:limit:yposition 5 |
Query Syntax |
DISPlay:WINDow:ANNotation:LIMit:YPOSition? |
Return Type |
Numeric |
0 |
Applicable Models: All
(Read-Write) Sets the marker readouts to coupled (one combination annotation) or not coupled (one annotation per trace). This setting is per Window scope. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<bool> |
ON (or 1) - Marker readouts are coupled |
Examples |
DISP:WIND:ANN:MARK:COUP ON |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:COUPle? |
Return Type |
Boolean |
ON |
Applicable Models: All This command replaces DISP:WIND:ANN:MARK:SINGle (Read-Write) Sets the number of marker readouts to display per trace. Display up to 20 marker readouts per window. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<num> |
Number of marker readouts to display. Choose a value between 1 and 16. |
Examples |
DISP:WIND:ANN:MARK:NUMB 7 |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:NUMBer? |
Return Type |
Numeric |
5 |
Applicable Models: All
(Read-Write) Sets the X-axis position of marker readouts. Readouts are right-justified at the specified position. This function is used when :DISP:WIND:ANN:MARK:COUP:STAT is off. Use :DISP:WIND:ANN:MARK:XPOS is used when :DISP:WIND:ANN:MARK:COUP:STAT is on. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<mnum> |
Measurement. If unspecified, value is set to 1. |
<num> |
X-axis position. Choose a value between 1 (far left) and 10 (far right). |
Examples |
DISP:WIND:ANN:MARK:MEAS:XPOS 1.5 |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:MEASure:XPOSition? |
Return Type |
Numeric |
10 |
Applicable Models: All
(Read-Write) Sets the Y-axis position of marker readouts. Readouts are top-justified at the specified position. This function is used when :DISP:WIND:ANN:MARK:COUP:STAT is off. Use :DISP:WIND:ANN:MARK:YPOS is used when :DISP:WIND:ANN:MARK:COUP:STAT is on. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<mnum> |
Measurement. If unspecified, value is set to 1. |
<num> |
Y-axis position. Choose a value between 1 (bottom) and 10 (top). |
Examples |
DISP:WIND:ANN:MARK:MEAS:YPOS 1.5 |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:MEASure:YPOSition? |
Return Type |
Numeric |
10 |
Applicable Models: All (Read-Write) For the X-axis (stimulus), sets the number digits to display after the decimal point in marker readouts. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<num> |
Number of digits to display. Choose a value between 2 and 6. |
Examples |
DISP:WIND:ANN:MARK:RES:STIM 2 |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:RESolution:STIMulus? |
Return Type |
Numeric |
3 |
Applicable Models: All (Read-Write) For the Y-axis (response), sets the number digits to display after the decimal point in marker readouts. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<num> |
Number of digits to display. Choose a value between 1 and 4. |
Examples |
DISP:WIND:ANN:MARK:RES:RESP 1 |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:RESolution:RESPonse? |
Return Type |
Numeric |
2 |
Applicable Models: All Note: This command is replaced by DISP:WIND:ANN:MARK:NUMB (Read-Write) Either shows marker readout of only the active trace or other traces simultaneously. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<bool> |
ON (or 1) - Shows the readout of only the active marker for each trace. OFF (or 0) - Shows up to 5 marker readouts per trace, up to 20 total readouts. |
Examples |
DISP:WIND:ANN:MARK:SING ON |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:SINGle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Read-Write) Specifies the size of the marker readout text. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<char> |
Readout text size. Choose from:NORMal | LARGe |
Examples |
DISP:WIND:ANN:MARK:SIZE LARG |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:SIZE? |
Return Type |
Character |
NORMal |
Applicable Models: All (Read-Write) Specifies whether to show or hide the Marker readout (when markers are ON) on the selected window. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<ON | OFF> |
ON (or 1) - turns marker readout ON. OFF (or 0) - turns marker readout OFF. |
Examples |
DISP:WIND:ANN:MARK ON |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Sets the symbol to display for marker position. See other SCPI Marker commands. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<char> |
Marker symbol. Choose from: TRIangle FLAG LINE |
Examples |
DISP:WIND:ANN:MARK:SYMB TRI display:window:annotation:marker:symbol line |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:SYMBol? |
Return Type |
Character |
TRIangle |
Applicable Models: All
(Read-Write) Shows the marker readouts only for active trace or for all traces. This setting is per Window scope. See this toolbars |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<char> |
ACTive - readout is turned on for active trace only. ALL - readout is turned on for all traces. |
Examples |
DISP:WIND:ANN:MARK:VIS ACT display:windows:annotation:marker:visible all |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:VISible? |
Return Type |
Character |
ALL |
Applicable Models: All (Read-Write) Specifies whether or not to force marker symbols to be displayed above the trace. When ON, all marker symbols will be displayed above the trace and the active marker will be filled solid. See other SCPI Marker commands. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<ON | OFF> |
ON (or 1) - ALL marker symbols are displayed above the trace. Only the active marker is filled solid. OFF (or 0) - ONLY the active marker is displayed above the trace. The active marker is not filled solid. |
Examples |
DISP:WIND:ANN:MARK:SYMB:ABOV ON |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:SYMBol:ABOVe:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF - ON in IM Spectrum and SA measurement classes |
Applicable Models: All (Read-Write) Sets the X-axis position of marker readouts. Readouts are right-justified at the specified position. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<num> |
X-axis position. Choose a value between 1 (far left) and 10 (far right). |
Examples |
DISP:WIND:ANN:MARK:XPOS 1.5 |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:XPOSition? |
Return Type |
Numeric |
10 |
Applicable Models: All (Read-Write) Sets the Y-axis position of marker readouts. Readouts are top-justified at the specified position. See other SCPI Marker commands. Learn more about Marker readout. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<num> |
Y-axis position. Choose a value between 1 (bottom) and 10 (top). |
Examples |
DISP:WIND:ANN:MARK:YPOS 1.5 |
Query Syntax |
DISPlay:WINDow:ANNotation:MARKer:YPOSition? |
Return Type |
Numeric |
10 |
Applicable Models: All (Read-Write) Set and read the scope for trace annotation. Either display trace annotation for all traces or just the active trace. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<enum> |
Choose from: ALL ACTive |
Examples |
DISP:WIND:ANN:SCOP ACT |
Query Syntax |
DISPlay:WINDow:ANNotation[:TRACe]:SCOPe? |
Return Type |
Enumeration |
Default |
ALL |
Applicable Models: All (Read-Write) Specifies whether to show or hide the Trace Status at the top of the window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<ON | OFF> |
ON (or 1) - turns the buttons ON. |
Examples |
DISP:WIND:ANN ON |
Query Syntax |
DISPlay:WINDow:ANNotation[:TRACe]:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Turns ON or OFF the X-axis scale label in display window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<bool> |
ON or 1 - Turns ON the X-axis scale. |
Examples |
DISP:WIND:ANN:X ON |
Query Syntax |
DISPlay:WINDow:ANNotation:X? |
Return Type |
Boolean |
ON or 1 |
Applicable Models: All (Read-Write) Set and read the scope for the stimulus information on the display title bar. Either display the stimulus information for all traces or just the active trace. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<enum> |
Choose from: ALL ACTive |
Examples |
DISP:WIND:ANN:XAX:SCOP ACT |
Query Syntax |
DISPlay:WINDow:ANNotation:XAXis:SCOPe? |
Return Type |
Enumeration |
Default |
ALL |
Applicable Models: All (Read-Write) Turns ON or OFF the Y-axis scale label in display window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<bool> |
ON or 1 - Turns ON the Y-axis scale. |
Examples |
DISP:WIND:ANN:Y ON |
Query Syntax |
DISPlay:WINDow:ANNotation:Y? |
Return Type |
Boolean |
ON or 1 |
Applicable Models: All (Read-only) Returns the trace numbers for the specified window. Note: If there are no traces in the window, this query returns the "EMPTY" string. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
Example |
Window 1 with four traces: |
Return Type |
String of Character values separated by commas |
Not applicable |
Applicable Models: All (Read-Write) Specifies whether to disable or enable all analyzer display information in the specified window. Marker data is not updated. More CPU time is spent making measurements instead of updating the display. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<ON | OFF> |
ON (or 1) - turns the display ON. |
Examples |
DISP:WIND:ENABle ON |
Query Syntax |
DISPlay:WINDow<wnum>:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Write-only) This command feeds a specified window to the sheet. If there is a window in the sheet, the sheet is visible. If there is no window in the sheet, the sheet is not visible. If no windows exists in the system, one empty sheet is visible. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<snum> |
Sheet number |
Examples |
DISP:WIND:FEED 5 |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Write-only) Add a new window according to the <int> parameter. |
|
Parameters |
|
<int> |
Add Type (optional) - 0: Window (default), 1: Trace + Window, 2: Trace + Channel + Window |
Examples |
DISP:WINDS:NEW 1 |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-only) Returns the lowest window number which has less than the maximum number of traces. Basically, returns the first window which has room for another trace. Note that the window may need to be turned on first (i.e. disp:wind:stat ON may be needed). |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
Examples |
DISP:WIND:NEXT |
Query Syntax |
DISPlay:WINDow<wnum>:NEXT? |
Return Type |
Not Applicable |
Not Applicable |
Applicable Models: All (Read-Write) Sets or returns the window setting of Maximized or Normal. To arrange all of the windows, use DISP:ARR. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1 |
<char> |
Window size. Choose from: MAX | NORM |
Examples |
DISP:WIND:SIZE MAX |
Query Syntax |
DISPlay:WINDow:SIZE? |
Not Applicable |
Applicable Models: All (Read-Write) Write to create or delete a window on the screen or Read whether a window is present. |
|
Parameters |
|
<wnum> |
Window number to create; choose any integer between 1 and the maximum number of windows allowed in the VNA. |
<ON | OFF> |
ON (or 1) - The window <wnum> is created. |
Examples |
DISP:WIND ON |
Query Syntax |
DISPlay:WINDow<wnum>:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
Window number "1" ON |
Applicable Models: All (Read-Write) Write to show the specified table at the bottom of the analyzer screen or Read to determine what table is visible. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1 |
<char> |
Table to show. Choose from: |
Examples |
DISP:WIND:TABLe SEGM |
Query Syntax |
DISPlay:WINDow<wnum>:TABLe? |
OFF |
Applicable Models: N522xB, N524xB with Phase Noise Option S93031xB (Read-Write) Enable or disable displaying the integrated noise table. |
|
Parameters |
|
<wnum> |
Window number to create; choose any integer between 1 and the maximum number of windows allowed in the VNA. |
<ON | OFF> |
ON (or 1) - Display the integrated noise table. |
Examples |
DISP:WIND:TABL:INO:ENAB ON |
Query Syntax |
DISPlay:WINDow<wnum>:TABLe:INOise:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: N522xB, N524xB with Phase Noise Option S93031xB (Read-Write) Enable or disable displaying the spot noise table. |
|
Parameters |
|
<wnum> |
Window number to create; choose any integer between 1 and the maximum number of windows allowed in the VNA. |
<ON | OFF> |
ON (or 1) - Display the spot noise table. |
Examples |
DISP:WIND:TABL:SNO:ENAB ON |
Query Syntax |
DISPlay:WINDow<wnum>:TABLe:SNOise:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: N522xB, N524xB with Phase Noise Option S93031xB (Read-Write) Enable or disable displaying the spurious table. |
|
Parameters |
|
<wnum> |
Window number to create; choose any integer between 1 and the maximum number of windows allowed in the VNA. |
<ON | OFF> |
ON (or 1) - Display the spurious table. |
Examples |
DISP:WIND:TABL:SPUR:ENAB ON |
Query Syntax |
DISPlay:WINDow<wnum>:TABLe:SPURious:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Read-Write) Sets data in the window title area. The title is turned ON and OFF with DISP:WIND:TITL:STAT OFF. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<string> |
Title to be displayed. Any characters, enclosed with quotes. If the title string exceeds 50 characters, an error will be generated and the title not accepted. Newer entries replace (not append) older entries. |
Examples |
DISP:WIND:TITL:DATA 'hello' |
Query Syntax |
DISPlay:WINDow<wnum>:TITLe:DATA? |
Return Type |
String |
NA |
Applicable Models: All (Read-Write) Turns display of the title string ON or OFF. When OFF, the string remains, ready to be redisplayed when turned back ON. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<ON | OFF> |
ON (or 1) - turns the title string ON. |
Examples |
DISP:WIND:TITL ON |
Query Syntax |
DISPlay:WINDow<wnum>:TITLe[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Write-only) Deletes the specified trace from the specified window. The measurement parameter associated with the trace is not deleted. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<tnum> |
The number of the trace to be deleted; if unspecified, value is set to 1. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
Examples |
DISP:WIND:TRAC:DEL |
Query Syntax |
Not Applicable |
Not Applicable |
Applicable Models: All (Write-only) Creates a new trace <tnum> and associates (feeds) a measurement <name> to the specified window<wnum>. This command should be executed after creating a new measurement with CALCulate:MEASure:DEFine. Note: Window <wnum> must already be turned on before this command can be used. Turn on the window state using DISPlay:WINDow:STATe. To feed the same measurement to multiple traces, create another measurement with the same <parameter>, but different <name>, using the CALC:PAR:DEF command. The analyzer will collect the data only once. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<tnum> |
Trace number to be created. Choose any Integer between 1 and the VNA maximum number of traces per window allowed. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<name> |
Name of the measurement that was defined with CALC:PAR:DEF<name>,<parameter> |
Example |
CALCulate1:PARameter:DEFine 'CH1_S11',s11,1 CALCulate1:PARameter:SELect 'CH1_S11' DISPlay:WINDow1:STATe ON DISPlay:WINDow1:TRACe1:FEED 'CH1_S11' |
Query Syntax |
Not applicable |
"CH1_S11" |
Applicable Models: All (Write-only) Creates a new trace <tnum> for an existing measurement (MNUM) and associates (feeds) the measurement number to the specified window<wnum>. A measurement is created using the CALC:MEAS:DEF command. Measurements created in the system all have unique numbers. Similarly, every window has a unique number and the numbers are displayed in the lower-left corner of each window. Every window has the capacity to hold a finite number of traces from 1 to N, where N is the maximum number of traces per window. Each window uses the same range of trace numbers. For example, window 1 can have a trace 1 and so can window 2. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<tnum> |
Trace number to be created. Choose any Integer between 1 and the VNA maximum number of traces per window allowed. Note: After executing the DISP:WIND:TRAC:FEED:MNUM command, a new trace is added to the specified window and the trace number of the channel which appears as the Tr annotation on the Trace Status display is the actual measurement number. |
<int> |
Number of an existing measurement. The range is 1 to 2000. |
Examples |
CALC:MEAS2:DEF "S22" |
Query Syntax |
Not applicable |
Not applicable |
Applicable Models: All (Read-Write) Sets and returns the grid line type (solid | dotted) for all open windows. Grid is returned to solid when the VNA is Preset. Learn more. |
|
Parameters |
|
<value> |
Line type. Choose from: SOLid - solid lines DOTTed - dotted lines |
Examples |
DISP:WIND:TRAC:GREAT:GRID:LTYPE SOL |
Query Syntax |
DISPlay:WINDow:TRACe:GRATicule:GRID:LTYPE? |
Return Type |
Character |
SOLID |
Applicable Models: All (Read-Write) Turns the memory trace ON or OFF. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<ON | OFF> |
ON (or 1) - turns the memory trace ON. |
Examples |
DISP:WIND:TRAC:MEM ON |
Query Syntax |
DISPlay:WIND<wnum>:TRACe<tnum>:MEMory:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
Applicable Models: All (Write-only) Moves a trace from one window to another window. |
|
Parameters |
|
<fromWin> |
Window number to move the trace from. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Trace number to be moved. If unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<toWin> |
Number of the window to move the trace to. If the window does not exist, it will be created. |
Examples |
DISP:WIND:TRAC2:MOVE 2 |
Query Syntax |
Not applicable |
Not applicable |
Applicable Models: All (Read-only) Returns the next unused trace number. For example, if trace #1, #2, and #3 are being used, then this command will return 4. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. |
Examples |
DISP:WIND:TRAC:NEXT? |
Return Type |
Integer |
Not Applicable |
Applicable Models: All (Write-only) Activates the specified trace in the specified window for front panel use. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
Examples |
DISP:WIND:TRAC:SEL |
Query Syntax |
Not applicable |
NA |
Applicable Models: All (Read-Write) Turns the display of the specified trace in the specified window ON or OFF. When OFF, the measurement behind the trace is still active. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<ON | OFF> |
ON (or 1) - turns the trace ON. |
Examples |
DISP:WIND:TRAC ON |
Query Syntax |
DISPlay:WIND<wnum>:TRACe<tnum>:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Writes and read data to the trace title area. The trace title is embedded in the trace status field. Learn more about Trace Titles. Newer entries replace (not append) older entries. The title is turned ON and OFF with DISP:WIND:TRAC:TITL:STAT. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Trace number of the specified window. If unspecified, value is set to 1. Use Display:Cat? to read the window numbers. Use Disp:Window:Cat? to read the trace numbers of the specified window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<string> |
Title to be displayed. Any characters (not spaces) enclosed with quotes. |
Examples |
DISP:WIND:TRAC:TITL:DATA 'MyNewMeas' |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>TITLe:DATA? |
Return Type |
String |
Not Applicable |
Applicable Models: All (Read-Write) Turns display of the Trace Title ON or OFF. When turned OFF, the previous trace title returns. Set a new trace title using DISP:WIND:TRAC:TITL:DATA |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1 Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Trace number of the specified window. If unspecified, value is set to 1. Use Display:Cat? to read the window numbers. Use Disp:Window:Cat? to read the trace numbers of the specified window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<bool> |
ON (or 1) - turns the title ON. OFF (or 0) - turns the title OFF. |
Examples |
DISP:WIND:TRAC:TITL ON |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:TITLe[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Sets the X axis Reference Level of the specified trace in the specified window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<num> |
Reference level value. |
Examples |
DISP:WIND:TRAC:X:RLEV 0 |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:X[:SCALe]:RLEVel? |
Return Type |
Numeric |
Not Applicable |
Applicable Models: All (Read-Write) Sets the Reference Position of the specified trace in the specified window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<num> |
Reference position on the screen measured in horizontal graticules from the bottom. Choose a value between 0 and 10. |
Examples |
DISP:WIND:TRAC:X:RPOS 0 display:window2:trace2:x:rposition 10 |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:X[:SCALe]:RPOSition? |
Return Type |
Numeric |
5 |
Applicable Models: All (Write-only) Performs an Autoscale on the specified trace in the specified window, providing the best fit display. Autoscale is performed only when the command is sent; it does NOT keep the trace autoscaled indefinitely. Autoscale behaves differently when scale coupling is enabled. How it behaves depends on the scale coupling method. Learn more. See Also, DISPlay:WINDow:Y:AUTO which performs an Autoscale All. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
Examples |
DISP:WIND:TRAC:Y:AUTO |
Query Syntax |
Not applicable |
Not applicable |
Applicable Models: All (Read-Write) Sets and returns the method of scale coupling. Learn more about Scale coupling. |
|
Parameters |
|
<char> |
OFF - NO scale coupling for any windows. WINDow - Scale settings are coupled for traces in each window. ALL - Scale settings are coupled for traces in ALL selected windows. Enable the selected windows using DISP:WIND:TRAC:Y:COUP ON |
Examples |
DISP:WIND:TRAC:Y:COUP:METH ALL Display:window2:trace:y:scale:method window |
Query Syntax |
DISPlay:WINDow:TRACe:Y[:SCALe]:COUPle:METHod? |
Return Type |
Character |
OFF |
Applicable Models: All (Read-Write) Enables and disables scale coupling for the specified window. Learn more about Scale coupling. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1 Use Disp:Cat? to read the existing window numbers. |
<bool> |
ON (or 1) - Scale coupling enabled for specified window. OFF (or 0) - Scale coupling disabled for specified window. |
Examples |
DISP:WIND:TRAC:Y:COUP ON Display:window2:trace:y:scale:couple:state off |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe:Y[:SCALe]:COUPle[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
Applicable Models: All (Read-Write) Sets the Y axis Per Division value of the specified trace in the specified window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<num> |
Units / division value. The range of acceptable values is dependent on format and domain. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
Examples |
DISP:WIND:TRAC:Y:PDIV 1 |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:Y[:SCALe]:PDIVision? |
Return Type |
Numeric |
10 |
Applicable Models: All (Read-Write) Sets the Y axis Reference Level of the specified trace in the specified window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<num> |
Reference level value. The range of acceptable values is dependent on format and domain. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
Examples |
DISP:WIND:TRAC:Y:RLEV 0 |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:Y[:SCALe]:RLEVel? |
Return Type |
Numeric |
Not Applicable |
Applicable Models: All (Read-Write) Sets the Reference Position of the specified trace in the specified window. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<num> |
Reference position on the screen measured in horizontal graticules from the bottom. Choose a value between 0 and 10. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
Examples |
DISP:WIND:TRAC:Y:RPOS 0 display:window2:trace2:y:rposition maximum |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:Y[:SCALe]:RPOSition? |
Return Type |
Numeric |
5 |
Applicable Models: All (Read-Write) Sets the minimum scale value for the Log Y-axis. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<num> |
Minimum scale value. Range from 10f to 500P. |
Examples |
DISP:WIND:TRAC:Y:BOTT 0 display:window2:trace2:y:bottom 100 |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:Y[:SCALe]:BOTTom? |
Return Type |
Numeric |
1 |
Applicable Models: All (Read-Write) Sets the maximum scale value for the Log Y-axis. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<num> |
Maximum scale value. Range from 20f to 1E. |
Examples |
DISP:WIND:TRAC:Y:TOP 0 display:window2:trace2:y:top 100 |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:Y[:SCALe]:TOP? |
Return Type |
Numeric |
1k |
Applicable Models: All (Read-Write) Sets or returns format type for Y axis graph, either linear or logarithmic. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1 Use Disp:Cat? to read the existing window numbers. |
<tnum> |
Any existing trace number; if unspecified, value is set to 1. Use Disp:Wind:Cat? to read the trace numbers in an existing window. Note: This is NOT the trace number of the channel which appears as the Tr annotation on the Trace Status display. This <tnum> is the trace number within the specified window, and is used ONLY for remote programs. |
<char> |
choose either LINear or LOGarithmic |
Examples |
DISP:WIND:TRACY:SPAC LOG Display:window2:trace2:y:spacing logarithmic |
Query Syntax |
DISPlay:WINDow<wnum>:TRACe<tnum>:Y:SPACing? |
Return Type |
char |
Lin |
Applicable Models: All (Write-only) Scales ALL of the traces to fit in the same window. This is equivalent to "Autoscale All" from the front panel. Autoscale behaves differently when scale coupling is enabled. How it behaves depends on the scale coupling method. Learn more. Autoscale is performed only when the command is sent; it does NOT keep the trace autoscaled indefinitely. See Also, DISPlay:WINDow:TRACe:Y:AUTO which Autoscales only the specified trace. |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1. Use Disp:Cat? to read the existing window numbers. |
Examples |
DISP:WIND:Y:AUTO |
Query Syntax |
Not applicable |
Not applicable |
Applicable Models: All (Read-Write) Sets or returns the number of divisions in all the graphs, for the selected channel |
|
Parameters |
|
<wnum> |
Any existing window number. If unspecified, value is set to 1 Use Disp:Cat? to read the existing window numbers. |
<bool> |
ON or 1 - Scale coupling enabled for specified window. OFF or 0 - Scale coupling disabled for specified window. |
<num> |
Number of divisions is between 4 to 30. Units / division value. The range of acceptable values is dependent on format and domain. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
Examples |
DISP:WIND:Y:DIV 12 Display:window2:y:scale:divisions 12 |
Query Syntax |
DISPlay:WINDow<wnum>:Y[:SCALe]:DIVisions? |
Return Type |
Boolean |
10 |