Only the Main and Layout Setup commands corresponding to the Scalar Mixer/Converter + Phase measurement class are documented here. All other commands are identical to the Setup commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtabs on the graphic below.
Click here to view links to Setup commands for all Measurement Classes.