Sense:Correction:Collect:Ckit Commands


Use to change the definitions of calibration kit standards.

SENSe:CORRection:COLLect:CKIT:

       | CATalog?

       | CLISt

       | CLABel

       | CONNector

             | ADD

             | CATalog?

             | DELete

             | FNAMe

             | SNAMe

       | DESCription

       | INFormation?

       | NAME

       | OLAB

       | OLISt?

       | ORDer

       | PORT[:SELect]

       | SELect

       | STANdard

             | CO, C1, C2, C3

             | CHARacter

             | DATA

                  | LOAD

             | DELay

             | FMAXimum

             | FMINimum

             | IMPedance

             | LO, L1, L2, L3

             | LABel

             | LOSS

             | REMove

             | SDEScription

             | [SELect]

             | TYPE

             | TZReal

             | TZImag

       | TRLoption

             | IMPedance

             | LRLChar

             | RPLane

 

Click on a keyword to view the command details.

Blue keywords are superseded commands.

Most of these commands act on the currently selected standard from the currently selected calibration kit.

Note: You should provide data for every definition field - for every standard in your calibration kit. If a field is not set, the default value may not be what you expect.

For more information, read Specifying Calibration Standards and Kits for Keysight Vector Network Analyzers (Application Note 1287-11)


SENSe:CORRection:COLLect:CKIT:CATalog?

Applicable Models: All

(Read-only) Returns the names of the first 95 mechanical cal kits in your VNA that can be used for unguided calibrations.  

Examples

SENS:CORR:COLL:CKIT:CAT?

Return Type

A comma-separated string

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:CLISt <class>, <list_stds>

Applicable Models: All

(Write-Read) Assigns the calibration class for the standard

Parameters

 

<class>

Specify the calibration classes:

SA - OPEN Standards (standards in the SA class are not always Opens)

SB - SHORT Standards

SC  - LOAD Standards

THRU - Thru

FWDT - Forward Trans

FWDM - Forward Match

REVT - Reverse Trans

REVM - Reverse Match

TRLT - TRL Thru

TRLR - TRL Reflection

TRLLm - TRL Line

UTHRu - Unknown Thru

ISOL - Isolation

<list_stds>

List of standard IDs (Same as SENS:CORR:COLL:CKIT:OLIS). A standard ID can be between 1 and 1000.

Examples

SENS:CORR:COLL:CKIT:CLIST SA,1,2,5
SENS:CORR:COLL:CKIT:CLIST? SA

Return Type

Numeric; returns standard number of the selected class

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:CLABel <class>, <label>

Applicable Models: All

(Write-Read) Defines the label for the standard classes.

Parameters

 

<class>

Specify the calibration classes:

SA - OPEN Standards (standards in the SA class are not always Opens)

SB - SHORT Standards

SC  - LOAD Standards

TRAN - Thru

FWDT - Forward Trans

FWDM - Forward Match

REVT - Reverse Trans

REVM - Reverse Match

TRLT - TRL Thru

TRLR - TRL Reflection

TRLLm - TRL Line

UTHRu - Unknown Thru

ISOL - Isolation

<label>

Label of standard

 

Examples

SENS:CORR:COLL:CKIT:CLABEL SA,"OPEN"
SENS:CORR:COLL:CKIT:CLABEL? SA

Return Type

String; returns the label.

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:CONNector:ADD <family>,<start>,<stop>,<z0>,<gender>,<media>,<cutoff>

Applicable Models: All

(Write only) Creates a new connector.  The connector is automatically added to the list of available connectors for the currently selected cal kit.  If a connector includes both male and female connectors, each connector must be added separately.

Parameters

 

<family>

(String) Name of connector family. Limited to 50 characters.

<start>

Start frequency

<stop>

Stop frequency

<z0>

Characteristic Impedance of the connector in ohms.

<gender>

Connector gender. Choose from:
MALE
FEMALE
NONE

<media>

Media of the connector. Choose from:

COAX - coaxial
WAVE
- waveguide

<cutoff>

Cutoff frequency of the connector (waveguide only).

Examples

SENS:CORR:COLL:CKIT:CONN:ADD "PSC 1.8 mm",0 HZ,999.9 GHZ,50,FEMALE,COAX,0.0
SENS:CORR:COLL:CKIT:CONN:ADD "PSC 1.8 mm",0 HZ,999.9 GHZ,50,MALE,COAX,0.0

Query Syntax

Not applicable

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:CONNector:CATalog?

Applicable Models: All

(Read-only) Returns a comma-separated list of all connectors defined within the currently selected cal kit.  The returned string includes the connector family name followed by the connector gender, if any.  Kits may include a primary connector family name and additional connector family names.

Connector family names are case sensitive.  A connector family named "PSC 2.4" is different from a connector family named "psc 2.4".

Learn more about Connector Family Name.

Examples

SENS:CORR:COLL:CKIT:CONN:CAT?

'Returned string

"Type-N (50) male, Type-N (50) female"

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:CONNector:DELete

Applicable Models: All

(Write-only) Deletes the primary connector family name from the selected kit.  The VNA allows multiple connector families for each kit.  If a kit includes multiple connector families, only the first listed (primary) connector family name is deleted.  

Once the connector family is deleted, the connector may not be assigned to any new or existing standard within the kit.  

The previously defined standards retain their association to the deleted connector name. To reassign standards to a new connector family name, use SENS:CORR:COLL:CKIT:CONN:SNAMe.

Examples

SENS:CORR:COLL:CKIT:CONN:DEL

Query Syntax

Not Applicable

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:CONNector:FNAMe <name>

Applicable Models: All

(Read-Write)  Replaces the primary connector family name from the selected kit with a new connector family name.  The connector family name is replaced in all standards in the kit that share that name.  The VNA allows multiple connector families for each kit.  If a kit includes multiple connector families, only the first listed (primary) connector family name is replaced.  Use the query form of this command to return the name of the primary connector family.

Parameters

 

<name>

New connector family name.  Limited to 50 characters.

Examples

SENS:CORR:COLL:CKIT:CONN:FNAM 'MYPSC35'

Sense:correction:collect:ckit:connector:name 'My Type N'

Query Syntax

SENSe:CORRection:COLLect:CKIT:CONNector:FNAMe?

Return Type

String

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:CONNector:SNAMe <family>,<gender>,<port>

Applicable Models: All

(Read-Write)  Assigns a family name to the currently selected standard from the currently selected kit. Specify each port of a 2-port standard individually. Use the query form of this command to read the connector family name assigned to the current standard.  The name is not assigned unless the connector family name is previously defined within the selected kit.

Parameters

 

<family>

String. Connector family name.

<gender>

Connector gender. Choose from:
MALE
FEMALE
NONE

<port>

Number of the connector port to be assigned the connector family name. 2-port standards such as a thru line must be assigned separately. It is not relevant which connector is port 1 or port 2.

1  Specifies a 1-port standard or the first port of a 2-port standard.

2  Specifies the second port of a 2-port standard.

Examples

SENS:CORR:COLL:CKIT:CONN:SNAMe "Type-N (50)",MALE,1

Query Syntax

SENSe:CORRection:COLLect:CKIT:CONNector:SNAMe?

Return Type

String

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:DESCription <string>

Applicable Models: All

(Read-Write) Modifies the cal kit description field of the selected kit. This description appears in the Edit VNA Cal Kit dialog box.

Parameters

 

<string>

Description of the cal kit. Limited to 50 characters.

Examples

SENS:CORR:COLL:CKIT:DESC "My New CalKit"

Query Syntax

SENSe:CORRection:COLLect:CKIT:DESCription?

Return Type

String

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:INFormation? <module>[,char]

Applicable Models: All

(Read Only)  Reads characterization information from an ECal module.

Parameters

 

<module>

Specifies which ECal module to read from.  Choose from:

ECAL1

.through.

ECAL50

[char]

 

Optional argument.

Specifies which characterization within the ECal module to read information from.  If this argument is not used, the default is CHAR0.  CHAR1 through CHAR5 are for user characterizations that may have been written to the module by the User Characterization feature on the VNA.  Choose from:

CHAR0   Factory characterization (data that was stored in the ECal module by Keysight)

CHAR1   User characterization #1

CHAR2   User characterization #2

- through -

CHAR12   User characterization #12

Examples

SENS:CORR:COLL:CKIT:INF? ECAL4
sense:correction:collect:ckit:information? ecal2,char1

 

Example return string:

 

ModelNumber: 85092-60007, SerialNumber: 01386, ConnectorType: N5FN5F, PortAConnector: Type N (50) female, PortBConnector: Type N (50) female, MinFreq: 30000, MaxFreq: 9100000000, NumberOfPoints: 250, Calibrated: July 4 2002

Return Type

Character

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:NAME <name>

Applicable Models: All

(Read-Write) Sets a name for the selected calibration kit.

Parameters

 

<name>

Calibration Kit name. Any string name, can include numerics, period, and spaces; any length (although the dialog box display is limited to about 30 characters).

Examples

SENS:CORR:COLL:CKIT:NAME 'MYAPC35'
sense:correction:collect:ckit:name 'mytypen'

Query Syntax

SENSe:CORRection:COLLect:CKIT:NAME?

Return Type

String

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:OLABel<class> <name> - Superseded

This command is replaced by SENS:COR:CKIT:CLAB.

Applicable Models: All

(Read-Write) Sets the label for the calibration class designated by <class>.  The label is used in the prompts for connecting the calibration standards associated with that <class>.

Parameters

 

<class>

Number of the calibration class. Choose a number between:  1 and 18.  The <class> numbers are associated with the following calibration Classes:

 

Class

Description

Port 1

 

 

1

SA

Reflection standard

2

SB

Reflection standard

3

SC

Reflection standard

4

FWD TRANS

Thru/Delay standard

Port 2

 

 

5

SA

Reflection standard

6

SB

Reflection standard

7

SC

Reflection standard

8

REV TRANS

Thru/Delay standard

3-port analyzers only

Port 3

 

 

9

S33A

Reflection standard

10

S33B

Reflection standard

11

S33C

Reflection standard

12

S32T

Thru/Delay standard

13

S23T

Thru/Delay standard

14

S31T

Thru/Delay standard

15

S13T

Thru/Delay standard

TRL Calibrations

16

TRL "T"

Thru standard

17

TRL "R"

Reflect standard

18

TRL "L"

Line standard

<name>

Label for the calibration class.  Must be enclosed in quotes.  Any string between 1 and 12 characters long.  Cannot begin with a numeric.

Examples

SENS:CORR:COLL:CKIT:OLAB3 'LOADS'

sense:correction:collect:ckit:olabel4 'Thru'

Return Type

String

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:OLISt[class]? - Superseded

This command is replaced by SENS:CORR:CKIT:CLIS.

Applicable Models: All

(Read-only) Returns seven values of standards that are assigned to the specified class.

This command ALWAYS applies to the Cal Kit that is selected (using SENS:CORR:COLL:CKIT:SEL) when this ORDer command is sent.

Parameters

 

<class>

Number of the calibration class to be queried. The <class> numbers are associated with the following calibration Classes:

 

Class

Description

Port 1

   

1

SA

Reflection standard

2

SB

Reflection standard

3

SC

Reflection standard

4

FWD TRANS

Thru/Delay standard

Port 2

   

5

SA

Reflection standard

6

SB

Reflection standard

7

SC

Reflection standard

8

REV TRANS

Thru/Delay standard

3-port analyzers ONLY (N3381A/2A/3A)

4-port analyzers use S11 and S22 classes (see example program)

Port 3

   

9

S33A

Reflection standard

10

S33B

Reflection standard

11

S33C

Reflection standard

12

S32T

Thru/Delay standard

13

S23T

Thru/Delay standard

14

S31T

Thru/Delay standard

15

S13T

Thru/Delay standard

TRL Calibration

16

TRL "T"

Thru standard

17

TRL "R"

Reflect standard

18

TRL "L"

Line standard

Examples

SENS:CORR:COLL:CKIT:OLIS?
Always returns 7 standard numbers. Unassigned standards return 0

Return Type

Numeric; returns the <class> number of the selected standard.

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:ORDer<class> <std> [,<std>] [,<std>] [,<std>] [,<std>] [,<std>] [,<std>]- Superseded

This command is replaced by SENS:CORR:CKIT:CLIS.

Applicable Models: All

(Read-Write) Sets a standard number to a calibration class. This command does NOT set or dictate the order for measuring the standards. For more information, see Assigning Standards to a Calibration Class.

This command ALWAYS applies to the Cal Kit that is selected (using SENS:CORR:COLL:CKIT:SEL) when this ORDer command is sent.

Parameters

 

<class>

Number of the calibration class that is assigned to <standard>. Choose a number between: 1 and 18.  The <class> numbers are associated with the following calibration Classes:

 

Class

Description

STAN#

Port 1

 

   

1

SA

Reflection standard

STAN1

2

SB

Reflection standard

STAN2

3

SC

Reflection standard

STAN3

4

FWD TRANS

Thru/Delay standard

STAN4

Port 2

 

 

 

5

SA

Reflection standard

STAN1

6

SB

Reflection standard

STAN2

7

SC

Reflection standard

STAN3

8

REV TRANS

Thru/Delay standard

STAN4

3-port analyzers ONLY (N3381A/2A/3A)

4-port analyzers use S11 and S22 classes (see example program)

Port 3

 

 

 

9

S33A

Reflection standard

STAN1

10

S33B

Reflection standard

STAN2

11

S33C

Reflection standard

STAN3

12

S32T

Thru/Delay standard

STAN4

13

S23T

Thru/Delay standard

STAN4

14

S31T

Thru/Delay standard

STAN4

15

S13T

Thru/Delay standard

STAN4

TRL Calibration

16

TRL "T"

Thru standard

STAN4

17

TRL "R"

Reflect standard

STAN1

18

TRL "L"

Line standard

STAN3

<std>

Standard number to be assigned to the class; Choose a standard between 1 and 30. One standard is mandatory; up to six additional standards are optional.

Examples

'Assigns standard 3 to S11A class:
SENS:CORR:COLL:CKIT:ORD1 3

'Assigns standard 2 and 5 to S21T class class:
sense:correction:collect:ckit:order4 2,5

Query Syntax

SENSe:CORRection:COLLect:CKIT:ORDer<class>?

'Returns only the first standard assigned to the specified class. To query the remaining standards, use SENSe:CORRection:COLLect:CKIT:OLIST[1-15]?

Return Type

Numeric

Default

Not Applicable


SENSe<cnum>:CORRection:COLLect:CKIT:PORT<n>[:SELect] <string>

Applicable Models: All

(Read-Write)  Sets and returns the name of the Cal Kit to use for Unguided cal.

This command effectively does the same task as SENS:CORR:COLL:CKIT but specifies the cal kit by name.

Note:  During an Unguided cal, you can access ONLY mechanical cal kits #1 through #95. However, there is no limit to the number of cal kits that can be imported.

Parameters

 

<cnum>

Currently not used. The unguided cal kit selection is for all ports on all channels.

<n>

Currently not used. The unguided cal kit selection is for all ports on all channels.

<string>

 

Cal Kit name enclosed in quotes. Use SENS:CORR:COLL:CKIT:CAT? to read a list of all available Cal Kits in the VNA.

Examples

SENS:CORR:COLL:CKIT:PORT "85052B"
sense2:correction:collect:ckit:port:select "85052D"

Query Syntax

SENSe<cnum>:CORRection:COLLect:CKIT:PORT<n>:SELECT?

Return Type

String

Default

Last kit selected


SENSe<cnum>:CORRection:COLLect:CKIT[:SELect] <num>

Applicable Models: All

(Read-Write)  Selects (makes active) a calibration kit for performing an UNGUIDED calibration or for modifying standards. All subsequent "CKIT" commands that are sent apply to this selected calibration kit. Select a calibration standard using SENS:CORR:COLL:CKIT:STAN <num>. Kits 1 to approximately kit 43 are factory installed Cal Kits.  Note that staring in release A.20.95.XX, six new calkits were added that impact the index.  If previous ordering is desired, manage the calkits by using the Modify Calibration Kits dialog to select “2023 Defaults”.

Note:  During an Unguided cal, you can access ONLY mechanical cal kits #1 through #95. However, there is no limit to the number of cal kits that can be imported.

This command effectively does the same task as SENS:CORR:COLL:CKIT:PORT which specifies the cal kit by name instead of this command which specifies by number.

Parameters

 

<cnum>

Any existing channel number; if unspecified, value is set to 1.

<num>

The number of the calibration kit. Choose from:

Use SENSe:CORRection:COLLect:CKIT:RESet to restore Cal Kits to default values.

 

Name

1

Cal Kit 1

2

Cal Kit 2

3

Cal Kit 3

 

         ''

 

         ''

94

Cal Kit 94

95

Cal Kit 95

99

ECal module

Note: Always check the list of available cal kits using SENSe:CORRection:COLLect:CKIT:CATalog? to ensure that the correct cal kit is selected.

Examples

SENS:CORR:COLL:CKIT 2
sense2:correction:collect:ckit:select 7

Query Syntax

SENSe<cnum>:CORRection:COLLect:CKIT?

Return Type

Numeric

Default

Last kit selected


SENSe:CORRection:COLLect:CKIT:STANdard:C0 <num>

Applicable Models: All

(Read-Write) Sets the C0 value (the first capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for C0 in femtofarads (1E-15)

Examples

The following commands set C0=15 femtofarads:

SENS:CORR:COLL:CKIT:STAN:C0 15
sense:correction:collect:ckit:standard:c0 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:C0?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:C1 <num>

Applicable Models: All

(Read-Write) Sets the C1 value (the second capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for C1.

Examples

The following two commands set C1=15:

SENS:CORR:COLL:CKIT:STAN:C1 15
sense:correction:collect:ckit:standard:c1 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:C1?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:C2 <num>

Applicable Models: All

(Read-Write) Sets the C2 value (the third capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for C2.

Examples

The following two commands set C2:

SENS:CORR:COLL:CKIT:STAN:C2 15
sense:correction:collect:ckit:standard:c2 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:C2?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:C3 <num>

Applicable Models: All

(Read-Write) Sets the C3 value (the fourth capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for C3.

Examples

The following two commands set C3

SENS:CORR:COLL:CKIT:STAN:C3 15
sense:correction:collect:ckit:standard:c3 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:C3?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:CHARacter <char>

Applicable Models: All

(Read-Write) Sets the media type of the selected calibration standard.

Parameters

 

<char>

Media type of the standard. Choose from:
Coax
- Coaxial Cable
Wave
- Waveguide

Examples

SENS:CORR:COLL:CKIT:STAN:CHAR COAX
sense:correction:collect:ckit:standard:character wave

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:CHARacter?

Return Type

Numeric

Default

Coax


SENSe:CORRection:COLLect:CKIT:STANdard:DATA:LOAD <string>

Applicable Models: All

(Write-only) Loads response (and optionally accuracy) data from a file for the selected database standard. Accuracy data is loaded if the file being loaded contains accuracy data. Learn more.

Parameters

 

<string>

Path and filename.

Examples

SENS:CORR:COLL:CKIT:STAN:DATA:LOAD "c:\users\public\network analyzer\database_file.dat"

Default

Not Applicable

SENSe:CORRection:COLLect:CKIT:STANdard:DELay <num>

Applicable Models: All

(Read-Write) Sets the electrical delay value for the selected standard.

Parameters

 

<num>

Electrical delay in picoseconds


Examples

The following two commands set delay to 50 picoseconds

SENS:CORR:COLL:CKIT:STAN:DEL 50e-12
sense2:correction:collect:ckit:standard:delay 50ps

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:DELay?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:FMAXimum <num>

Applicable Models: All

(Read-Write) Sets the maximum frequency for the selected standard.

Parameters

 

<num>

Maximum frequency in Hertz.

Examples

SENS:CORR:COLL:CKIT:STAN:FMAX 9e9
sense:correction:collect:ckit:standard:fmaximum 9Ghz

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:FMAXimum?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:FMINimum <num>

Applicable Models: All

(Read-Write) Sets the minimum frequency for the selected standard.

Parameters

 

<num>

Minimum frequency in Hertz.

Examples

SENS:CORR:COLL:CKIT:STAN:FMIN 1e3
sense:correction:collect:ckit:standard:fminimum 1khz

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:FMINimum?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:IMPedance <num>

Applicable Models: All

(Read-Write) Sets the characteristic impedance for the selected standard.

Parameters

 

<num>

Impedance in Ohms

Examples

SENS:CORR:COLL:CKIT:STAN:IMP 75
sense:correction:collect:ckit:standard:impedance 50.3

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:IMPedance?

Return Type

Numeric

Default

50


SENSe:CORRection:COLLect:CKIT:STANdard:L0 <num>

Applicable Models: All

(Read-Write) Sets the L0 value (the first inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for L0 in femtohenries (1E-15)

Examples

The following two commands set L0=15  femtohenries:

SENS:CORR:COLL:CKIT:STAN:L0 15
sense:correction:collect:ckit:standard:l0 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:L0?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:L1 <num>

Applicable Models: All

(Read-Write) Sets the L1 value (the second inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for L1.

Examples

The following two commands set L1=15:

SENS:CORR:COLL:CKIT:STAN:L1 15
sense:correction:collect:ckit:standard:l1 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:L1?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:L2 <num>

Applicable Models: All

(Read-Write) Sets the L2 value (the third inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for L2.

Examples

The following two commands set L2=15:

SENS:CORR:COLL:CKIT:STAN:L2 15
sense:correction:collect:ckit:standard:l2 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:L2?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:L3 <num>

Applicable Models: All

(Read-Write) Sets the L3 value (the fourth inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com.

Parameters

 

<num>

Value for L3.

Examples

The following two commands set L3=15:

SENS:CORR:COLL:CKIT:STAN:L3 15
sense:correction:collect:ckit:standard:l3 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:L3?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:LABel <name>

Applicable Models: All

(Read-Write) Sets the label for the selected standard. The label is used to prompt the user to connect the specified standard.

Parameters

 

<name>

Label for the standard; Must be enclosed in quotes. Any string between 1 and 12 characters long. Cannot begin with a numeric.

Examples

SENS:CORR:COLL:CKIT:STAN:LAB 'OPEN'
sense:correction:collect:ckit:standard:label 'Short2'

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:LABel?

Return Type

String

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:LOSS <num>

Applicable Models: All

(Read-Write) Sets the insertion loss for the selected standard.

Parameters

 

<num>

Insertion loss in Gohms / sec. (GigaOhms per second of electrical delay)

Examples

SENS:CORR:COLL:CKIT:STAN:LOSS 3.5e9
sense:correction:collect:ckit:standard:loss 3

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:LOSS?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:REMove

Applicable Models: All

(Write only) Deletes the selected standard from the selected cal kit.

Examples

SENS:CORR:COLL:CKIT:STAN:REMove

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:SDEScription <string>

Applicable Models: All

(Read-Write) Modifies the description of the selected standard of the selected kit. This description appears in the edit kit dialog box.

Parameters

 

<string>

Description of the standard.

Examples

SENS:CORR:COLL:CKIT:STAN:SDES "My New Standard"

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:SDEScription?

Return Type

String

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard[:SELECT] <num>

Applicable Models: All

(Read-Write) Selects the calibration standard. All subsequent "CKIT" commands to modify a standard will apply to the selected standard. Select a calibration kit using SENS:CORR:COLL:CKIT:SEL

Parameters

 

<num>

Number of the standard. Choose any number between:
1
and 1000

Examples

SENS:CORR:COLL:CKIT:STAN 3
sense:correction:collect:ckit:standard:select 8

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard[:SELect]?

Return Type

Numeric

Default

1


SENSe:CORRection:COLLect:CKIT:STANdard:TYPE <char>

Applicable Models: All

(Read-Write) Sets the type for the selected standard.

Parameters

 

<char>

Choose from:
OPEN
SHORT
LOAD

SLOAD
(sliding load)

THRU (through)

ARBI (arbitrary)

DATabased (data-based)

Examples

SENS:CORR:COLL:CKIT:STAN:TYPE LOAD
sense:correction:collect:ckit:standard:type short

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:TYPE?

Return Type

Character

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:TZReal <num>

Applicable Models: All

(Read-Write) Sets the TZReal component value of the Terminal Impedance for the selected standard.

Note: Only applicable when the Standard Type is set to ARBI

Parameters

 

<num>

Value for TZReal in Ohms


Examples

The following commands set TZReal=15 Ohms:

SENS:CORR:COLL:CKIT:STAN:TZReal 15
sense:correction:collect:ckit:standard:TZReal 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:TZReal?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:STANdard:TZImag <num>

Applicable Models: All

(Read-Write) Sets the TZImag component value of the Terminal Impedance for the selected standard.

Note: Only applicable when the Standard Type is set to ARBI

Parameters

 

<num>

Value for TZImag in Ohms

Examples

The following two commands set TZImag=15 Ohms:

SENS:CORR:COLL:CKIT:STAN:TZImag 15
sense:correction:collect:ckit:standard:TZImag 15

Query Syntax

SENSe:CORRection:COLLect:CKIT:STANdard:TZImag?

Return Type

Numeric

Default

Not Applicable


SENSe:CORRection:COLLect:CKIT:TRLoption:IMPedance <char>

Applicable Models: All

(Read-Write) Sets the reference impedance when using this TRL cal kit. Learn more.

Before sending this command, select a cal kit using SENS:CORR:COLL:CKIT:SELect.

Parameters

 

<char>

Choose from:

SYSTem - The system impedance is used as the reference impedance. During a Guided or Unguided Cal, the Z0 of the Cal standard's connector definition sets the System Z0.

Make this selection when the desired test port impedance differs from the impedance of the LINE standard. Also, make this selection when skin effect impedance correction is desired for coax lines.

LINE  The impedance of the line standard is used as the reference impedance, or center of the Smith Chart. Any reflection from the line standard is assumed to be part of the directivity error.

Examples

SENS:CORR:COLL:CKIT:TRL:IMP SYST

sense:correction:collect:ckit:trloption:impedance line

Query Syntax

SENSe:CORRection:COLLect:CKIT:TRLoption:IMPedance?

Return Type

Character

Default

LINE


SENSe:CORRection:COLLect:CKIT:TRLoption:LRLChar <bool>

 Applicable Models: All

(Read-Write)  This setting ONLY applies if an LRL Cal Kit is being modified AND Testport Reference Plane is set to THRU AND the TRL Thru class standard and the TRL Line/Match class standard both have the same values for Offset Z0 and Loss. Otherwise, this setting is ignored.

Before sending this command, select a cal kit using SENS:CORR:COLL:CKIT:SELect.

Parameters

 

<bool>

Choose from:

1 or ON - Automatically correct for line loss and dispersion characteristics.

0 or OFF - Select when anomalies appear during a calibrated measurement which may indicate different loss and impedance values for the Line standards.

Examples

SENS:CORR:COLL:CKIT:TRL:LRLC 1

sense:correction:collect:ckit:trloption:lrlchar off

Query Syntax

SENSe:CORRection:COLLect:CKIT:TRLoption:LRLChar?

Return Type

Boolean

Default

OFF


SENSe:CORRection:COLLect:CKIT:TRLoption:RPLane <char>

Applicable Models: All

(Read-Write) Sets the reference impedance when using this cal kit. Learn more.

Before sending this command, select a cal kit using SENS:CORR:COLL:CKIT:SELect.

Parameters

 

<char>

Choose from:

THRU  The THRU standard definition is used to establish the measurement reference plane. Select if the THRU standard is zero-length or very short.

REFLect  The REFLECT standard definition is used to establish the position of the measurement reference plane. Select if the THRU standard is not appropriate AND the delay of the REFLECT standard is well defined.  Also, select If a flush short is used for the REFLECT standard because a flush short provides a more accurate phase reference than a Thru standard.

Examples

SENS:CORR:COLL:CKIT:TRL:RPL THRU

sense:correction:collect:ckit:trloption:rplane reflect

Query Syntax

SENSe:CORRection:COLLect:CKIT:TRLoption:RPLane?

Return Type

Character

Default

THRU