Sense:Source Command


SENSe:SOURce

     | PLLBandwidth

          |  CATalog

          | [:VALue]

     | RECeiver

      | GAIN[:VALue]

         | ALL[:VALUE]

         | CATalog

         | COUPling

             | ALL[:VALue]

             | [:STATe]

         | LIST


SENSe<cnum>:SOURce:PLLBandwidth:CATalog?

Applicable Models: M98xxA, P50xxA/B, P93xxB, E5080B, E5081A

(Read-Write) Lists PLL bandwidth type for SENSe<cnum>:SOURce:PLLBandwidth[:VALue].

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

Examples

SENSe1:SOUR:PLLB:CAT?
sense2:source:pllbandwidth:catalog?

Query Syntax

SENSe<cnum>:SOURce:PLLBandwidth:CATalog?

Return Type

<sting>, available setting list with comma separated chars

Default

Not applicable


SENSe<cnum>:SOURce:PLLBandwidth[:VALue] <type>

Applicable Models:  M98xxA, P50xxA/B, P93xxB, E5080B, E5081A

(Read-Write) Sets and read the settings for PLL bandwidth for RF source and LO. The source and LO settings are coupled.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<type>

choose from:

  • AUTO: Use an appropriate PLL bandwidth automatically.

  • NARRow: Use the narrow PLL bandwidth. The phase noise of the RF and local sources decreases while the cycle time increases.

Examples

SENSe1:SOUR:PLLB NARR  
sense2:source:pllbandwidth narrow

Query Syntax

SENSe<cnum>:PLLBandwidth[:VALue]?

Return Type

Enumeration

Default

AUTO


SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN[:VALue] <string>

Applicable Models:  M98xxA, P50xxA/B, P93xxB, E5080B, E5081A,

(Read-Write) Sets the gain settings to a specified port. Use SENS:SOUR:REC:GAIN:CAT? to return a list of available gain states for the specified port.

Note: (M983xA) This command works only when the gain coupling is enabled by :SENS:SOUR:REC:GAIN:COUP:ALL.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<sport>

Source port number of the VNA. If unspecified, value is set to 1

<rport>

Receiver port number of the VNA. If unspecified, value is set to 1

<string>

Receiver gain state. Not case sensitive.

choose from:

  • Auto

  • Low

  • High

Examples

SENSe:SOUR1:REC2:GAIN "Low" ' Low for S21 measurement
sense:source2:receiver2:gain:value "High"  ' High for S22 measurement

Query Syntax

SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN[:VALue] ?

Return Type

<sting>, available setting list with comma separated chars

Default

Not


SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:AUTorange

Applicable Models: 

(Read-Write) Sets all gains to "auto". Source/Receiver port ignored.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<sport>

Ignored

<rport>

Ignored

Examples

SENSe:SOUR1:REC2:GAIN:AUT ON

Query Syntax

SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:AUT?

Return Type

Boolean (0: OFF, 1: ON)

Default

OFF


SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:ALL[:VALue] <string>

Applicable Models:  M98xxA, P50xxA/B, P93xxB, E5080B, E5081A,

(Read-Write) Sets the gain settings to all ports. Use SENS:SOUR:REC:GAIN:CAT? to return a list of available gain states for the VNA.

Note: (M983xA) This command works only when the gain coupling is enabled by :SENS:SOUR:REC:GAIN:COUP:ALL.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<sport>

Ignored

<rport>

Ignored

<string>

Receiver gain state. Not case sensitive.

choose from:

  • Auto

  • Low

  • High

Examples

SENSe:SOUR1:REC2:GAIN:ALL "Low" ' Low for all measurements
sense:source2:receiver2:gain:all:value "High"  ' High for all measurements

Query Syntax

SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:ALL[:VALue] ?

Return Type

String. "MIXED" is returned when the settings are not the same.

Default

Auto


SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:CATalog

Applicable Models:  M98xxA, P50xxA/B, P93xxB, E5080B, E5081A,

(Read only) Reads a list of valid state for the receiver gain on the specified port.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<sport>

Source port number of the VNA. If unspecified, value is set to 1

<rport>

Receiver port number of the VNA. If unspecified, value is set to 1

Examples

SENSe:SOUR1:REC2:GAIN:CAT?
sense:source2:receiver2:gain:catalog?

Query Syntax

SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:CATalog?

Return Type

String (Comma-separated list of strings.) ("Auto,Low,High" is returned.)

Default

Auto


SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:COUPling:ALL[:VALue] <type>

Applicable Models: M983xA,

(Read-Write) Set and read the setting for receiver gain coupling for all port in the specified channel. This command does not wok for NF, NFX, SA, MOD, and MODX measurement class.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<sport>

Ignored

<rport>

Ignored

<Type>

choose from:

  • OFF

  • ON

  • Mixed (Read only) This is returned when the setting is not same in the multi-module configuration of M980xA and M983xA

Examples

SENSe:SOUR1:REC:GAIN:COUP:ALL ON  
sense:source2:receiver:gain:coupling:all:value on

Query Syntax

SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:COUPling:ALL[:VALue]?

Return Type

Enum

Default

ON


SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:COUPling[:STATe]

Applicable Models: M983xA,

(Read only) Returns the status per port for receiver gain coupling.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<sport>

Ignored

<rport>

Receiver port number of the VNA. If unspecified, value is set to 1

Examples

SENSe:SOUR1:REC:GAIN:COUP? 
sense:source2:receiver:gain:coupling:state?

Query Syntax

SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:COUPling[:STATe]?

Return Type

Boolean (0: OFF, 1: ON)

Default

ON


SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:LIST?

Applicable Models:  M98xxA, P50xxA/B, P93xxB, E5080B, E5081A,

(Read only) Gets the data array for actual gain setting of each measurement points. High: 1, Low: 0. The number of returned data is the same as the NOP.

Parameters

<cnum>

Any existing channel number. If unspecified, value is set to 1

<sport>

Source port number of the VNA. If unspecified, value is set to 1

<rport>

Receiver port number of the VNA. If unspecified, value is set to 1

Examples

SENSe:SOUR1:REC2:GAIN:LIST?
sense:source2:receiver2:gain:list?

Query Syntax

SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:LIST?

Return Type

Data block

Default

Not Applicable