Receiver Gain

The receiver gain can be fixed on the M98xxA and P50xxA/B. When the receiver gain is lower than expected, for example due to an unexpected spurious signal, this function allows you to fix the gain level to improve the dynamic range. The measurement speed is almost the same even if the range is fixed.

Note: Receiver Gain for P937xB always set at LOW.

How to make Receiver Gain settings

Use one of the following methods to set port power. The softkey is available on standard measurement class only.

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Setup > Internal Hardware > Receiver Gain.... or Rcvr Gain Mode

  1. Click Instrument > Setup  > Internal Hardware> Internal Hardware > Receiver Gain... or Rcvr Gain Mode

Programming Commands

If the gain is automatic, or varies by source port, calibration will take place in multiple gain settings. The analyzer has the independent error terms for high and low receiver settings. Each error terms can be monitored in Cal Set Viewer. Error terms with square brackets refer to high [1] or low [0] settings. Error terms without any square brackets refer to the low gain. When calibration is acquired in the high gain setting, a maximum power of -25 dBm will be used. 

Note: The wideband/reference calibration set must have the same switched gain settings as the user cal set.

Calibration Time Reduction (Fixed Gain Calibration)

When receiver gain settings includes AUTO or combination of High and Low, the analyzer measures the error terms for both high and low settings automatically. Hence, the analyzer make sweeps three times in the calibration.

When receiver gain settings are all FIXED (high or low) and have same state for each source port, the VNA takes sweep for the calibration only one time for specified gain setting in order to reduce the calibration time.

For example, the following setting can reduce the calibration time.

Receiver gain setting

Receiver port

1

2

3

4

Source Port

1

Low

High

Low

High

2

Low

High

Low

High

3

Low

High

Low

High

4

Low

High

Low

High

 

Receiver gain setting

Receiver port

1

2

3

4

Source Port

1

Low

High

High

High

2

Low

High

High

High

3

Low

High

High

High

4

Low

High

High

High

 

Receiver Overload / ADC Overflow

When the receiver gain is set at Auto, the pre-measurement is done to select the proper range (HIGH or LOW). SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:LIST? returns the information which range is used at each test point.

The receiver overload/ADC overflow may occur in the following conditions when the receiver gain is set at HIGH (including HIGH in AUTO setting)

Receiver overload can be turned off in the preference.

M983xA Gain Coupling and M983xA/M980xA Receiver Gain Control for Application

Application

Receiver Gain Control

Gain Coupling

(M983xA only)

RF Atten and IF Gain Control

(M983xA only)

Note

Standard

Available

Available

Available

 

Pulse measurement

Available

Available

Available

Receiver Gain is set at LOW internally when AUTO

FOM

Available

Available

Available

Receiver Gain is set at RF:LOW, IF:AUTO internally when AUTO

Noise Figure, Noise Figure Converter in Noise Path (Bypass)

-

-

-

High/Medium/Low in Noise Figure dialog box

Noise Figure, Noise Figure Converter in S parameter

Disabled

Always off "Manual"

Available

 

Spectrum Analysis, Modulation, Modulation Converter

Disabled

Always off "Manual"

Available

 

SMC, SMC+Phase, Gain Compression, Gain Compression Converter, Active Hot Parameter

Disabled: Fixed at Auto

Available

Available

Receiver Gain is set at RF:LOW, IF:AUTO internally

Diff IQ, IMD, IMD Converter

Disabled: Fixed at Low

Available

Available

 

Enhanced TD

Disabled: Fixed at Low

Always  on "Per Source"

Disable

Receiver Gain is set at RF:LOW, IF:LOW internally.

 

Receiver Gain dialog box help

M980xA, P50xxA/B

This dialog provides basic control receiver for a specific port.

This table consists of source port rows and receiver port columns. Each cell is corresponded to measurements in the active channel. (e.g. ‘Receiver port 1 – Source port 3’ is corresponded to S13, a1,3 and b1,3.)

The each cell sets the setting by the following drop down list.

  • Auto - (Default) Receiver gain is controlled automatically for each measurement points according to the input signal level.

  • High - Fix the gain setting at high

  • Low - Fix the gain setting at low

Set All Gains - Sets all cells at one time.

M983xA

 

Gain Coupling: When this is checked, the receiver gain can be set from Auto/High/Low. When this is not checked, the selection is disabled and RF attenuator and IF gain can be set independently at the Path Configurator.

Note: When the mult-port (multi-module) configuration is made by both M980xA and M983xA, the selection of Manual is not applied to M980xA because there is no RF & IF path configuration.

Note: In "Manual", the receiver gain for Bypass 20 GHz/44 GHz is fixed at a certain value according to the frequency.

Note: When the receiver gain is set at AUTO, the gain is fixed at LOW when the "RF In Switch" selects "External".

 

Reciever Gain Mode

Desctiption

Per Source

The receiver gain can be set at a specific port.

This table consists of source port rows and receiver port columns. Each cell is corresponded to measurements in the active channel. (e.g. ‘Receiver port 1 – Source port 3’ is corresponded to S13, a1,3 and b1,3.)

The each cell sets the setting by the following drop down list.

  • Auto - (Default) Receiver gain is controlled automatically for each measurement points according to the input signal level.

  • High - Fix the gain setting at high

  • Low - Fix the gain setting at low

Set All Gains - Sets all cells at one time

Autorange

The all receiver gains are set at Auto.

Manual

RF attenuator and IF gain can be set independently at the Path Configurator. Selection for High/Low/Auto is disabled.

 

Receiver Gain for Segment Sweep dialog box help

In Sweep Segment Table Dialog, Check the check box of Receiver Gain.

M980xA, P50xxA/B

M983xA

This dialog provides basic control receiver gain of the specified segment for a specific port in the segment sweep. The receiver gain in Segment Table dialog box should be turned on, then click Edit under Rev Gain column in the Segment Table,

The setting description is the same as the Receiver Gain above.