Mechanical Devices


Other System Configuration Topics

Overview

Note: To prevent premature wear, the VNA does not allow attenuators or other mechanical switches to switch continuously.

These mechanical devices are set for the entire channel. When more than one channel is used, and a mechanical device setting is NOT the same for all channels, only the ACTIVE channel is allowed to sweep. All other channels are Blocked - NOT allowed to sweep. Blocked channels will resume sweeping when they are made ACTIVE, or when the conflict is resolved.

Press Trigger > Main > Restart to cause ALL channels to sweep once. Then the active channel will resume sweeping continuously.

The Mechanical Devices dialog shows the settings of all of the switches and attenuators in the VNA. The settings for all active channels are shown side-by-side for easy comparison. This dialog allows you to determine the settings which would cause mechanical devices to switch between states on consecutive sweeps, potentially leading to device wear-out. It also allows you to determine if the conflict can be resolved to enable continuous sweeps on all channels.

The following are the mechanical devices that are potentially shown in the dialog. These components may not appear in your VNA model:

How to access Mechanical Devices settings

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Setup > Internal Hardware > Mechanical Devices...

  1. Click Instrument

  2. Select Setup
  3. Select Internal Hardware

  4. Select Mechanical Devices...

Remote commands

SCPI: SENSe<cnum>:SWEep:BLOCked?

COM: IsBlocked Property

Mechanical Devices dialog box help

See Mechanical Devices Overview (scroll up)

The devices that appear in the table depend on the VNA model and options.

> Yellow highlighted cell indicates the Active channel.

 Blue  highlighted cells indicate the following:

  • The channel is NOT able to sweep. Blocked is shown in the top row.

  • The highlighted device settings differ from that of the sweeping channels.

To modify entries in the table, click a cell.

When a selection is changed, the new setting is applied immediately.

Limitations

  • Measurement Class can NOT be changed from this dialog.

  • The dialog does NOT report device settings for multiport test sets.

  • This dialog does NOT report device settings for external sources.

Copy Active  Available ONLY when there is a conflict which causes at least one channel to be Blocked.  When clicked, the mechanical device settings of the Active channel are copied to the Blocked channels.  A warning message appears to remind you that power to one or more channels may be increased.  Exception: When one or more Noise channels are present, then the settings of the two Noise switches are be determined by the lowest-numbered Noise channel if none are the active channel.

Trigger  Launches the Trigger dialog box.

OK  Closes the dialog box.

Cancel  Does not apply changes that were made, and closes the dialog box.