Last updated: 2014-11-28
CALL[:CELL]:CLPControl:DOWNlink:DPCHannel:LEVel:RECord:COUNt
CALL[:CELL]:CLPControl:DOWNlink:DPCHannel:LEVel:RECord:STARt
CALL[:CELL]:CLPControl:DOWNlink:DTCHannel:TARGet:QUALity:STATe
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries Maximum DPCH Level. |
|
Setting |
Range:-20.00 dB to 0 dB Resolution:0.01 Increment: 0.1 |
|
Query |
Same as setting |
|
*RST Setting |
0dB |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:DPCHANNEL:LEVEL:MAXIMUM -18" |
|
Function |
Sets/queries Minimum DPCH Level. |
|
Setting |
Range:-20.00 dB to 0 dB Resolution:0.01 Increment: 0.1 |
|
Query |
Same as setting |
|
*RST Setting |
-20.00dB |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:DPCHANNEL:LEVEL:MINIMUM -19" |
|
Function |
Sets/queries the DPCH Level Sequence Record Count. This setting can be changed when DPCH power offset sequence record is not started. |
|
Setting |
Range: 1 to 30000 Resolution:1 Increment: 1 |
|
Query |
Same as setting |
|
*RST Setting |
1000 |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:DPCHANNEL:LEVEL:RECORD:COUNT 1000" |
|
Function |
This action starts the recording of DPCH power offset sequence. |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:DPCHANNEL:LEVEL:RECORD:START" |
|
Function |
This action stops the recording of DPCH power offset sequence. |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:DPCHANNEL:LEVEL:RECORD:STOP" |
|
Function |
Sets/queries the Target Quality on DTCH. This setting can be changed in Idle state in Active Cell operating mode or Downlink Closed Loop Power Control State is set to Off. |
|
Setting |
Range: 0.01% to 100% Resolution:0.01% Increment: 0.01% |
|
Query |
Same as setting |
|
*RST Setting |
0.01% |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:DTCHANNEL:TARGET:QUALITY 0.01" |
|
Function |
Sets/queries whether the BLER target is to be assigned to a DTCH. This setting can be changed in Idle state in Active Cell operating mode or Downlink Closed Loop Power Control State is set to Off. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Same as setting |
|
*RST Setting |
0 (Off) |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:DTCHANNEL:TARGET:QUALITY:STATE 0" |
|
Function |
Sets/queries Downlink Closed Loop Power Control State. |
|
Setting |
Range: ON|OFF |
|
Query |
Same as setting |
|
*RST Setting |
OFF |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:DOWNlINK:STATE ON" |
|
Function |
This action sends an additional Down TPC command to the UE to decrease its power by one step. This operation is only allowed when the UL CL Power Ctrl Mode is set to Alternating bits. |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:UPLINK:IMMEDIATE:DOWN" |
|
Function |
This action sends an additional Up TPC command to the UE to increase its power by one step. This operation is only allowed when the UL CL Power Ctrl Mode is set to Alternating bits. |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:CLPCONTROL:UPLINK:IMMEDIATE:UP" |
|
Function |
Sets/queries the uplink closed power control mode when in the active cell operating mode. See UL CL Power Ctrl Mode. |
|
Setting |
Range: ACTive | ALTernating| UP | DOWN |
|
Query |
Range: ACT | ALT| UP | DOWN |
|
*RST Setting |
ACT |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:CLPControl:UPLink:MODE ACTive" |
|
Function |
Sets/queries UL CL Power Ctrl Step Size when in the active cell operating mode. |
|
Setting |
Range: 1|2|3 dB |
|
Query |
Range: 1|2|3 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CLPControl:UPLink:STEPsize 2" |