Last updated: 2014-11-28
The settings below can be set in active cell operating mode only when the call status is Idle, or in other operating modes.
If BCCH Update Page is set to Auto and you change the settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure ; If BCCH Update Page is set to Inhibit (the default value) and you change the settings while your UE is camped to the test set, the UE is informed to re-read the BCCH to observe the change (see CALL:BCCHannel:UPDAte:PAGE AUTO).
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries Network Mode of Operation in TD-SCDMA network: If the setting is 1, the network operates in mode I that the MSC (Mobile Switching Centre) and the SGSN (Serving GPRS Support Node) are connected together; else if the setting is 2, the network operates in Mode II that these two network elements are not inter-connected. |
|
Setting |
Range: 1|2 |
|
Query |
Range: 1|2 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:NMOPeration:TDSCdma 2" |