Last updated: 2014-11-28
The settings below can be set in active cell operating mode only when the call status is Idle, or in other operating modes.
If BCCH Update Page is set to Auto and you change the settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure ; If BCCH Update Page is set to Inhibit (the default value) and you change the settings while your UE is camped to the test set, the UE is informed to re-read the BCCH to observe the change (see CALL:BCCHannel:UPDAte:PAGE AUTO).
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the Routing Area Code (RAC) when using the TD-SCDMA application. It can be set when PS domain information is set to "Present". |
|
Setting |
Range: 0 to 255 |
|
Query |
Range: 0 to 255 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:RACode:TATDscdma 2" |
|
Function |
Sets/queries the Routing Area Code (RAC) for the currently selected application. It can be set when PS domain information is set to "Present". |
|
Setting |
Range: 0 to 255 |
|
Query |
Range: 0 to 255 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:RACode 2" |