Last updated: 2014-11-28
The UE must be set to receive the downlink signal on the proper frequency. You can set the downlink frequency manually or automatically, depending upon the RF Gen Freq Ctrl setting.
When RF Gen Freq Ctrl is set to Auto , the downlink frequency is determined by the Channel setting.
RF Gen Freq
When RF Gen Freq Ctrl is set to Manual , the downlink frequency is determined by the RF Gen Freq setting. The RF Gen Freq setting is only applicable to TD-SCDMA Test operating mode and CW Operating Mode (in CW operating mode, generator frequency control is always manual).
GPIB Commands: CALL:CONTrol, CALL:RFGenerator